Article [#4533] write/erase flash cause watchdog not working

[#4533] write/erase flash cause watchdog not working

Submitted By: david wang

Open Date

2008-10-15 23:25:08     Close Date

2008-12-17 14:52:39

Priority:

Medium High     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2008R1.5-RC3     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

0.2

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

u-boot-1.1.6-2008R1.5     Toolchain version or rev.:

App binary format:

N/A     

Summary: write/erase flash cause watchdog not working

Details:

  If I add flash write operation into crash_test, the watchdog daemon can't reboot the system successfully after crash, and the board hang. By a jtag ice, I found it did assert a reset, but the u-boot not start. After one day's debugging, I thing I have found the problem making the board hang. I put a hardware breakpoint at 0x20000000 and another at 0x20000004. if every thing goes well, each breakpoint should be hit once when the system reboot , just like manual rest in u-boot. In my test, it can only reach the first breakpoint, not the next. I use x command to check the flash, it show me all of 0x00800080, that means the flash is not ready. But, I just find the problem, I don't know why the flash status is not ready, and how to fix it. Does anyone have any idea? Thanks

  pls try my test program -- see attached file, in your stamp board to help me find out it's a hardware or software issue? Thanks a lot!  The only thing you should change is the flash device. In my test , I use dev/mtd3. I have create 8 mtd device in my board.

  I'm using my bf537 board which is very simular to STAMP board, with a intel 28f320c3t flash.

Follow-ups

--- Mike Frysinger                                           2008-12-17 14:52:38

not a bug in the watchdog/software.  limitation in hardware.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

crash_test.c    application/octet-stream    977    david wang

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.