Article [#4541] breakpoint in kgdb would trigger twice

[#4541] breakpoint in kgdb would trigger twice

Submitted By: Mingquan Pan

Open Date

2008-10-17 05:33:10     Close Date

2008-12-03 22:56:30

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Duplicate

Uboot version or rev.:

    Toolchain version or rev.:

Oct 10

App binary format:

N/A     

Summary: breakpoint in kgdb would trigger twice

Details:

breakpoint in kgdb through uart port would fails after serveral times on trunk head. When set break kgdb_test on host, cat /proc/kgdbtest on target sometimes would break 2 times, and sometimes would not stop at all.

## Starting application at 0x001962c0 ...

Linux version 2.6.26.5-ADI-2009R1-pre-svn5430-dirty (test@uclinux50-bf537-stamp-ad9960-ad1836) (gcc version 4.1.2 (ADI svn)) #8 Fri Oct 17 15:42:56 CST 208

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:                                                                                                                                                ...

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 20) is a BFIN-UART

kgdb: Registered I/O driver kgdboc.

brd: module loaded

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1                                                                                    

root:/> PHY: 0:01 - Link is Up - 100/Full

init: /bin/watchdogd respawning too fast

SysRq : GDB

Entering KGDB

root:/> init: /bin/watchdogd respawning too fast

cat /proc/kgdbtest

kgdb name(12): hello world!, 85, 16

ttyBF0: 1 input overrun(s)

root:/>                                                                                                                                                   

On host:test@uclinux50-bf537-stamp-ad9960-ad1836:~/work/cruise/checkouts/uclinux-dist> bfin-uclinux-gdb linux-2.6.x/vmlinux

GNU gdb 6.6

Copyright (C) 2006 Free Software Foundation, Inc.

GDB is free software, covered by the GNU General Public License, and you are

welcome to change it and/or distribute copies of it under certain conditions.

Type "show copying" to see the conditions.

There is absolutely no warranty for GDB.  Type "show warranty" for details.

This GDB was configured as "--host=i686-pc-linux-gnu --target=bfin-uclinux"...

(gdb) set remotebaud 57600

(gdb) target remote /dev/ttyUSB0

Remote debugging using /dev/ttyUSB0

kgdb_breakpoint () at kernel/kgdb.c:1675

1675            atomic_set(&kgdb_setting_breakpoint, 0);

(gdb) break kgdb_test

Breakpoint 1 at 0x8ade: file arch/blackfin/kernel/kgdb_test.c, line 48.

(gdb) c

Continuing.

[New Thread 156]

[Switching to Thread 156]

Breakpoint 1, kgdb_test (name=<value optimized out>, len=<value optimized out>, count=<value optimized out>, z=16) at arch/blackfin/kernel/kgdb_test.c:48

48      {

(gdb) c

Continuing.

Follow-ups

--- Sonic Zhang                                              2008-10-20 05:39:22

Can't replicate.

--- Mingquan Pan                                             2008-12-03 03:45:34

Now it is always triggering to stop 2 twice at one breakpoint on the trunk

kernel and this is not exclusive to uart port, but also happens when through

ethernet port.

bfin> boote

Loading .text @ 0x00001000 (1102560 bytes)

Loading .rodata @ 0x0010e2e0 (268408 bytes)

Loading __ksymtab @ 0x0014fb58 (15960 bytes)

Loading __ksymtab_gpl @ 0x001539b0 (5096 bytes)

Loading __ksymtab_strings @ 0x00154d98 (47079 bytes)

Loading __param @ 0x00160580 (380 bytes)

Clearing .bss @ 0x00160700 (88820 bytes)

Loading .data @ 0x001761f4 (65036 bytes)

Loading .init.text @ 0x00186000 (101560 bytes)

Loading .init.data @ 0x0019ecb8 (13744 bytes)

Loading .init.setup @ 0x001a2268 (668 bytes)

Loading .initcall.init @ 0x001a2504 (572 bytes)

Loading .con_initcall.init @ 0x001a2740 (4 bytes)

Loading .init.ramfs @ 0x001a2744 (3519124 bytes)

Loading .text_l1 @ 0xffa00000 (7148 bytes)

sh_addr: FFA00000, p_paddr: 004FD9D8

Loading from: 024E9000 to 004FD9D8, size: 7148

Loading .data_l1 @ 0xff800000 (224 bytes)

sh_addr: FF800000, p_paddr: 004FF5C4

Loading from: 024EB000 to 004FF5C4, size: 224

## Starting application at 0x00194310 ...

Linux version 2.6.28-rc2-ADI-2009R1-pre-svn5794 (test@my-local-machine) (gcc

version 4.1.2 (ADI svn)) #5 Wed Dec 3 15:51:26 CST 2008

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010e2e0

  rodata    = 0x0010e2e0-0x001606fc

  bss       = 0x00160700-0x001761f4

  data      = 0x001761f4-0x00186000

    stack   = 0x00184000-0x00186000

  init      = 0x00186000-0x00500000

  available = 0x00500000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: console=ttyBF0,57600 kgdboe=@10.100.4.50/,@10.100.4.174/

kgdboe: local port 6443

kgdboe: local IP 10.100.4.50

kgdboe: interface eth0

kgdboe: remote port 6442

kgdboe: remote IP 10.100.4.174

kgdboe: remote ethernet address ff:ff:ff:ff:ff:ff

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 51640k/65536k RAM, (3560k init code, 1076k kernel code, 480k

data, 1024k dma, 7756k reserved)

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)

PDA for CPU0 reserved at 00161a38

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 100

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1,

mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

kgdboe: local port 6443

kgdboe: local IP 10.100.4.50

kgdboe: interface eth0

kgdboe: remote port 6442

kgdboe: remote IP 10.100.4.174

kgdboe: remote ethernet address ff:ff:ff:ff:ff:ff

kgdboe: device eth0 not up yet, forcing it

kgdboe: carrier detect appears untrustworthy, waiting 4 seconds

PHY: 0:01 - Link is Up - 100/Full

kgdb: Registered I/O driver kgdboe.

kgdboe: debugging over ethernet enabled

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-08 22:24:45 UTC (685485)

Freeing unused kernel memory: 3560k freed

dma_alloc_init: dma_page @ 0x004fa000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.13.1 (2008-12-03 15:28:28 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/> cat /kinit: /bin/watchdogd respawning too fast

root:/> cat proc/kgdbtest

kgdb name(12): hello world!, 85, 16

L1(before change) : data variable addr = 0xff800000, data value is 0

L1 : code function addr = 0xffa00390

L1(after change) : data variable addr = 0xff800000, data value is 10

root:/> cat proc/kgdbtest

kgdb name(12): hello world!, 85, 16

L1(before change) : data variable addr = 0xff800000, data value is 10

L1 : code function addr = 0xffa00390

L1(after change) : data variable addr = 0xff800000, data value is 20

root:/> init: /bin/watchdogd respawning too fast

init: /bin/watchdogd respawning too fast

init: /bin/watchdogd respawning too fast

On host:

test@my-local-machine:~/work/cruise/checkouts/uclinux-dist> bfin-uclinux-gdb

/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x/vmlinux

GNU gdb 6.6

Copyright (C) 2006 Free Software Foundation, Inc.

GDB is free software, covered by the GNU General Public License, and you are

welcome to change it and/or distribute copies of it under certain conditions.

Type "show copying" to see the conditions.

There is absolutely no warranty for GDB.  Type "show warranty" for

details.

This GDB was configured as "--host=i686-pc-linux-gnu

--target=bfin-uclinux"...

(gdb) target remote udp:10.100.4.50:6443

warning: The remote protocol may be unreliable over UDP.

Some events may be lost, rendering further debugging impossible.

Remote debugging using udp:10.100.4.50:6443

kgdb_breakpoint () at kernel/kgdb.c:1722

1722            atomic_set(&kgdb_setting_breakpoint, 0);

(gdb)  b kgdb_test

Breakpoint 1 at 0x8baa: file arch/blackfin/kernel/kgdb_test.c, line 77.

(gdb) c

Continuing.

[New Thread 157]

[Switching to Thread 157]

Breakpoint 1, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

Breakpoint 1, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

[New Thread 159]

[Switching to Thread 159]

Breakpoint 1, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

Breakpoint 1, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

--- Mingquan Pan                                             2008-12-03 03:46:16

Now it is always triggering to stop 2 twice at one breakpoint on the trunk

kernel and this is not exclusive to uart port, but also happens when through

ethernet port.

bfin> boote

Loading .text @ 0x00001000 (1102560 bytes)

Loading .rodata @ 0x0010e2e0 (268408 bytes)

Loading __ksymtab @ 0x0014fb58 (15960 bytes)

Loading __ksymtab_gpl @ 0x001539b0 (5096 bytes)

Loading __ksymtab_strings @ 0x00154d98 (47079 bytes)

Loading __param @ 0x00160580 (380 bytes)

Clearing .bss @ 0x00160700 (88820 bytes)

Loading .data @ 0x001761f4 (65036 bytes)

Loading .init.text @ 0x00186000 (101560 bytes)

Loading .init.data @ 0x0019ecb8 (13744 bytes)

Loading .init.setup @ 0x001a2268 (668 bytes)

Loading .initcall.init @ 0x001a2504 (572 bytes)

Loading .con_initcall.init @ 0x001a2740 (4 bytes)

Loading .init.ramfs @ 0x001a2744 (3519124 bytes)

Loading .text_l1 @ 0xffa00000 (7148 bytes)

sh_addr: FFA00000, p_paddr: 004FD9D8

Loading from: 024E9000 to 004FD9D8, size: 7148

Loading .data_l1 @ 0xff800000 (224 bytes)

sh_addr: FF800000, p_paddr: 004FF5C4

Loading from: 024EB000 to 004FF5C4, size: 224

## Starting application at 0x00194310 ...

Linux version 2.6.28-rc2-ADI-2009R1-pre-svn5794 (test@my-local-machine) (gcc

version 4.1.2 (ADI svn)) #5 Wed Dec 3 15:51:26 CST 2008

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010e2e0

  rodata    = 0x0010e2e0-0x001606fc

  bss       = 0x00160700-0x001761f4

  data      = 0x001761f4-0x00186000

    stack   = 0x00184000-0x00186000

  init      = 0x00186000-0x00500000

  available = 0x00500000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: console=ttyBF0,57600 kgdboe=@10.100.4.50/,@10.100.4.174/

kgdboe: local port 6443

kgdboe: local IP 10.100.4.50

kgdboe: interface eth0

kgdboe: remote port 6442

kgdboe: remote IP 10.100.4.174

kgdboe: remote ethernet address ff:ff:ff:ff:ff:ff

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 51640k/65536k RAM, (3560k init code, 1076k kernel code, 480k

data, 1024k dma, 7756k reserved)

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)

PDA for CPU0 reserved at 00161a38

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 100

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1,

mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

kgdboe: local port 6443

kgdboe: local IP 10.100.4.50

kgdboe: interface eth0

kgdboe: remote port 6442

kgdboe: remote IP 10.100.4.174

kgdboe: remote ethernet address ff:ff:ff:ff:ff:ff

kgdboe: device eth0 not up yet, forcing it

kgdboe: carrier detect appears untrustworthy, waiting 4 seconds

PHY: 0:01 - Link is Up - 100/Full

kgdb: Registered I/O driver kgdboe.

kgdboe: debugging over ethernet enabled

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-08 22:24:45 UTC (685485)

Freeing unused kernel memory: 3560k freed

dma_alloc_init: dma_page @ 0x004fa000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.13.1 (2008-12-03 15:28:28 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/> cat /kinit: /bin/watchdogd respawning too fast

root:/> cat proc/kgdbtest

kgdb name(12): hello world!, 85, 16

L1(before change) : data variable addr = 0xff800000, data value is 0

L1 : code function addr = 0xffa00390

L1(after change) : data variable addr = 0xff800000, data value is 10

root:/> cat proc/kgdbtest

kgdb name(12): hello world!, 85, 16

L1(before change) : data variable addr = 0xff800000, data value is 10

L1 : code function addr = 0xffa00390

L1(after change) : data variable addr = 0xff800000, data value is 20

root:/> init: /bin/watchdogd respawning too fast

init: /bin/watchdogd respawning too fast

init: /bin/watchdogd respawning too fast

On host:

test@my-local-machine:~/work/cruise/checkouts/uclinux-dist> bfin-uclinux-gdb

/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x/vmlinux

GNU gdb 6.6

Copyright (C) 2006 Free Software Foundation, Inc.

GDB is free software, covered by the GNU General Public License, and you are

welcome to change it and/or distribute copies of it under certain conditions.

Type "show copying" to see the conditions.

There is absolutely no warranty for GDB.  Type "show warranty" for

details.

This GDB was configured as "--host=i686-pc-linux-gnu

--target=bfin-uclinux"...

(gdb) target remote udp:10.100.4.50:6443

warning: The remote protocol may be unreliable over UDP.

Some events may be lost, rendering further debugging impossible.

Remote debugging using udp:10.100.4.50:6443

kgdb_breakpoint () at kernel/kgdb.c:1722

1722            atomic_set(&kgdb_setting_breakpoint, 0);

(gdb)  b kgdb_test

Breakpoint 1 at 0x8baa: file arch/blackfin/kernel/kgdb_test.c, line 77.

(gdb) c

Continuing.

[New Thread 157]

[Switching to Thread 157]

Breakpoint 1, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

Breakpoint 1, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

[New Thread 159]

[Switching to Thread 159]

Breakpoint 1, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

Breakpoint 1, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

--- Mingquan Pan                                             2008-12-03 04:47:32

And before the second unexpected stop for the breakpoint, if you delete this

breakpoint, and run continue, the app can't get running and has such error:

(gdb) c

Continuing.

Breakpoint 2, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

[New Thread 197]

[Switching to Thread 197]

Breakpoint 2, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) d 2

(gdb) info b

No breakpoints or watchpoints.

(gdb) c

Continuing.

Program received signal SIGTRAP, Trace/breakpoint trap.

kgdb_test (name=<value optimized out>, len=<value optimized out>,

count=<value optimized out>, z=3) at arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

Program received signal SIGTRAP, Trace/breakpoint trap.

kgdb_test (name=<value optimized out>, len=<value optimized out>,

count=<value optimized out>, z=3) at arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

Program received signal SIGTRAP, Trace/breakpoint trap.

kgdb_test (name=<value optimized out>, len=<value optimized out>,

count=<value optimized out>, z=3) at arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) b kgdb_test

Breakpoint 3 at 0x8baa: file arch/blackfin/kernel/kgdb_test.c, line 77.

(gdb) c

Continuing.

Breakpoint 3, kgdb_test (name=<value optimized out>, len=<value

optimized out>, count=<value optimized out>, z=3) at

arch/blackfin/kernel/kgdb_test.c:77

77      {

(gdb) c

Continuing.

[New Thread 198]

[Switching to Thread 198]

--- Sonic Zhang                                              2008-12-03 22:56:30

Duplicated bug of 4603

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.