Article [#4600] pass console=null in kernel command string doesn't work on trunk

[#4600] pass console=null in kernel command string doesn't work on trunk

Submitted By: Mingquan Pan

Open Date

2008-11-04 01:07:34     Close Date

2008-11-04 04:51:25

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

Oct 10

App binary format:

N/A     

Summary: pass console=null in kernel command string doesn't work on trunk

Details:

pass console=null in kernel command string doesn't work on trunk head kernel, it just still outputs to the default ttyBF0 device.

Linux version 2.6.26.5-ADI-2009R1-pre-svn5496 (test@46-bf561-gdbproxy) (gcc version 4.1.2 (ADI svn)) #6 Tue Nov 4 13:22:51 CST 2008

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00109140

  rodata    = 0x00109140-0x0015bca8

  bss       = 0x0015bcc0-0x0016b058

  data      = 0x0016b058-0x0017a000

    stack   = 0x00178000-0x0017a000

  init      = 0x0017a000-0x004fc000

  available = 0x004fc000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

boot memmap: 00000000004fc000 - 00000000037ff000 (usable)

On node 0 totalpages: 14335

  DMA zone: 112 pages used for memmap

  DMA zone: 0 pages reserved

  DMA zone: 14223 pages, LIFO batch:3

  Normal zone: 0 pages used for memmap

  Movable zone: 0 pages used for memmap

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: console=ttyBF0,57600 console=null ip=10.100.4.50

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Kernel managed physical pages: 14335

Memory available: 51656k/65536k RAM, (3592k init code, 1056k kernel code, 452k data, 1024k dma, 7756k reserved)

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)

net_namespace: 192 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

Setting up Blackfin MMR debugfs

msgmni has been set to 100

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 21:37:32 UTC (77852)

IP-Config: Guessing netmask 255.0.0.0

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.0.0.0, gw=255.255.255.255,

     host=10.100.4.50, domain=, nis-domain=(none),

     bootserver=255.255.255.255, rootserver=255.255.255.255, rootpath=

Freeing unused kernel memory: 3592k freed

dma_alloc_init: dma_page @ 0x004f9000 - 256 pages at 0x03f00000

PHY: 0:01 - Link is Up - 100/Full

root:/>

root:/>                                                                                                                                                   

Follow-ups

--- Mike Frysinger                                           2008-11-04 01:52:17

console is cumulative.  your command line has:

console=ttyBF0,57600 console=null ip=...

so it's working fine

--- Mingquan Pan                                             2008-11-04 04:51:25

Yes, I made a mistake here. Sorry.Close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.