Article [#4601] when pass bootargs console=null into kernel from u-boot, the booted up kernel can't be pinged through

[#4601] when pass bootargs console=null into kernel from u-boot, the booted up kernel can't be pinged through

Submitted By: Mingquan Pan

Open Date

2008-11-04 01:25:31     Close Date

2008-12-01 11:38:39

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

Oct 10

App binary format:

N/A     

Summary: when pass bootargs console=null into kernel from u-boot, the booted up kernel can't be pinged through

Details:

when pass bootargs console=null into kernel from u-boot, the booted up kernel can't be pinged through.

This happens after the kernel is upgraded to 2.6.28.

bfin> boote

Loading .text @ 0x00001000 (1090880 bytes)

Loading .rodata @ 0x0010b540 (261576 bytes)

Loading .init.rodata @ 0x0014b308 (80 bytes)

Loading __ksymtab @ 0x0014b358 (15872 bytes)

Loading __ksymtab_gpl @ 0x0014f158 (5048 bytes)

Loading __ksymtab_strings @ 0x00150510 (46718 bytes)

Loading __init_rodata @ 0x0015bb90 (172 bytes)

Loading __param @ 0x0015bc3c (380 bytes)

Clearing .bss @ 0x0015bdc0 (65376 bytes)

Loading .data @ 0x0016bd20 (66272 bytes)

Loading .init.text @ 0x0017c000 (100616 bytes)

Loading .init.data @ 0x00194908 (13656 bytes)

Loading .init.setup @ 0x00197e60 (588 bytes)

Loading .initcall.init @ 0x001980ac (548 bytes)

Loading .con_initcall.init @ 0x001982d0 (4 bytes)

Loading .init.ramfs @ 0x001982d4 (3531229 bytes)

Loading .text_l1 @ 0xffa00000 (6976 bytes)

sh_addr: FFA00000, p_paddr: 004F64B1

Loading from: 024E8000 to 004F64B1, size: 6976

Loading .data_l1 @ 0xff800000 (224 bytes)

sh_addr: FF800000, p_paddr: 004F7FF1

Loading from: 024EA000 to 004F7FF1, size: 224

## Starting application at 0x0018a280 ...

Linux version 2.6.28-rc2-ADI-2009R1-pre-svn5576 (test@my-local-machine) (gcc version 4.1.2 (ADI svn)) #27 Tue Nov 4 14:24:07 CST 2008

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010b540

  rodata    = 0x0010b540-0x0015bdb8

  bss       = 0x0015bdc0-0x0016bd20

  data      = 0x0016bd20-0x0017c000

    stack   = 0x0017a000-0x0017c000

  init      = 0x0017c000-0x004f9000

  available = 0x004f9000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled

Data Cache Enabled (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 ip=10.100.4.50 console=null

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 51668k/65536k RAM, (3572k init code, 1065k kernel code, 451k data, 1024k dma, 7756k reserved)

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 100

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin BF5xx on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

turn off boot console early_BFuart0

Then on host,run :

test@my-local-machine:~/work/cruise/checkouts/uclinux-dist> ping 10.100.4.50

PING 10.100.4.50 (10.100.4.50) 56(84) bytes of data.

From 10.100.4.174: icmp_seq=2 Destination Host Unreachable

From 10.100.4.174 icmp_seq=2 Destination Host Unreachable

From 10.100.4.174 icmp_seq=3 Destination Host Unreachable

From 10.100.4.174 icmp_seq=4 Destination Host Unreachable

--- 10.100.4.50 ping statistics ---

5 packets transmitted, 0 received, +4 errors, 100% packet loss, time 4001ms

, pipe 3

Follow-ups

--- Mike Frysinger                                           2008-11-04 01:53:21

i dont think you have any services defined in /etc/inittab.  if you dont have

any defined, then init will exit, and the kernel will panic ... this is correct

behavior ...

--- Mingquan Pan                                             2008-11-04 03:50:55

but if the kernel command line is only : root=/dev/mtdblock0 rw

earlyprintk=serial,uart0,57600

ip=10.100.4.50 and not with console=null, after the kernel is booted up, it

could be pinged through. And it is fine before the upgrade, with the same kernel

configuration.

--- Mike Frysinger                                           2008-11-04 04:02:52

do you have USER_INIT_CONSOLE_SH turned on ?  if so, then this is still correct

behavior as with a console, init will spawn a console shell and manage that

post your /etc/inittab as well as your configuration (make bugreport)

--- Mingquan Pan                                             2008-11-04 05:06:13

the USER_INIT_CONSOLE_SH is always turnded on by default, it is also on before

the upgrade.

The thing I don't understand is that why before the upgrade this usage is ok,

but not now.

the /etc/inittab and config file are pretty much like the default.

root:/> cat /etc/inittab

# inittab for uClinux

# Format:

# ttyline:termcap-entry:getty-command

#httpd:unknown:/bin/httpd

#sh:unknown:/bin/sh

#ttyS0::respawn:-/bin/sh

#sh:console:respawn:/bin/sh

#console::askfirst:-/bin/sh

inetd:unknown:/sbin/inetd

slog:unknown:/sbin/syslogd -n

klog:unknown:/sbin/klogd -n

watchdogd:unknown:/bin/watchdogd -f -s

config file is attached.

--- Mike Frysinger                                           2008-11-04 05:11:56

according to that inittab and config file, it looks like it should work OK ...

--- Sonic Zhang                                              2008-11-13 01:35:31

Fixed. Should check if tty_driver d is NULL before call kref_get() in

tty_driver_kref_get().

--- Mingquan Pan                                             2008-11-14 05:03:48

Yes,fixed. Close.

--- Mingquan Pan                                             2008-11-25 03:28:27

It is fixed on the other boards except bf533 board, so reopen it. The error log

is same:

bfin> bootelf

Loading phdr 0 to 0x00001000 (1413092 bytes)

Loading phdr 1 to 0x00169b4c (2500142 bytes)

Loading phdr 2 to 0x003cc17a (6952 bytes)

Loading phdr 3 to 0x003cdca2 (192 bytes)

## Starting application at 0x00183150 ...

Linux version 2.6.28-rc2-ADI-2009R1-pre-svn5746

(test@uclinux76-bf533-stamp-elf) (gcc version 4.1.2 (ADI svn)) #41 Mon Nov 24

01:32:55 MST 2008

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 128MB

Kernel Managed Memory: 128MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010b470

  rodata    = 0x0010b470-0x00159fe4

  bss       = 0x00159ff0-0x00169b4c

  data      = 0x00169b4c-0x00178000

    stack   = 0x00176000-0x00178000

  init      = 0x00178000-0x003ce000

  available = 0x003ce000-0x037ff000

  DMA Zone  = 0x07f00000-0x08000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Warning: Compiled for Rev 3, but running on Rev 4

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 398 MHz core clock and 79 MHz System Clock

NOMPU: setting up cplb tables for global access

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line:

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 52864k/131072k RAM, (2392k init code, 1065k kernel code, 435k

data, 1024k dma, 73292k reserved)

Calibrating delay loop... 792.57 BogoMIPS (lpj=1585152)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (57 KB free)

PDA for CPU0 reserved at 0015b194

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 103

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 20300300 IRQ 40 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:04:8b

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs_base@ffc00500, dma channel@5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1973-03-25 20:24:52 UTC (101939092)

Freeing unused kernel memory: 2392k freed

dma_alloc_init: dma_page @ 0x003cb000 - 256 pages at 0x07f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.12.2 (2008-11-24 00:36:35 MST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/>

(Back at uclinux76-bf533-stamp-elf.analog.com)

----------------------------------------------------

Linux Kermit>q

Closing /dev/ttyS0...OK

sh-3.00$ telnet 10.100.4.50

Trying 10.100.4.50...

Failed inital telnet

--- Sonic Zhang                                              2008-12-01 05:16:03

can't replicate. looks your uboot doesn't forward the bootargs to kernel.

--- Mike Frysinger                                           2008-12-01 11:38:39

u-boot-2008.10 doesnt pass kernel args via bootelf as noted in other bugs

--- Mingquan Pan                                             2008-12-03 02:10:54

so change this test case to use uImage instead of linux.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.vender    application/octet-stream    45450    Mingquan Pan

config.kernel    application/octet-stream    32824    Mingquan Pan

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.