Article [#4612] Build kgdb kernel failed in BF561-EZKIT

[#4612] Build kgdb kernel failed in BF561-EZKIT

Submitted By: Vivi Li

Open Date

2008-11-06 02:57:16     Close Date

2008-11-10 23:28:34

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Duplicate

Uboot version or rev.:

    Toolchain version or rev.:

toolchain-2008_Oct_10

App binary format:

N/A     

Summary: Build kgdb kernel failed in BF561-EZKIT

Details:

Build kgdb kernel failed in BF561-EZKIT.

--

  CHK     include/linux/compile.h^M

  UPD     include/linux/compile.h^M

  CC      init/version.o^M

  LD      init/built-in.o^M

  LD      .tmp_vmlinux1^M

arch/blackfin/kernel/built-in.o: In function `test_proc_output':^M

arch/blackfin/kernel/kgdb_test.c:88: relocation truncated to fit: R_pcrel24 against symbol `kgdb_l2_test' defined in .l2.text section in arch/blackfin/kernel/built-in.o^M

arch/blackfin/kernel/built-in.o: In function `kgdb_l2_test':^M

arch/blackfin/kernel/kgdb_test.c:67: relocation truncated to fit: R_pcrel24 against symbol `printk' defined in .text section in kernel/built-in.o^M

arch/blackfin/kernel/kgdb_test.c:68: relocation truncated to fit: R_pcrel24 against symbol `printk' defined in .text section in kernel/built-in.o^M

arch/blackfin/kernel/kgdb_test.c:70: relocation truncated to fit: R_pcrel24_jump_l against symbol `printk' defined in .text section in kernel/built-in.o^M

make[1]: *** [.tmp_vmlinux1] Error 1^M

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

make: *** [linux] Error 1^M

--

Follow-ups

--- Sonic Zhang                                              2008-11-10 23:28:34

This is a duplicated bug of 4562.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.