Article [#4791] reserver memory on bf533 stamp fails

[#4791] reserver memory on bf533 stamp fails

Submitted By: Mingquan Pan

Open Date

2009-01-09 05:58:46     Close Date

2009-01-09 06:31:22

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

N/A     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

Nov 11

App binary format:

N/A     

Summary: reserver memory on bf533 stamp fails

Details:

reserver memory on bf533 stamp fails.

U-Boot 2008.10-svn1496 (ADI-2009R1-pre) (Dec  3 2008 - 12:16:52)

CPU:   ADSP bf533-0.3 (Detected Rev: 0.3)

Board: ADI BF533 Stamp board

       Support:   blackfin.uclinux.org/

Clock: VCO: 497.664 MHz, Core: 497.664 MHz, System: 99.532 MHz

RAM:   128 MB

Fl

RAM size is 128 MB.

ash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   MAC:   F2:06:01:61:68:B5

Hit any key to stop autoboot:  0

bfin> set bootargs root=/dev/mtdblock0 rw mem=32M max_mem=64M

bfin> set serverip 10.100.4.174

bfin> set ipaddr 10.100.4.50

bfin> save

Saving Environment to Flash...

Un-Protected 1 sectors

Erasing Flash...

. done

Erased 1 sectors

Writing to Flash... done

Protected 1 sectors

bfin> tftpboot 0x2000000 linux

Using MAC Address F2:06:01:61:68:B5

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'linux'.

Load address: 0x2000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #################################################################

         ##################

done

Bytes transferred = 5022453 (4ca2f5 hex)

Image size is 4ca2f5

bfin> run addip

bfin> bootelf

Loading phdr 0 to 0x00001000 (1414084 bytes)

Loading phdr 1 to 0x00168808 (3000008 bytes)

Loading phdr 2 to 0x00444ed0 (6692 bytes)

Loading phdr 3 to 0x004468f4 (192 bytes)

## Starting application at 0x00183180 ...

Linux version 2.6.28-rc2-ADI-2009R1-pre-svn5955 (test@uclinux75-bf533-stamp-wb) (gcc version 4.1.2 (ADI svn)) #65 Fri Jan 9 05:22:52 CST 2009

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 128MB

Kernel Managed Memory: 128MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010af30

  rodata    = 0x0010af30-0x0015a3c4

  bss       = 0x0015a3d0-0x00168808

  data      = 0x00168808-0x00178000

    stack   = 0x00176000-0x00178000

  init      = 0x00178000-0x00447000

  available = 0x00447000-0x037ff000

  DMA Zone  = 0x07f00000-0x08000000

Hardware Trace Active and Enabled

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 497 MHz core clock and 99 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line:

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

bfin-rtc: invalid date; resetting

console [ttyBF0] enabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 52380k/131072k RAM, (2876k init code, 1063k kernel code, 437k data, 1024k dma, 73292k reserved)

Calibrating delay loop... 991.23 BogoMIPS (lpj=1982464)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (57 KB free)

PDA for CPU0 reserved at 0015b0bc

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 102

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 20300300 IRQ 40 [nowait]

eth0: Ethernet addr: f2:06:01:61:68:b5

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 18:08:37 UTC (65317)

Freeing unused kernel memory: 2876k freed

dma_alloc_init: dma_page @ 0x00444000 - 256 pages at 0x07f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.13.2 (2009-01-08 17:34:37 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/>

************** STEP 3: Starting test.

cat /proc/meminfo

MemTotal:          55256 kB

Mem

Case 1 ...PASS

Case 2 ...FAIL

Follow-ups

--- Mingquan Pan                                             2009-01-09 06:31:22

Sorry, this is because the parameters are not passed in. It is ok by using

uImage. Close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.