Article [#4811] serial uart 1 case send data from host to target frequently see diffs

[#4811] serial uart 1 case send data from host to target frequently see diffs

Submitted By: Mingquan Pan

Open Date

2009-01-16 01:30:16     Close Date

2009-03-03 03:24:03

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

EZKIT Lite

Processor:

BF548     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

Dec 12

App binary format:

N/A     

Summary: serial uart 1 case send data from host to target frequently see diffs

Details:

serial uart 1 case send data from host to target frequently see diffs.

bfin> bootm

## Booting image at 02000000 ...

   Image Name:   Linux-2.6.28-ADI-2009R1-pre-svn5

   Created:      2009-01-12  14:44:09 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4762634 Bytes =  4.5 MB

   Load Address: 00001000

   Entry Point:  002795c8

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 2795c8

Linux version 2.6.28-ADI-2009R1-pre-svn5994 (test@uclinux61-bf548-std) (gcc version 4.1.2 (ADI svn)) #12 Mon Jan 12 14:43:52 GMT 2009

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001aab00

  rodata    = 0x001aab00-0x00239bd4

  bss       = 0x00239be0-0x0024bc7c

  data      = 0x0024bc7c-0x00264000

    stack   = 0x00262000-0x00264000

  init      = 0x00264000-0x00907000

  available = 0x00907000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 3

Reset caused by Software reset

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF548 Rev 0.1

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15747

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 ip=10.100.4.50 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf548-ezkit:eth0:off

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 53660k/65536k RAM, (6796k init code, 1702k kernel code, 742k data, 2048k dma, 584k reserved)

Calibrating delay loop... 1044.48 BogoMIPS (lpj=2088960)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

Blackfin L2 SRAM: 128 KB (128 KB free)

PDA for CPU0 reserved at 0023b498

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, musb-dma, host, debug=0

musb_hdrc: USB Host mode controller at ffc03c00 using DMA, IRQ 82

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

dma_alloc_init: dma_page @ 0x009a3000 - 512 pages at 0x03e00000

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 104

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bf54x-lq043: FrameBuffer initializing...

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 48) is a BFIN-UART

bfin-uart.1: ttyBF1 at MMIO 0xffc03100 (irq = 42) is a BFIN-UART

brd: module loaded

smsc911x: Driver version 2007-07-13.

eth0: SMSC911x MAC Address: 00:e0:22:fe:b8:54

Driver 'sd' needs updating - please use bus_type methods

Driver 'sr' needs updating - please use bus_type methods

register bfin atapi driver

scsi0 : pata-bf54x

ata1: PATA max UDMA/66 irq 68

ata1.00: ATA-6: TOSHIBA MK4032GAX, AD101A, max UDMA/100

ata1.00: 78140160 sectors, multi 16: LBA48

ata1.00: configured for UDMA/66

blk_queue_max_hw_segments: set to minimum 1

scsi 0:0:0:0: Direct-Access     ATA      TOSHIBA MK4032GA AD10 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 78140160 512-byte hardware sectors: (40.0 GB/37.2 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sd 0:0:0:0: [sda] 78140160 512-byte hardware sectors: (40.0 GB/37.2 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sda: sda1 sda2

sd 0:0:0:0: [sda] Attached SCSI disk

physmap platform flash device: 02000000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Using buffer write method

Using auto-unlock on power-up/resume

cfi_cmdset_0001: Erase suspend on write enabled

RedBoot partition parsing not available

Using physmap partition information

Creating 3 MTD partitions on "physmap-flash.0":

0x00000000-0x00040000 : "bootloader(nor)"

0x00040000-0x00440000 : "linux kernel(nor)"

0x00440000-0x01000000 : "file system(nor)"

BF5xx on-chip NAND FLash Controller Driver, Version 1.2 (c) 2007 Analog Devices, Inc.

bf5xx-nand bf5xx-nand.0: page_size=256, data_width=8, wr_dly=3, rd_dly=3

NAND device: Manufacturer ID: 0x20, Chip ID: 0xda (ST Micro NAND 256MiB 3,3V 8-bit)

Creating 2 MTD partitions on "NAND 256MiB 3,3V 8-bit":

0x00000000-0x00400000 : "linux kernel(nand)"

0x00400000-0x10000000 : "file system(nand)"

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader(spi)"

0x00040000-0x00200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@4

bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc02300, dma channel@5

input: bf54x-keys as /devices/platform/bf54x-keys/input/input0

bf54x-keys: Blackfin BF54x Keypad registered IRQ 76

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc00700

i2c-bfin-twi i2c-bfin-twi.1: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc02200

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

hid_zpff: Unknown symbol _input_ff_create_memless

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

ASoC version 0.13.2

dma rx:0 tx:1, err irq:10, regs:ffc00800

AD1980 SoC Audio Codec

asoc: AC97 <-> bf5xx-ac97 mapping ok

ALSA device list:

  #0: bf5xx-board (AD1980)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-06-01 04:22:33 UTC (1086063753)

usb 1-1: new high speed USB device using musb_hdrc and address 2

usb 1-1: configuration #1 chosen from 1 choice

eth0: SMSC911x/921x identified at 0x24000000, IRQ: 175

eth0: link down

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf548-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 6796k freed

eth0: link up, 100Mbps, full-duplex, lpa 0x41E1

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.13.2 (2009-01-12 14:41:54 GMT) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/>

Starting test for Serial UART 1...

su ******************************

test@uclinux61-bf548-std:~/work/cruise/checkouts/uclinux-dist/testsuites/serial> su

Password:

uclinux61-bf548-std:/home/test/work/cruise/checkouts/uclinux-dist/testsuites/serial #

Case 1 ...PASS

Case 1 ...PASS

rmmod pl2303

uclinux61-bf548-std:/home/test/work/cruise/checkouts/uclinux-dist/testsuites/serial #

Case 2 ...PASS

Case 2 ...PASS

modprobe pl2303

uclinux61-bf548-std:/home/test/work/cruise/checkouts/uclinux-dist/testsuites/serial #

Case 3 ...PASS

Case 3 ...PASS

root:/> cat /proc/kallsyms > ccc

root:/> stty -F /dev/ttyBF1 ispeed 57600 ospeed 57600 -icrnl igncr

root:/> cat /dev/ttyBF1 > aaa

test@uclinux61-bf548-std:~/work/cruise/checkouts/uclinux-dist/testsuites/serial> rcp root@10.100.4.50:/ccc .

test@uclinux61-bf548-std:~/work/cruise/checkouts/uclinux-dist/testsuites/serial> stty -F /dev/ttyUSB0 ispeed 57600 ospeed 57600 -icrnl -ixon igncr -opost -onlcr -isig -icanon -iexten -echo -echoe -echok -echoke -hupcl -echoctl

test@uclinux61-bf548-std:~/work/cruise/checkouts/uclinux-dist/testsuites/serial>  cat ccc > /dev/ttyUSB0

test@uclinux61-bf548-std:~/work/cruise/checkouts/uclinux-dist/testsuites/serial> ^C

root:/>

root:/> Catted file is got on target.

diff -u ccc aaa

--- ccc Tue Jun  1 04:22:39 2004

+++ aaa Tue Jun  1 04:24:08 2004

@@ -1,6 +1,3 @@

-00001000 T _do_one_initcall

-00001000 T __stext

-00001000 T _text

00001000 T __text

00001168 t _run_init_process

00001180 t _init_post

root:/>

Two files diffs.

Case 4 ...FAIL

Case 4 ...FAIL

Follow-ups

--- Sonic Zhang                                              2009-02-05 22:50:54

test script should add flags "min 1 time 0" to tty device.

--- Mingquan Pan                                             2009-02-11 01:52:38

It still sees the diff by add "min 1 time 0".

## Booting image at 02000000 ...

   Image Name:   Linux-2.6.28.3-ADI-2009R1-pre-sv

   Created:      2009-02-08   0:28:48 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4046779 Bytes =  3.9 MB

   Load Address: 00001000

   Entry Point:  0018a35c

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 18a35c

Linux version 2.6.28.3-ADI-2009R1-pre-svn6073

(test@uclinux50-bf537-ad9960-ad1836) (gcc version 4.1.2 (ADI svn)) #12 Sun Feb 8

08:28:26 CST 2009

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Warning: limiting memory to 56MB due to hardware anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0010a310

  rodata    = 0x0010a310-0x0015c564

  bss       = 0x0015c570-0x0016b01c

  data      = 0x0016b01c-0x0017c000

    stack   = 0x0017a000-0x0017c000

  init      = 0x0017c000-0x007a0000

  available = 0x007a0000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

ip=10.100.4.50

ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:1:eth0:off

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 48952k/65536k RAM, (6288k init code, 1060k kernel code, 456k

data, 1024k dma, 7756k reserved)

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)

PDA for CPU0 reserved at 0015d658

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

stamp_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 95

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 20) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1,

mdc_clk=2500000Hz(mdc_div=19)@sclk=100MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1971-04-28 20:14:23 UTC (41717663)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=1, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 6288k freed

dma_alloc_init: dma_page @ 0x0079c000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            -   blackfin.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.13.2 (2009-02-08 08:24:14 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/>

Starting test for Serial UART 1...

spawn /bin/bash******************

su

test@uclinux50-bf537-ad9960-ad1836:~/work/cruise/checkouts/uclinux-dist/testsuites/serial>

su

Password:

uclinux50-bf537-ad9960-ad1836:/home/test/work/cruise/checkouts/uclinux-dist/testsuites/serial

#

Case 1 ...PASS

Case 1 ...PASS

rmmod pl2303

uclinux50-bf537-ad9960-ad1836:/home/test/work/cruise/checkouts/uclinux-dist/testsuites/serial

#

Case 2 ...PASS

Case 2 ...PASS

modprobe pl2303

uclinux50-bf537-ad9960-ad1836:/home/test/work/cruise/checkouts/uclinux-dist/testsuites/serial

#

Case 3 ...PASS

Case 3 ...PASS

PHY: 0:01 - Link is Up - 100/Full

root:/> cat /proc/kallsyms > ccc

root:/> stty -F /dev/ttyBF1 ispeed 57600 ospeed 57600 -icrnl igncr min 1

time 0

root:/> cat /dev/ttyBF1 > aaa

spawn /bin/sh

uclinux50-bf537-ad9960-ad1836:~/work/cruise/checkouts/uclinux-dist/testsuites/serial>

rcp root@10.100.4.50:/ccc .

uclinux50-bf537-ad9960-ad1836:~/work/cruise/checkouts/uclinux-dist/testsuites/serial>

stty -F /dev/ttyUSB0 ispeed 57600 ospeed 57600 -icrnl -ixon igncr -opost -onlcr

-isig -icanon -iexten -echo -echoe -echok -echoke -hupcl -echoctl min 1 time 0

uclinux50-bf537-ad9960-ad1836:~/work/cruise/checkouts/uclinux-dist/testsuites/serial>

cat ccc > /dev/ttyUSB0

uclinux50-bf537-ad9960-ad1836:~/work/cruise/checkouts/uclinux-dist/testsuites/serial>

^C

root:/>

root:/> Catted file is got on target.

diff -u ccc aaa

--- ccc Wed Apr 28 20:14:31 1971

+++ aaa Wed Apr 28 20:15:47 1971

@@ -1,6 +1,3 @@

-00001000 T _do_one_initcall

-00001000 T __stext

-00001000 T _text

00001000 T __text

00001164 t _run_init_process

0000117c t _init_post

root:/>

Two files diffs.

Case 4 ...FAIL

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.