Article [#4824] AD1980 AC97 reset failed in BF527-EZKIT

[#4824] AD1980 AC97 reset failed in BF527-EZKIT

Submitted By: Vivi Li

Open Date

2009-01-20 05:15:05     Close Date

2009-02-04 05:43:03

Priority:

Medium     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

EZKIT Lite

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Not reproducible

Uboot version or rev.:

    Toolchain version or rev.:

toolchain 4.1-2008_Dec_12

App binary format:

N/A     

Summary: AD1980 AC97 reset failed in BF527-EZKIT

Details:

AD1980 AC97 reset failed in BF527-EZKIT.

--

Linux version 2.6.28-ADI-2009R1-pre-svn6027 (test@uboot30-527ezkit) (gcc version 4.1.2 (ADI svn)) #9

console [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00139750

  rodata    = 0x00139750-0x0019a1f4

  bss       = 0x0019a200-0x001a986c

  data      = 0x001a986c-0x001bc000

    stack   = 0x001ba000-0x001bc000

  init      = 0x001bc000-0x007b8000

  available = 0x007b8000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 9

Blackfin support (C) 2004-2008 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.0

Blackfin Linux support by   blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15747

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 consolf

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console handover: boot [early_BFuart0] -> real [ttyBF0]

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 55000k/65536k RAM, (6128k init code, 1249k kernel code, 523k data, 2048k dma, 584)

Calibrating delay loop... 1044.48 BogoMIPS (lpj=2088960)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

PDA for CPU0 reserved at 0019b130

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin GPIO Controller

Blackfin DMA Controller

ezkit_init(): registering device resources

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

musb_hdrc: version 6.0, pio, host, debug=0

musb_hdrc: USB Host mode controller at ffc03800 using PIO, IRQ 59

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

usb usb1: configuration #1 chosen from 1 choice

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 107

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-otp: initialized

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

bfin_mac_mdio: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1, mdc_clk=2500000Hz(mdc_d)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x00000000-0x00040000 : "bootloader(spi)"

0x00040000-0x00200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma c7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

hid_tmff: Unknown symbol _input_ff_create_memless

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.18rc3.

ASoC version 0.13.2

dma rx:3 tx:4, err irq:15, regs:ffc00800

AD1980 SoC Audio Codec

dma_alloc_init: dma_page @ 0x03a9a000 - 512 pages at 0x03e00000

asoc: AC97 <-> bf5xx-ac97 mapping ok

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

bf5xx_ac97_cold_reset: Not implemented

AD1980 AC97 reset failed

AC97 link error

soc-audio: probe of soc-audio failed with error -5

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1974-09-17 23:56:30 UTC (148694190)

IP-Config: Gateway not on directly connected network.

Freeing unused kernel memory: 6128k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

kf 8a.   :     _a88P         For further infPHmatY: 0 ch:03 out- Lin_/"k i_: s Up 8 P|-      1   0-l

  n.uclinux.org/

\    YP"    `| 8P  `.          -   docs.blackfin.uclinux.org/

/     \.___.d|    .'           -   www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    -   www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.13.2 (2009-01-20 15:36:30 GMT) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/>

--

Follow-ups

--- Cliff Cai                                                2009-01-21 02:46:09

It should be OK.Actually,the interface labled "sport0" is sport0A,

So,you should select PORTG for sport0A,and turn sw17 sw20 all off.

Cliff

--- Vivi Li                                                  2009-02-04 05:43:03

OK now. Close it.

Thanks!

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.