Article [#4945] verify spidev works with multiple devices/cs

[#4945] verify spidev works with multiple devices/cs

Submitted By: Mike Frysinger

Open Date

2009-02-26 13:36:42     Close Date

2009-12-04 01:07:49

Priority:

Medium     Assignee:

Yi Li

Status:

Closed     Fixed In Release:

N/A

Found In Release:

snaps     Release:

Category:

Drivers     Board:

STAMP

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Out of Date

Uboot version or rev.:

    Toolchain version or rev.:

trunk

App binary format:

N/A     

Summary: verify spidev works with multiple devices/cs

Details:

there is a report here:

  blackfin.uclinux.org/gf/project/uclinux-dist/forum/?action=ForumBrowse&_forum_action=MessageReply&message_id=70026

attempting to use spidev with cs 1 and cs 5 results in only one working

we need to verify that writing to one at a time works and that writing to both works (in other words, write a few bytes to cs1, then a few to cs5, then a few to cs1, etc...)

Follow-ups

--- Yi Li                                                    2009-03-27 04:57:46

Do we need to connect real spi devices to reproduce?

If yes, we do not have proper hardware to connect multiple spi devices on a spi

bus. I used to use BF537-STAMP + spi-mmc + ad1836 to test multiple devices. But

this is not enough for this case.

--- Mike Frysinger                                           2009-03-27 12:19:56

the ad1836 only uses SPI for register setup i thought, not normal playing.  so

unless your test was more about constantly changing mixer settings than playing

audio, that test might not be so useful.

however, since SPI can be wiggled by the master only without any slave devices

hooked up, i would put a scope on the CS pins and write a test app that simply

writes bytes back and worth between multiple spidev's and make sure that the

CS's do not mix.

--- Yi Li                                                    2009-04-14 03:34:32

This bug does not exist in svn trunk. I tested using svn-6626 linux-kernel,

using the "spidev_test" program, on BF537-STAMP.

I connect SPI_SSEL1 and SPI_SSEL5 to scope. When running:

root:/> spidev_test -D /dev/spidev0.5

spi mode: 0

bits per word: 8

max speed: 500000 Hz (500 KHz)

FF FF FF FF FF FF

FF FF FF FF FF FF

FF FF FF FF FF FF

FF FF FF FF FF FF

FF FF FF FF FF FF

FF FF FF FF FF FF

FF FF

Only SPI_SSEL5 pulls down. And when running:

root:/> spidev_test -D /dev/spidev0.1

Only SPI_SSEL1 pulls down.

The CS work as expected.

--- Mike Frysinger                                           2009-04-14 03:43:02

and it works if you run them at the same time ?

spidev_test -D /dev/spidev0.5 &

spidev_test -D /dev/spidev0.1 &

--- Yi Li                                                    2009-04-14 03:48:14

Attached the scope image when running "root:/> spidev_test -D

/dev/spidev0.5

". ch1 is spi_sck, ch2 is spi_sse11, ch3 is spi_ssel5.

--- Yi Li                                                    2009-04-14 05:49:12

I modified spitest.c as this:

Index: Documentation/spi/spidev_test.c

===================================================================

--- Documentation/spi/spidev_test.c    (revision 6266)

+++ Documentation/spi/spidev_test.c    (working copy)

@@ -150,6 +150,7 @@ int main(int argc, char *argv[])

{

     int ret = 0;

     int fd;

+    int i = 0;

     parse_opts(argc, argv);

@@ -194,7 +195,8 @@ int main(int argc, char *argv[])

     printf("bits per word: %d\n", bits);

     printf("max speed: %d Hz (%d KHz)\n", speed, speed/1000);

-    transfer(fd);

+    for (i = 0; i < 1024; i++)

+        transfer(fd);

     close(fd);

Then run:

spidev_test -D /dev/spidev0.1 > /dev/null &

spidev_test -D /dev/spidev0.5 > /dev/null

It works as expected (as far as I can see fromt the scope). see attached

spidev2.png.

--- Yi Li                                                    2009-04-14 05:52:45

Comparing spidev.png and spidev2.png, Ch2 is a little different. I am not clear

about the reason.

--- Mike Frysinger                                           2009-04-14 06:21:17

is it floating ?  if it floats too high, that'd be the same thing as asserting

the CS ...

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

spidev.png    image/png    16583    Yi Li

spidev2.png    image/png    18578    Yi Li

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.