Article [#5101] Random hang when repeating test hardware error trap

[#5101] Random hang when repeating test hardware error trap

Submitted By: Graf Yang

Open Date

2009-04-29 01:54:12     Close Date

2009-05-04 23:22:07

Priority:

Medium     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Kernel Functions     Board:

N/A

Processor:

BF533     Silicon Revision:

0.4

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

2009R1-rc5

App binary format:

FDPIC     

Summary: Random hang when repeating test hardware error trap

Details:

system will random hang when repeating test the hardware error, may hang on the 8th, or the 19th.

It existed on 0.3 533(when doing hardware error testing), and 0.2 537(when doing dcplb miss testing). It is frequently on 0.4 533.

root:/> traps_test 18                                                      

                                                                      

RuEnxng test ternal Memory Addressing Error                                   

HW Error context                                                              

CURRENT PROCESS:                                                              

COMM=traps_test1 PID=142                                                      

CPU = 0                                                                       

TEXT = 0x00366000-0x003677ec        DATA = 0x003627ec-0x003631e8              

BSS = 0x003631e8-0x00340000  USER-STACK = 0x0035fea0                         

                                                                              

return address: [0x00366fdc]; contents of:                                    

0x00366fb0:  bbf0  b9f0  6408  bbe0  b9ea  9151  ac53  0061                   

0x00366fc0:  e801  0000  0010  0000  e800  0005�

(here the system hang, watchdog seems can't reboot it)

Follow-ups

--- Graf Yang                                                2009-05-04 06:11:59

This bug is caused by watchdog fail.

When watchdog time out, the board hang there, not reset.

--- Mike Frysinger                                           2009-05-04 13:17:08

not a bug then ...

--- Graf Yang                                                2009-05-04 21:57:25

Is it a bootrom bug? I can not find it in anomaly list.

--- Mike Frysinger                                           2009-05-04 22:08:36

the bootrom is not executed at all on the BF533 in bypass mode

the Blackfin system is known to not be recoverable under some circumstances and

i imagine this is one of them (e.g. CFI flash is put into some intermediate mode

where reading is not possible, and then a reset occurs)

--- Sonic Zhang                                              2009-05-04 22:50:56

Is it better to turn of watchdog when running trap test?

--- Mike Frysinger                                           2009-05-04 22:58:53

no ... Graf's test case is running traps over and over in a tight loop.  that

doesnt occur in the normal test case that gets run on the test bench.

it is also triggering a bug in our hardware handling code that Robin is working

on fixing, so once that gets resolved, it should be much less of an issue.

--- Graf Yang                                                2009-05-04 23:22:07

It is not a bug, I will close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.