Article [#5126] Build sqlite fails at trunk for dlfcn.h when built as FLAT

[#5126] Build sqlite fails at trunk for dlfcn.h when built as FLAT

Submitted By: Vivi Li

Open Date

2009-05-14 06:29:45     Close Date

2009-05-15 02:01:43

Priority:

Medium     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Make Errors     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1_rc6

App binary format:

N/A     

Summary: Build sqlite fails at trunk for dlfcn.h when built as FLAT

Details:

Build sqlite fails at trunk for dlfcn.h.

Bellow is the log and config file is attached.

--

bfin-uclinux-gcc -DPACKAGE_NAME=\"sqlite\" -DPACKAGE_TARNAME=\"sqlite\" -DPACKAGE_VERSION=\"3.6.14\" -DPACKAGE_STRING=\"sqlite\ 3.6.14\" -DPACKAGE_BUGREPORT=\"http://www.sqlite.org\" -DPACKAGE=\"sqlite\" -DVERSION=\"3.6.14\" -D_FILE_OFFSET_BITS=64 -DSTDC_HEADERS=1 -DHAVE_SYS_TYPES_H=1 -DHAVE_SYS_STAT_H=1 -DHAVE_STDLIB_H=1 -DHAVE_STRING_H=1 -DHAVE_MEMORY_H=1 -DHAVE_STRINGS_H=1 -DHAVE_INTTYPES_H=1 -DHAVE_STDINT_H=1 -DHAVE_UNISTD_H=1 -DHAVE_FDATASYNC=1 -DHAVE_USLEEP=1 -DHAVE_LOCALTIME_R=1 -DHAVE_GMTIME_R=1 -I. -I../sqlite-3.6.14   -DEMBED -D__uClinux__ -I/home/test/work/cruise/checkouts/uclinux-dist  -mcpu=bf537-0.2 -DSQLITE_THREADSAFE=1  -pipe -Wall -g -O2      -mcpu=bf537-0.2 -c ../sqlite-3.6.14/shell.c^M

bfin-uclinux-gcc -DPACKAGE_NAME=\"sqlite\" -DPACKAGE_TARNAME=\"sqlite\" -DPACKAGE_VERSION=\"3.6.14\" "-DPACKAGE_STRING=\"sqlite 3.6.14\"" -DPACKAGE_BUGREPORT=\"http://www.sqlite.org\" -DPACKAGE=\"sqlite\" -DVERSION=\"3.6.14\" -D_FILE_OFFSET_BITS=64 -DSTDC_HEADERS=1 -DHAVE_SYS_TYPES_H=1 -DHAVE_SYS_STAT_H=1 -DHAVE_STDLIB_H=1 -DHAVE_STRING_H=1 -DHAVE_MEMORY_H=1 -DHAVE_STRINGS_H=1 -DHAVE_INTTYPES_H=1 -DHAVE_STDINT_H=1 -DHAVE_UNISTD_H=1 -DHAVE_FDATASYNC=1 -DHAVE_USLEEP=1 -DHAVE_LOCALTIME_R=1 -DHAVE_GMTIME_R=1 -I. -I../sqlite-3.6.14 -DEMBED -D__uClinux__ -I/home/test/work/cruise/checkouts/uclinux-dist -mcpu=bf537-0.2 -DSQLITE_THREADSAFE=1 -pipe -Wall -g -O2 -mcpu=bf537-0.2 -c ../sqlite-3.6.14/sqlite3.c -o sqlite3.o^M

../sqlite-3.6.14/sqlite3.c:24771:19: error: dlfcn.h: No such file or directory^M

../sqlite-3.6.14/sqlite3.c: In function 'unixDlOpen':^M

../sqlite-3.6.14/sqlite3.c:24774: warning: implicit declaration of function 'dlopen'^M

../sqlite-3.6.14/sqlite3.c:24774: error: 'RTLD_NOW' undeclared (first use in this function)^M

../sqlite-3.6.14/sqlite3.c:24774: error: (Each undeclared identifier is reported only once^M

../sqlite-3.6.14/sqlite3.c:24774: error: for each function it appears in.)^M

../sqlite-3.6.14/sqlite3.c:24774: error: 'RTLD_GLOBAL' undeclared (first use in this function)^M

../sqlite-3.6.14/sqlite3.c:24774: warning: return makes pointer from integer without a cast^M

../sqlite-3.6.14/sqlite3.c: In function 'unixDlError':^M

../sqlite-3.6.14/sqlite3.c:24788: warning: implicit declaration of function 'dlerror'^M

../sqlite-3.6.14/sqlite3.c:24788: warning: assignment makes pointer from integer without a cast^M

../sqlite-3.6.14/sqlite3.c: In function 'unixDlSym':^M

../sqlite-3.6.14/sqlite3.c:24814: error: 'dlsym' undeclared (first use in this function)^M

../sqlite-3.6.14/sqlite3.c: In function 'unixDlClose':^M

../sqlite-3.6.14/sqlite3.c:24819: warning: implicit declaration of function 'dlclose'^M

make[4]: *** [sqlite3.lo] Error 1^M

make[4]: *** Waiting for unfinished jobs....^M

make[4]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/lib/sqlite/build-sqlite-3.6.14'^M

make[3]: *** [all] Error 2^M

make[3]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/lib/sqlite'^M

--

Follow-ups

--- Mike Frysinger                                           2009-05-14 07:21:56

the newer sqlite defaults to loadable extensions without any checks.  fixed

configure logic in trunk.

--- Vivi Li                                                  2009-05-15 02:01:43

OK now. Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.sqlite    application/octet-stream    32637    Vivi Li

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.