Article [#5190] [ltp] sysctl01, sysctl03, sysctl04 fail since 2009.4.1

[#5190] [ltp] sysctl01, sysctl03, sysctl04 fail since 2009.4.1

Submitted By: Sonic Zhang

Open Date

2009-06-02 04:20:52     Close Date

2009-06-04 04:14:33

Priority:

Medium     Assignee:

Vivi Li

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

09-r1

App binary format:

N/A     

Summary: [ltp] sysctl01, sysctl03, sysctl04 fail since 2009.4.1

Details:

ltp test case sysctl01, sysctl03, sysctl04 fail since 2009.4.1

************** STEP 2906: Start to test [sysctl01]

************** STEP 2907: get test case [sysctl01] from server

^M

root:/bin>

************** STEP 2908: execute [sysctl01] ...

sysctl01^M

warning: process `sysctl01' used the deprecated sysctl system call with 1.1.^M

swsctl01    1  FAIL  :  sysctl(2) failed u

---fail

nexpectedly errno:38arning: process `sysctl01' used the deprecated sysctl system call with ^M

1.2.^M

sysctl01    2  FAIL  :  sysctl(2) fai

---fail

led unexpectedly errno:38^M

sysctl01    3  FAIL  :  sysctl(2) failed unex

---fail

pectedly errno:38^M

root:/bin>

---done

************** STEP 2909: goto test_cleanup

sending marker

echo 1239258967^M

got marker back

1239258967^M

root:/bin>

got marker back

got kernel prompt

************** STEP 2910: remove testcase done

rm -f /bin/sysctl01^M

root:/bin> ^M

root:/bin>

System is fine.

===== Recording result: sysctl01 is FAIL

Follow-ups

--- Mike Frysinger                                           2009-06-02 04:24:12

we disable sysctl in our defconfigs on purpose:

# CONFIG_SYSCTL_SYSCALL is not set

this isnt a function should care about ...

--- Sonic Zhang                                              2009-06-03 06:00:56

Vivi should disable sysctl test cases in LTP since we don't support

CONFIG_SYSCTL_SYSCALL in kernel by default.

--- Vivi Li                                                  2009-06-04 04:14:33

OK, disable sysctl test.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.