Article [#5216] fail to read/write SATA hard disk connected to bf537 IDE daughter board via SATA/IDE converter

[#5216] fail to read/write SATA hard disk connected to bf537 IDE daughter board via SATA/IDE converter

Submitted By: Barry Song

Open Date

2009-06-08 04:23:31     Close Date

2009-07-24 01:26:35

Priority:

Medium     Assignee:

Barry Song

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

2009R1_RC6

App binary format:

N/A     

Summary: fail to read/write SATA hard disk connected to bf537 IDE daughter board via SATA/IDE converter

Details:

Test board: BF537-STAMP; cf/ide-ata/nand EXTENDER board; SATA/IDE converter board

Kernel codes:Trunk head

ATA can work, but SATA can't work.

This bug is reported from customer.

1. SATA device can be found while system start-up:

scsi0 : pata_platform

ata1: PATA max PIO0 mmio cmd 0x20314020 ctl 0x2031401c irq 55

ata1.00: qc timeout (cmd 0x27)

ata1.00: failed to read default max address (err_mask=0x4)

ata1.00: HPA support seems broken, skipping HPA handling

ata1.00: configured for PIO

scsi 0:0:0:0: Direct-Access     ATA      Hitachi HTS54161 SB4O PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 312581808 512-byte hardware sectors: (160 GB/149 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sd 0:0:0:0: [sda] 312581808 512-byte hardware sectors: (160 GB/149 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

2. when reading /dev/sda by fdisk/cat etc commands, kernel will give the following log:

root:/> fdisk /dev/sda

irq 55: nobody cared (try booting with the "irqpoll" option)

Hardware Trace:

   0 Target : <0x00004b20> { _dump_stack + 0x0 }

     Source : <0x0002e2e4> { ___report_bad_irq + 0x1c } CALL pcrel

   1 Target : <0x0002e2e4> { ___report_bad_irq + 0x1c }

     Source : <0x0002e340> { ___report_bad_irq + 0x78 } JUMP.S

   2 Target : <0x0002e340> { ___report_bad_irq + 0x78 }

     Source : <0x00010d1a> { _printk + 0x16 } RTS

   3 Target : <0x00010d16> { _printk + 0x12 }

     Source : <0x0001154c> { _vprintk + 0x128 } RTS

   4 Target : <0x00011540> { _vprintk + 0x11c }

     Source : <0x00011532> { _vprintk + 0x10e } IF !CC JUMP

   5 Target : <0x0001152a> { _vprintk + 0x106 }

     Source : <0x00011664> { _vprintk + 0x240 } JUMP.S

   6 Target : <0x00011664> { _vprintk + 0x240 }

     Source : <0x00010b3e> { _wake_up_klogd + 0x1a } RTS

   7 Target : <0x00010b24> { _wake_up_klogd + 0x0 }

     Source : <0x00010ff8> { _release_console_sem + 0xb4 } JUMP.L

   8 Target : <0x00010ff2> { _release_console_sem + 0xae }

     Source : <0x00010fd8> { _release_console_sem + 0x94 } IF !CC JUMP

   9 Target : <0x00010fce> { _release_console_sem + 0x8a }

     Source : <0x000242ce> { _up + 0x3e } RTS

  10 Target : <0x000242c8> { _up + 0x38 }

     Source : <0x000242ba> { _up + 0x2a } IF !CC JUMP

  11 Target : <0x00024290> { _up + 0x0 }

     Source : <0x00010fca> { _release_console_sem + 0x86 } CALL pcrel

  12 Target : <0x00010fb6> { _release_console_sem + 0x72 }

     Source : <0x00010f90> { _release_console_sem + 0x4c } IF !CC JUMP

  13 Target : <0x00010f7e> { _release_console_sem + 0x3a }

     Source : <0x00010fa6> { _release_console_sem + 0x62 } IF CC JUMP

  14 Target : <0x00010fa0> { _release_console_sem + 0x5c }

     Source : <0x00010a16> { __call_console_drivers + 0x7a } RTS

  15 Target : <0x00010a10> { __call_console_drivers + 0x74 }

     Source : <0x000109d2> { __call_console_drivers + 0x36 } IF !CC JUMP

Stack info:

SP: [0x00e29cd8] <0x00e29cd8> /* kernel dynamic memory */

FP: (0x00e29cf0)

Memory from 0x00e29cd0 to 00e2a000

00e29cd0: 00e29cd8  0000000a [00000001]<0002e2e8> 001db0e0  00000000  001cd270  00000037

00e29cf0:(00000000)<0002e3e4> 001db0e0  001d6c04  00000006  00000000 <0002ee74> 001db0e0

00e29d10: 00000000  00000037  00000000  00000006  0000001f <0009d086><00008f06> 001d09a0

00e29d30: 00e28000  00e29eb8  0000ffff  00000001 <000151d2><ffa00300> 00000022  00e29eb8

00e29d50: 0000ffff  00003004  0009cf1e  000d6c04 <ffa00bb2> ffc00014  00000002  00000000

00e29d70: 00000005  00000000  00000019  00014de8 <0000d010> 00000000  00000000  00f84000

00e29d90: 00a0ed5c  00014de8 <ffa0032e> 0000000c  02002000  0000a3ca  ffa017a8  0000a3b2

00e29db0: ffa017a8  00000000  00000000  0000f3bf  00000000  0014068f  00000000  00000000

00e29dd0: 00000000  001da1f0  001ce7bc  00000000  00000000  00000000  00000000  00000000

00e29df0: 00000000  00000000  00000000  00000000  00000000  ffffffff  ffffffff  00000000

00e29e10: 00000001  001d09a0  00e28000  001cd270  001d73b8  00000094  001c855c  00000002

00e29e30: 00000000  0000ffff  0000000a  00000000  00000100  00000100  0000ffff  0000ffff

00e29e50: 001c855c  00000006  00000000  00000000  00000000 <0002ec40> 001da564  00e29fa4

00e29e70:<ffa0032e> 001d09a0  00e1d828  00000000  00000006  00000000  0000ffff  00000001

00e29e90: 00000001  037e8bec  0001000c <ffa00bb2> ffc00014  03794000  00e1d834  037e8bc0

00e29eb0: 00e29edc <0000a1be> 000d4fa6  00008050  00000000  00000000  00f84000  00a0ed5c

00e29ed0: 000d4fa6 <000d5298> 00000006  02003004  000d4f44  ffa017a8  000d4f22  ffa017a8

00e29ef0: 00000020  00000000  00000904  00000000  003d08c7  00000000  00000000  00000000

00e29f10: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00e29f30: 00000000  00000000  00000000  00000000  00000000  000f4240  00000000  00e29fa4

00e29f50: 00e21940  00e1d828  00000000  001d73b8  001dfc0c  03794074  03794000  00e1d834

00e29f70: 0000ffff  00000001  00000000  00000000  0000003f  0000ffff  0000ffff  03794074

00e29f90: 00000006  00000000 <000bda5a> 00e28000  00e28000  00000000 <000bc714> 00e1d800

00e29fb0: 00000000  00000000  00e1d800  00000000  00000000  00000000  00e1d800  00e1d800

00e29fd0: 00000000 <0002090c> 000bc694  00000000  00000000  00000000 <00001466> 00000000

00e29ff0: 00000000  00000000  ffffffff  00000006  037861e0

Return addresses in stack:

    address : <0x0002e2e8> { ___report_bad_irq + 0x20 }

   frame  1 : <0x0002e3e4> { _note_interrupt + 0x84 }

    address : <0x0002ee74> { _handle_level_irq + 0x9c }

    address : <0x0009d086> { _number + 0x2a2 }

    address : <0x00008f06> { _bfin_demux_gpio_irq + 0x72 }

    address : <0x000151d2> { _irq_enter + 0xa }

    address : <0xffa00300> { _asm_do_IRQ + 0x34 }

    address : <0xffa00bb2> { __common_int_entry + 0x72 }

    address : <0x0000d010> { _sys_sched_getscheduler + 0x18 }

    address : <0xffa0032e> { _asm_do_IRQ + 0x62 }

    address : <0x0002ec40> { _handle_simple_irq + 0x74 }

    address : <0xffa0032e> { _asm_do_IRQ + 0x62 }

    address : <0xffa00bb2> { __common_int_entry + 0x72 }

    address : <0x0000a1be> { _enqueue_task + 0xe }

    address : <0x000d5298> { _ata_scsi_error + 0x3bc }

    address : <0x000bda5a> { _scsi_run_host_queues + 0xe }

    address : <0x000bc714> { _scsi_error_handler + 0x80 }

    address : <0x0002090c> { _kthread + 0x50 }

    address : <0x00001466> { _kernel_thread_helper + 0x6 }

handlers:

[<000d71a8>] (_ata_sff_interrupt+0x0/0x194)

Disabling IRQ #55

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:20:00:00:00/00:00:00:00:00/e0 tag 0 pio 16384 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: configured for PIO

ata1: EH complete

ata1.00: limiting speed to UDMA7:PIO5

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:20:00:00:00/00:00:00:00:00/e0 tag 0 pio 16384 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: configured for PIO

ata1: EH complete

ata1.00: limiting speed to PIO0

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:20:00:00:00/00:00:00:00:00/e0 tag 0 pio 16384 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: configured for PIO

ata1: EH complete

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:20:00:00:00/00:00:00:00:00/e0 tag 0 pio 16384 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: configured for PIO

ata1: EH complete

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:20:00:00:00/00:00:00:00:00/e0 tag 0 pio 16384 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: configured for PIO

ata1: EH complete

INFO: task ata_aux:79 blocked for more than 120 seconds.

"echo 0 > /proc/sys/kernel/hung_task_timeout_secs" disables this message.

ata_aux       D ffa00934     0    79      2

Stack info:

SP: [0x037abca0] <0x037abca0> /* kernel dynamic memory */

FP: (0x037abcbc)

Memory from 0x037abca0 to 037ac000

037abca0:[00e377e0] 037813a0  037d30a0  00e37ae0  001c852c  00000002  037aa000 (037abcd8)

037abcc0:<ffa01c46> 030deebc  ffffffff  037abd48  037aa000  037aa000 (037abd50)<ffa020bc>

037abce0: 037aa000  037aa000  037abde8  7fffffff  00000000  00000002  001d73b8  00000001

037abd00: 00df00c8 <000af594> 00000068  00000001  030deebc <000be65e> 00e1d000  00000001

037abd20:<ffa01e68> 037aa000  7fffffff  00000000  037abeac <00090c1e> 030deebc  00000001

037abd40: 037813a0  0000c09c  037abdec  037abdec (037abeac)<00090cb6> 030deebc  030deebc

037abd60: 00000000  00b426e0  037abde8  00000000  00df00c8  00080000  00000000  037abe5c

037abd80: 00000001  00090bac  00df00c8  00df00d8  00000001  00000000  00000000  00000004

037abda0: 001dde6d  00000000  00000010  00000000 <0008e964> 00df00c8  00e1d000  037abeac

037abdc0: 00000000  00000000  037abeb8  001dde6c  fffffffe  037abde4  00000010  001aa5c0

037abde0: 001e16cc  037f37a0  00000000  037abd48  037abd48 <000bdf08> 030deebc  00e1d000

037abe00: 037abeac  00000000  00000000  037abeb8  00000000  00000000  0000ffff  00000000

037abe20: 00000001  037abf34 <000bdfa4> 00001d4c  00000005  00e1d000  00b426e0  00000000

037abe40: 0000000d  037abe60  00b38c0c  00000000  00000000  00b426e0  00001d4c  00000005

037abe60: 00000000  00000000 <000c3830> 00e03200  037abeb8  00000000  00000000  00000000

037abe80: 0000ffff  00000000  00b38be0  037abeb8  00000003  00000000  00000000  037abeb8

037abea0: 00001d4c  00000005  00000000 (00000000) 00000000  00000000  00000000  037aa000

037abec0: 037aa000 <000c45bc> 00e03200  00e1d000  00dfde00  00b3b800  03795458  0000ffff

037abee0: 03794000 <000af594> 00000068 <0000b944> 001c855c <0005f668> 00dfde00  03795300

037abf00: 000d0db4  00e03200  001c852c <000c32a8> 00e1d0ac <000c3346> 001df490  00e03200

037abf20: 03795458  0000ffff  037abf54 <0000bb9c> 001c855c <000c022e> 00e1d000  00b38be0

037abf40: 001c852c  00000000 <000d0e48> 03795458  001d5d60  037abf7c <ffa01c54><0001d9a4>

037abf60: 03795d78  037b4d40  001d73b8  037aa000  037abfac  00000000  037aa000  00000000

037abf80:<0001e33a> 037aa000  00000000 <0001e314> 037aa000  037aa000  037b4d40  037b4d48

037abfa0: 001d5d60  00000000  00000000  00000000  037813a0  00020cc4  037abfb8  037abfb8

037abfc0:<0002090c> 0001e298  00000000  00000000  037b4d40  00000000  00000000  00000000

037abfe0: 00000000  00000000 <00001466> 00000000  00000000  00000000  ffffffff  00000006

037ac000: 4c412023

Return addresses in stack:

   frame  1 : <0xffa01c46> { _schedule + 0x182 }

   frame  2 : <0xffa020bc> { _schedule_timeout + 0x6c }

    address : <0x000af594> { _get_device + 0x14 }

    address : <0x000be65e> { _scsi_request_fn + 0x24e }

    address : <0xffa01e68> { _wait_for_common + 0x84 }

    address : <0x00090c1e> { _blk_execute_rq_nowait + 0x4a }

   frame  3 : <0x00090cb6> { _blk_execute_rq + 0x62 }

    address : <0x0008e964> { _get_request_wait + 0x18 }

    address : <0x000bdf08> { _scsi_execute + 0x98 }

    address : <0x000bdfa4> { _scsi_execute_req + 0x5c }

    address : <0x000c3830> { _sd_spinup_disk + 0x60 }

    address : <0x000c45bc> { _sd_revalidate_disk + 0x68 }

    address : <0x000af594> { _get_device + 0x14 }

    address : <0x0000b944> { _dequeue_entity + 0x2c }

    address : <0x0005f668> { _revalidate_disk + 0x14 }

    address : <0x000c32a8> { _scsi_disk_get_from_dev + 0x24 }

    address : <0x000c3346> { _sd_rescan + 0x1e }

    address : <0x0000bb9c> { _pick_next_task_fair + 0x2c }

    address : <0x000c022e> { _scsi_rescan_device + 0x4a }

    address : <0x000d0e48> { _ata_scsi_dev_rescan + 0x94 }

    address : <0xffa01c54> { _schedule + 0x190 }

    address : <0x0001d9a4> { _run_workqueue + 0x7c }

    address : <0x0001e33a> { _worker_thread + 0xa2 }

    address : <0x0001e314> { _worker_thread + 0x7c }

    address : <0x0002090c> { _kthread + 0x50 }

    address : <0x00001466> { _kernel_thread_helper + 0x6 }

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:20:00:00:00/00:00:00:00:00/e0 tag 0 pio 16384 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: configured for PIO

sd 0:0:0:0: [sda] Result: hostbyte=0x00 driverbyte=0x08

sd 0:0:0:0: [sda] Sense Key : 0xb [current] [descriptor]

Descriptor sense data with sense descriptors (in hex):

        72 0b 00 00 00 00 00 0c 00 0a 80 00 00 00 00 00

        00 00 00 00

sd 0:0:0:0: [sda] ASC=0x0 ASCQ=0x0

end_request: I/O error, dev sda, sector 0

Buffer I/O error on device sda, logical block 0

Buffer I/O error on device sda, logical block 1

Buffer I/O error on device sda, logical block 2

Buffer I/O error on device sda, logical block 3

ata1: EH complete

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:08:00:00:00/00:00:00:00:00/e0 tag 0 pio 4096 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: configured for PIO

ata1: EH complete

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:08:00:00:00/00:00:00:00:00/e0 tag 0 pio 4096 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: failed to IDENTIFY (I/O error, err_mask=0x1)

ata1.00: revalidation failed (errno=-5)

ata1: soft resetting link

ata1.00: configured for PIO

ata1: EH complete

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:08:00:00:00/00:00:00:00:00/e0 tag 0 pio 4096 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: failed to IDENTIFY (I/O error, err_mask=0x1)

ata1.00: revalidation failed (errno=-5)

ata1: soft resetting link

ata1.00: configured for PIO

ata1: EH complete

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:08:00:00:00/00:00:00:00:00/e0 tag 0 pio 4096 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: failed to IDENTIFY (I/O error, err_mask=0x1)

ata1.00: revalidation failed (errno=-5)

ata1: soft resetting link

ata1.00: failed to IDENTIFY (I/O error, err_mask=0x1)

ata1.00: revalidation failed (errno=-5)

ata1: link is slow to respond, please be patient (ready=0)

ata1: soft resetting link

ata1.00: configured for PIO

ata1: EH complete

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:08:00:00:00/00:00:00:00:00/e0 tag 0 pio 4096 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: link is slow to respond, please be patient (ready=0)

ata1: device not ready (errno=-16), forcing hardreset

ata1: soft resetting link

ata1: link is slow to respond, please be patient (ready=0)

ata1: SRST failed (errno=-16)

ata1: soft resetting link

ata1: link is slow to respond, please be patient (ready=0)

ata1.00: revalidation failed (errno=-2)

ata1: soft resetting link

ata1.00: revalidation failed (errno=-2)

ata1: link is slow to respond, please be patient (ready=0)

ata1: soft resetting link

ata1.00: configured for PIO

ata1: EH complete

ata1.00: exception Emask 0x0 SAct 0x0 SErr 0x0 action 0x6 frozen

ata1.00: cmd 20/00:08:00:00:00/00:00:00:00:00/e0 tag 0 pio 4096 in

         res 40/00:00:00:00:00/00:00:00:00:00/00 Emask 0x4 (timeout)

ata1.00: status: { DRDY }

ata1: soft resetting link

ata1.00: configured for PIO

sd 0:0:0:0: [sda] Result: hostbyte=0x00 driverbyte=0x08

sd 0:0:0:0: [sda] Sense Key : 0xb [current] [descriptor]

Descriptor sense data with sense descriptors (in hex):

        72 0b 00 00 00 00 00 0c 00 0a 80 00 00 00 00 00

        00 00 00 00

sd 0:0:0:0: [sda] ASC=0x0 ASCQ=0x0

end_request: I/O error, dev sda, sector 0

Buffer I/O error on device sda, logical block 0

ata1: EH complete

fdisk: can't read from /dev/sdasd 0:0:0:0: [sda] 312581808 512-byte hardware sectors: (160 GB/149 GiB)

root:sd

root:/>

root:/>  0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sd 0:0:0:0: [sda] 312581808 512-byte hardware sectors: (160 GB/149 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

Follow-ups

--- Barry Song                                               2009-06-22 06:34:39

Even though SATA can't work at trunk head, with the log:

irq 55: nobody cared (try booting with the "irqpoll" option)

But it can work normally in 2009R1 release like the log:

...

scsi0 : pata_platform

ata1: PATA max PIO0 mmio cmd 0x20314020 ctl 0x2031401c irq 55

ata1.00: qc timeout (cmd 0x27)

ata1.00: failed to read default max address (err_mask=0x4)

ata1.00: HPA support seems broken, skipping HPA handling

ata1.00: configured for PIO

scsi 0:0:0:0: Direct-Access     ATA      Hitachi HTS54161 SB4O PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 312581808 512-byte hardware sectors: (160 GB/149 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support

DPO or FUA

sd 0:0:0:0: [sda] 312581808 512-byte hardware sectors: (160 GB/149 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support

DPO or FUA

sda: sda1 sda2

sd 0:0:0:0: [sda] Attached SCSI disk

sd 0:0:0:0: Attached scsi generic sg0 type 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs_base@ffc00500, dma channel@7

...

root:/> mount /dev/sda1 /mnt/

EXT2-fs warning (device sda1): ext2_fill_super: mounting ext3 filesystem as

ext2

EXT2-fs warning: mounting unchecked fs, running e2fsck is recommended

root:/> cd /mnt/

root:/mnt> ls

1.txt                    lost+found

root:/mnt> cat 1.txt

ajjajajajajaj

nkksdkjds

kasksdkldskla

barry

root:/mnt>

I will check what's the difference.

--- Barry Song                                               2009-06-23 04:06:16

By the workaround, SATA can work normally for SATA hard disk connected to bf537

IDE daughter board via SATA/IDE converter.

Index: libata-core.c

===================================================================

--- libata-core.c    (revision 6835)

+++ libata-core.c    (working copy)

@@ -6128,9 +6128,9 @@

     }

     /* enable irq after probe if it is asked to be disabled when request */

-    if (host->irq_flags & IRQF_DISABLED)

+/*    if (host->irq_flags & IRQF_DISABLED)

         enable_irq(host->irq);

-

+*/

     /* perform each probe asynchronously */

     for (i = 0; i < host->n_ports; i++) {

         struct ata_port *ap = host->ports[i];

Index: libata-sff.c

===================================================================

--- libata-sff.c    (revision 6835)

+++ libata-sff.c    (working copy)

@@ -1156,6 +1156,7 @@

             if (qc) {

                 if (likely(!(qc->err_mask & AC_ERR_HSM))) {

                     ap->ops->sff_irq_on(ap);

+                    enable_irq(ap->host->irq);

                     ata_qc_complete(qc);

                 } else

                     ata_port_freeze(ap);

Tt seems our hardwares fail to set the interrupt output low in the init phase.

So the workaround postpone the enable_irq until real transfer needs the irq.

--- Michael Hennerich                                        2009-07-10 11:00:52

Hi Barry,

I think this issue is caused by a Pull-Up resistor on the INTRQ line on the

CF-IDE-NAND Card.

Read this:

http://www.mail-archive.com/t13@tgi.com/msg00418.html//www.mail-archive.com/t13@tgi.com/msg00418.html

On the CF Card socket we also have that pull-up – but there we had no choice

since in PC-Card IO mode the Interrupt is asserted Low. So this was a tradeoff,

and at the time doing the card – it worked without errors.

The problem here is that the INTRQ signal output line has a high impedance when

no devices are

selected or interruption is disabled.

Like you noticed, recent Linux libata assumes the INTRQ staying inactive the

time between the IRQ is requested and the device is configured.

If this fix isn’t acceptable to mainline we should revert – and fix the

HW.

-Michael

--- Barry Song                                               2009-07-12 22:01:31

Hi Michael,

Yes. We are using a SW workaround to make our ATA-friend storage can work at

the same time without HW change. Then we are polling in the probe, then moving

to IRQ mode for data transfer. As you know, the workaround will not enter the

mainline only as our codes.

So do you think I should revert all to the original codes? But it seems the

workaround way has existed for a long time.

-Barry

--- Robin Getz                                               2009-07-12 22:16:50

Barry:

If we have been doing it wrong a long time, we still have been doing it wrong.

The goal is to be able to boot a kernel.org kernel (eventually) - if it is not

acceptable upstream - we should not be doing it, unless we have really good

reasons. Busted hardware (wrong pull up/down) isn't a good reason.

-Robin

--- Sonic Zhang                                              2009-07-12 23:25:24

Micheal means the IDE daughter board should be fixed. But, we have to keep this

walk around till it is done. Can Micheal change the schematics in the hardware

project? We can do it accordingly in Shanghai.

--- Barry Song                                               2009-07-24 01:26:35

After pulldown the IDE_IRQ, we can use normal mainline codes to access harddisk.

Codes are reverted. So closed.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.