Article [#5228] adp5520 keys doesn't function on branch head kernel

[#5228] adp5520 keys doesn't function on branch head kernel

Submitted By: Mingquan Pan

Open Date

2009-06-11 00:23:55     Close Date

2009-06-16 05:06:54

Priority:

Medium High     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

09r1-r7

App binary format:

N/A     

Summary: adp5520 keys doesn't function on branch head kernel

Details:

adp5520 keys doesn't function on branch head kernel, the event test case doesn't have receiving info printed when hitting the button on adp5520. while the led cases works ok.

root:/> event_test /dev/input/event0

Input driver version is 1.0.0

Input device ID: bus 0x18 vendor 0x1 product 0x5520 version 0x1

Input device name: "adp5520-keys"

Supported events:

  Event type 0 (Reset)

    Event code 0 (Reset)

    Event code 1 (Key)

  Event type 1 (Key)

    Event code 2 (1)

    Event code 3 (2)

    Event code 4 (3)

    Event code 5 (4)

    Event code 6 (5)

    Event code 7 (6)

    Event code 8 (7)

    Event code 9 (8)

    Event code 10 (9)

    Event code 11 (0)

    Event code 12 (Minus)

    Event code 13 (Equal)

    Event code 14 (Backspace)

    Event code 28 (Enter)

    Event code 41 (Grave)

    Event code 43 (BackSlash)

Testing ... (interrupt to exit)

^Croot:/>

root:/>

root:/> version

kernel:    Linux release 2.6.28.10-ADI-2009R1-svn6635, build #2 Thu Jun 11 11:56:49 CST 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8268, build #1 Thu Jun 11 11:55:57 CST 2009

Follow-ups

--- Michael Hennerich                                        2009-06-15 04:04:55

On the ADP5520 Demo Board:

How did you set J1 to J8 when testing the keypad?

-Michael

--- Mingquan Pan                                             2009-06-16 05:06:54

Yes, after setting J1-J8 to KP, the keys on adp5520 board works.

root:/bin> modprobe adp5520-keys

input: adp5520-keys as

/devices/platform/i2c-bfin-twi.0/i2c-adapter/i2c-0/0-0032/adp5520-keys.5520/input/input0

root:/bin> event_test /dev/input/event0

Input driver version is 1.0.0

Input device ID: bus 0x18 vendor 0x1 product 0x5520 version 0x1

Input device name: "adp5520-keys"

Supported events:

  Event type 0 (Reset)

    Event code 0 (Reset)

    Event code 1 (Key)

  Event type 1 (Key)

    Event code 2 (1)

    Event code 3 (2)

    Event code 4 (3)

    Event code 5 (4)

    Event code 6 (5)

    Event code 7 (6)

    Event code 8 (7)

    Event code 9 (8)

    Event code 10 (9)

    Event code 11 (0)

    Event code 12 (Minus)

    Event code 13 (Equal)

    Event code 14 (Backspace)

    Event code 28 (Enter)

    Event code 41 (Grave)

    Event code 43 (BackSlash)

Testing ... (interrupt to exit)

Event: time 285903.656000, type 1 (Key), code 41 (Grave), value 1

Event: time 285903.656000, type 0 (Reset), code 0 (Reset), value 0

Event: time 285903.968000, type 1 (Key), code 41 (Grave), value 0

Event: time 285903.968000, type 0 (Reset), code 0 (Reset), value 0

Event: time 285904.660000, type 1 (Key), code 5 (4), value 1

Event: time 285904.660000, type 0 (Reset), code 0 (Reset), value 0

Event: time 285904.920000, type 1 (Key), code 5 (4), value 0

Event: time 285904.920000, type 0 (Reset), code 0 (Reset), value 0

Event: time 285905.996000, type 1 (Key), code 9 (8), value 1

Event: time 285905.996000, type 0 (Reset), code 0 (Reset), value 0

Event: time 285906.176000, type 1 (Key), code 9 (8), value 0

Event: time 285906.176000, type 0 (Reset), code 0 (Reset), value 0          

So close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.