Article [#5394] run irattach in the background, reboot the kernel, error info shows up

[#5394] run irattach in the background, reboot the kernel, error info shows up

Submitted By: Vivi Li

Open Date

2009-07-24 03:29:07     Close Date

2009-08-05 02:57:39

Priority:

Medium     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1_rc9

App binary format:

N/A     

Summary: run irattach in the background, reboot the kernel, error info shows up

Details:

After run irattach in the background, reboot the kernel, error info shows up.

If irattach is not run in the background, reboot kernel will cause no error info.

--

root:/> modprobe bfin_sir

root:/> irattach irda0 -s&

164

root:/> reboot

NULL pointer access

Deferred Exception context

CURRENT PROCESS:

COMM=irattach PID=164

CPU = 0

TEXT = 0x001c0040-0x001c8aa0        DATA = 0x001c8ac0-0x001caae8

BSS = 0x001caae8-0x001caf30  USER-STACK = 0x001cbf70

return address: [0x001c1614]; contents of:

0x001c15f0:  1432  e129  fad4  5a79  e120  03fe  3049  5181

0x001c1600:  e14a  001c  e10a  ab44  9110  4828  104c  320e

0x001c1610:  6000  9b08 [9118] 0c80  1854  e12a  fad4  5a97

0x001c1620:  307a  2004  51c7  09be  1b3c  52be  640a  300f

ADSP-BF537-0.2 500(MHz CCLK) 125(MHz SCLK) (mpu off)

Linux version 2.6.28.10-ADI-2009R1-svn7051

Built with gcc version 4.1.2 (ADI svn)

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00062027  IPEND: 0030  SYSCFG: 0006

  EXCAUSE   : 0x27

  interrupts disabled

  physical IVG5 asserted : <0xffa00c34> { _evt_ivhw + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x037ba000> /* kernel dynamic memory */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x001c16b8> [ irattach + 0x1678 ]

PC  : <0x001c1614> [ irattach + 0x15d4 ]

DCPLB_FAULT_ADDR: <0x00000000> /* Maybe null pointer? */

ICPLB_FAULT_ADDR: <0x001c1614> [ irattach + 0x15d4 ]

PROCESSOR STATE:

R0 : 00000000    R1 : 001cabe8    R2 : 00000024    R3 : 40000000

R4 : 001cafd3    R5 : 000003de    R6 : 001cac0b    R7 : 001cabf5

P0 : 00000004    P1 : 001cac0b    P2 : 001cadf4    P3 : 00000000

P4 : 001cabe8    P5 : 001cadf4    FP : 001cb100    SP : 037b9f24

LB0: 001c379d    LT0: 001c379a    LC0: 00000000

LB1: 001c2c25    LT1: 001c2c24    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 001ca040

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 001ca82c

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 001cabc0  ASTAT: 02000000

Hardware Trace:

   0 Target : <0x00004cbc> { _trap_c + 0x0 }

     Source : <0xffa00674> { _exception_to_level5 + 0xa8 } CALL pcrel

   1 Target : <0xffa005cc> { _exception_to_level5 + 0x0 }

     Source : <0xffa004a4> { _bfin_return_from_exception + 0x20 } RTX

   2 Target : <0xffa00484> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa0051a> { _ex_trap_c + 0x46 } JUMP.S

   3 Target : <0xffa004d4> { _ex_trap_c + 0x0 }

     Source : <0xffa003ac> { _ex_workaround_261 + 0x1c } JUMP.S

   4 Target : <0xffa00390> { _ex_workaround_261 + 0x0 }

     Source : <0xffa0074e> { _trap + 0x66 } JUMP (P4)

   5 Target : <0xffa00708> { _trap + 0x20 }

     Source : <0xffa00704> { _trap + 0x1c } IF !CC JUMP

   6 Target : <0xffa006e8> { _trap + 0x0 }

     Source : <0xffa004a4> { _bfin_return_from_exception + 0x20 } RTX

   7 Target : <0xffa00484> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa003a2> { _ex_workaround_261 + 0x12 } IF !CC JUMP

   8 Target : <0xffa00390> { _ex_workaround_261 + 0x0 }

     Source : <0xffa0074e> { _trap + 0x66 } JUMP (P4)

   9 Target : <0xffa00708> { _trap + 0x20 }

     Source : <0xffa00704> { _trap + 0x1c } IF !CC JUMP

  10 Target : <0xffa006e8> { _trap + 0x0 }

     Source : <0x001c1612> [ irattach + 0x15d2 ] 0x9b08

  11 Target : <0x001c160e> [ irattach + 0x15ce ]

     Source : <0x001c16b8> [ irattach + 0x1678 ] JUMP.S

  12 Target : <0x001c16b8> [ irattach + 0x1678 ]

     Source : <0x001c5350> [ irattach + 0x5310 ] RTS

  13 Target : <0x001c534a> [ irattach + 0x530a ]

     Source : <0x001c535e> [ irattach + 0x531e ] JUMP.S

  14 Target : <0x001c5356> [ irattach + 0x5316 ]

     Source : <0x001c11a4> [ irattach + 0x1164 ] RTS

  15 Target : <0x001c1194> [ irattach + 0x1154 ]

     Source : <0x001c5352> [ irattach + 0x5312 ] CALL pcrel

Userspace Stack

Stack info:

SP: [0x001cabc0] <0x001cabc0> [ irattach + 0xabc0 ]

Memory from 0x001cabc0 to 001cb000

001cabc0:[00000000] 00000000  000000a4  001cb144  00000000  3e34313c  206e614a  30203120

001cabe0: 31303a30  2031343a  6c737973  315b676f  3a5d3436  746f6720  47495320  4d524554

001cac00: 20726f20  49474953  000a544e  00000000  00000000  00000000  00000000  00000000

001cac20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cac40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cac60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cac80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001caca0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cacc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cace0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cad00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cad20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cad40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cad60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cad80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cada0: 00000000  00000000  00000000  001cbbb5  00000000  00000002  00000001  00000000

001cadc0: 00000000  00000001  001cbfaa  00000001  00000000  00000002  00000003  008b8783

001cade0: 001cbf84  00001000  001c8a8a  00000000  00000001  00000009  00000000  20756854

001cae00: 206e614a  30203120  31303a30  2031343a  30373931  0000000a  00000000  00000010

001cae20: 00000000  032f9000  00000000  72690000  00306164  00000000  00000000  00000000

001cae40: 00000000  00000000  00000000  00000000  00000000  00435455  00000000  00000000

001cae60: 00000000  00000000  00000000  00000000  00000000  00000029  00000001  00000000

001cae80: 00000001  00000000  00000046  00000004  00000000  00000000  00000000  001ca85c

001caea0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001caec0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001caee0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001caf00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001caf20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001caf40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001caf60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001caf80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cafa0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

001cafc0: 00000000  00000000  001c8c34  00000000  001c8c34  001c120c  00000000  00000000

001cafe0: 00000000  00000001  00000000  00000000  00000002  00000001  00000000  001cbf99

Return addresses in stack:

Restarting system.þ

U-Boot 2008.10-svn1905 (ADI-2009R1-rc2) (Jun  8 2009 - 04:43:24)

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   4E:03:4E:03:4E:03

Hit any key to stop autoboot:  0

bfin>

--

Follow-ups

--- Graf Yang                                                2009-07-28 06:31:28

Use the daemon() to make irattach run background. Now is fixed on trunk and

09R1.

--- Vivi Li                                                  2009-08-05 02:57:39

OK now. Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.irda    application/octet-stream    32693    Vivi Li

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.