Article [#5428] u-boot can not receive any input when irda card is plugged into bf533-stamp

[#5428] u-boot can not receive any input when irda card is plugged into bf533-stamp

Submitted By: Vivi Li

Open Date

2009-08-10 01:09:24    

Priority:

Very Low     Assignee:

Nobody

Status:

Open     Fixed In Release:

N/A

Found In Release:

2009R1-RC6     Release:

Category:

N/A     Board:

STAMP

Processor:

BF533     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

N/A

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1_rc9

App binary format:

N/A     

Summary: u-boot can not receive any input when irda card is plugged into bf533-stamp

Details:

When irda add-on card is plugged into bf533-stamp, u-boot can not receive any input, then it boot into kernel automatically.

--

U-Boot 2008.10-svn1974 (ADI-2009R1-rc3) (Jul 17 2009 - 21:17:51)

CPU:   ADSP bf533-0.3 (Detected Rev: 0.3) (bypass boot)

Board: ADI BF533 Stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 497.664 MHz, Core: 497.664 MHz, System: 99.532 MHz

RAM:   128 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   MAC:   00:E0:22:FE:07:59

Hit any key to stop autoboot:  3

(press any key, no response, then it boot into kernel automatically)

--

Follow-ups

No Messages Were Found

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.