Article [#5445] jffs2 stress test fails on bf561 smp kernel

[#5445] jffs2 stress test fails on bf561 smp kernel

Submitted By: Mingquan Pan

Open Date

2009-08-16 21:00:40     Close Date

2010-01-04 00:05:38

Priority:

Medium High     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2009R1-RC6     Release:

Category:

N/A     Board:

N/A

Processor:

BF561     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Not reproducible

Uboot version or rev.:

    Toolchain version or rev.:

09r1-rc9

App binary format:

N/A     

Summary: jffs2 stress test fails on bf561 smp kernel

Details:

jffs2 stress test fails on bf561 smp kernel these days.

It can boot up serveral times with jffs2 as rootfs after images are flashed into board. but sometimes it would fails to react after booting up.

root:/> reboot

Restarting system.每

U-Boot 2008.10-svn1954 (ADI-2009R1-rc2) (Jul  1 2009 - 00:35:43)

CPU:   ADSP bf561-0.3 (Detected Rev: 0.5) (bypass boot)

Board: ADI BF561 EZ-Kit Lite board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 600 MHz, Core: 600 MHz, System: 100 MHz

RAM:   64 MB

Flash:  8 MB

In:    serial

Out:   serial

Err:   serial

Net:   MAC:   00:E0:22:FE:BA:2A

Hit any key to stop autoboot:  0

bfin>

bfin> bootm 20040000

## Booting kernel from Legacy Image at 20040000 ...

   Image Name:   Linux-2.6.28.10-ADI-2009R1-svn71

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    949615 Bytes = 927.4 kB

   Load Address: 00001000

   Entry Point:  0019d134

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 0019d134

Linux version 2.6.28.10-ADI-2009R1-svn7193 (test@uclinux65-561-SMP) (gcc version 4.1.2 (ADI svn)) #21 SMP Sun Aug 16 16:37:37 GMT 2009

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0011b280

  rodata    = 0x0011b280-0x0016de00

  bss       = 0x0016e000-0x0017fa84

  data      = 0x0017faa0-0x00192000

    stack   = 0x00190000-0x00192000

  init      = 0x00192000-0x001ad000

  available = 0x001ad000-0x03eff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF561 Rev 0.5

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 600 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-through)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16001

Kernel command line: root=/dev/mtdblock2 rw rootfstype=jffs2 earlyprintk=serial,uart0,57600

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 62196k/65536k RAM, (108k init code, 1128k kernel code, 476k data, 1024k dma, 600k reserved)

Calibrating delay loop... 1191.93 BogoMIPS (lpj=2383872)

Security Framework initialized

Mount-cache hash table entries: 512

CoreB bootstrap code to SRAM ff600000 via DMA.

Booting Core B.

Instruction Cache Enabled for CPU1

Data Cache Enabled for CPU1 (write-through)

Calibrating delay loop... 1191.93 BogoMIPS (lpj=2383872)

Brought up 2 CPUs

SMP: Total of 2 processors activated (2383.87 BogoMIPS).

Blackfin Scratchpad data SRAM: 4 KB

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 16 KB (15 KB free)

Blackfin L1 Instruction SRAM: 16 KB (15 KB free)

Blackfin L2 SRAM: 128 KB (127 KB free)

net_namespace: 296 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 2, 16384 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

JFFS2 version 2.2. (NAND) 漏 2001-2006 Red Hat, Inc.

msgmni has been set to 121

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 35) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 2) at 2c010300 IRQ 82 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:ba:2a

physmap platform flash device: 00800000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Amd/Fujitsu Extended Query Table at 0x0040

physmap-flash.0: Swapping erase regions for broken CFI table.

number of CFI chips: 1

cfi_cmdset_0002: Disabling erase-suspend-program due to code brokenness.

RedBoot partition parsing not available

Using physmap partition information

Creating 3 MTD partitions on "physmap-flash.0":

0x00000000-0x00040000 : "bootloader(nor)"

0x00040000-0x00200000 : "linux kernel(nor)"

0x00200000-0x00800000 : "file system(nor)"

TCP cubic registered

NET: Registered protocol family 17

VFS: Mounted root (jffs2 filesystem).

Freeing unused kernel memory: 108k freed

dma_alloc_init: dma_page @ 0x001a9000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.13.4 (2009-08-16 13:06:27 GMT) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/>

Case 5 ...PASS

Wait for 1 minutes before reboot.

root:/>

root:/> rebo

Last passed time: 2009_Aug_15_05_38, ucdist ver: 8726, kernel ver: 7193

Case 6 ...FAIL

Follow-ups

--- Graf Yang                                                2009-08-20 05:38:27

This bug is not reproducible after fixed bug [#5448].

--- Mingquan Pan                                             2010-01-04 00:05:45

Yeah, the jffs stress test is passed on bf561 SMP kernel now. Close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.