Article [#5472] Oprofile test fails as hush doesnt seem to pass command line args down

[#5472] Oprofile test fails as hush doesnt seem to pass command line args down

Submitted By: Vivi Li

Open Date

2009-08-30 23:38:41     Close Date

2009-09-02 19:24:15

Priority:

Medium     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

Tests     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1_rc9

App binary format:

N/A     

Summary: Oprofile test fails as hush doesnt seem to pass command line args down

Details:

Oprofile test fails as we use hush instead of bash in trunk, and it needs update to hush too.

Bellow is the error log:

--

Linux version 2.6.30.5-ADI-2010R1-pre-svn7247 (test@uclinux50-bf537-ad9960-ad1836) (gcc version 4.1.2 (ADI svn)) #6 Sun Aug 30 19

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00115b30

  rodata    = 0x00115b30-0x00171ef4

  bss       = 0x00172000-0x001a5da4

  data      = 0x001a5dc0-0x001b8000

    stack   = 0x001b6000-0x001b8000

  init      = 0x001b8000-0x00f0d000

  available = 0x00f0d000-0x037ff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14223

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

NR_IRQS:98

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 41360k/65536k RAM, (13652k init code, 1106k kernel code, 650k data, 1024k dma, 7744k reserved)

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (36 KB free)

net_namespace: 296 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 80

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

oprofile: using timer interrupt.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1971-04-09 02:31:04 UTC (40012264)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 13652k freed

dma_alloc_init: dma_page @ 0x00f08000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.14.3 (2009-08-30 13:39:50 CST) hush - the humble shell

root:/> PHY: 0:01 - Link is Up - 100/Full

root:/> /usr/bin/bfin_opcontrol --init

/bin/sh: invalid option -- -

BusyBox v1.14.3 (2009-08-30 13:39:50 CST) multi-call binary

No help available.

root:/>

--

Follow-ups

--- Mike Frysinger                                           2009-09-02 06:33:20

should be fixed already in 1.15.0 which is now in trunk

BusyBox v1.15.0 (2009-09-02 06:22:31 EDT) hush - the humble shell

root:/> /bfin_opcontrol -h

Unknown option . See opcontrol --help

root:/> /bfin_opcontrol --help

help:

--init   initialize oprofile system and create some directory

--setup  set some parameter for kernel performance monitor registers

--start-daemon launch oprofiled to collect data

--start  performance monitor counter begin to count

--stop   performance monitor counter stop

--dump   dump some samples from kernel

--list-event list all the event type in Blackfin

--help show the above message

--- Vivi Li                                                  2009-09-03 00:25:21

OK now. Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.