Article [#5484] adv7183 test failed in trunk on bf561-ezkit

[#5484] adv7183 test failed in trunk on bf561-ezkit

Submitted By: Vivi Li

Open Date

2009-09-02 22:28:20     Close Date

2009-10-13 03:57:37

Priority:

Medium     Assignee:

Michael Hennerich

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF561     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-rc9

App binary format:

N/A     

Summary: adv7183 test failed in trunk on bf561-ezkit

Details:

adv7183 test failed in trunk on bf561-ezkit.

Bellow is the log and kernel config file is attached:

--

Linux version 2.6.30.5-ADI-2010R1-pre-svn7256 (test@uclinux66-561ezkit) (gcc version 4.1.2 (ADI svn)) #4 Wed Sep 2 10:30:20 CST 9

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00100000-0x00207340

  rodata    = 0x00207340-0x002638d8

  bss       = 0x00264000-0x002751e4

  data      = 0x002751e4-0x00288000

    stack   = 0x00286000-0x00288000

  init      = 0x00288000-0x00b30000

  available = 0x00b30000-0x03dff000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF561 Rev 0.5

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 600 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

  L2 SRAM        : uncacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

  L2 SRAM        : uncacheable in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15747

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=30000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

NR_IRQS:121

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 51460k/65536k RAM, (8864k init code, 1052k kernel code, 516k data, 2048k dma, 1592k reserved)

Calibrating delay loop... 1196.03 BogoMIPS (lpj=2392064)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 16 KB (5 KB free)

Blackfin L2 SRAM: 128 KB (128 KB free)

net_namespace: 296 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

bio: create slab <bio-0> at 0

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 100

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 35) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 2c010300 IRQ 82 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:b1:3c

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@16

i2c-gpio i2c-gpio.0: using pins 1 (SDA) and 0 (SCL)

Linux video capture interface: v2.00

driver for ADV7183B get_camops

driver for ADV7183B get_camops

ADV7183B: detecting client on address 0x40

driver for ADV7183B init

ADV7183B: V4L driver Blackfin CMOS Camera now ready

ADV7183B: i2c driver ready

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

eth0: link down

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf561-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 8864k freed

dma_alloc_init: dma_page @ 0x00bf7000 - 512 pages at 0x03e00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - https://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.15.0 (2009-09-02 10:26:32 CST) hush - the humble shell

e

tooh:/0 : link up, 100Mbps, full-duplex, lpa 0x41E1

root:/>

root:/> ffmpeg -f video4linux -r 10.0 -s 720x288 -i /dev/video0 -qscale 6 -f mjpeg udp:10.100.4.174:1234

FFmpeg version SVN-r8802, Copyright (c) 2000-2007 Fabrice Bellard, et al.

  configuration: --prefix=/usr --source-path=/home/test/work/cruise/checkouts/uclinux-dist/lib/ffmpeg/build/../ffmpeg-svn-11114 -

  libavutil version: 49.5.0

  libavcodec version: 51.48.0

  libavformat version: 52.1.0

  built on Sep  2 2009 10:25:23, gcc: 4.1.2 (ADI svn)

[video4linux @ 0x381078]VIDIOCGCAP: Invalid argument

/dev/video0: I/O error occured

Usually that means that input file is truncated and/or corrupted.

root:/>

root:/> version

kernel:    Linux release 2.6.30.5-ADI-2010R1-pre-svn7256, build #4 Wed Sep 2 10:30:20 CST 2009

toolchain: bfin-linux-uclibc-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8802, build #50 Wed Sep 2 10:29:17 CST 2009

root:/>

--

Follow-ups

--- Michael Hennerich                                        2009-09-03 03:58:28

assign to me

-Michael

--- Michael Hennerich                                        2009-09-30 10:50:53

v4l_ioctl parameter list changed

fixed on trunk.

-Michael

--- Vivi Li                                                  2009-10-13 03:57:37

OK now on bf561-ezkit.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.camera_adv7183    application/octet-stream    31228    Vivi Li

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.