Article [#5537] bfindma test failed in latest trunk

[#5537] bfindma test failed in latest trunk

Submitted By: Vivi Li

Open Date

2009-09-15 04:09:01     Close Date

2009-10-30 00:01:29

Priority:

Medium     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

Drivers     Board:

N/A

Processor:

BF533     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-rc9

App binary format:

N/A     

Summary: bfindma test failed in latest trunk

Details:

bfindma test failed in latest trunk on bf533-ezkit.

Enable BFIN_DMA_INTERFACE in kernel config and BFIN_DMA in user config.

Bellow is the log in bf533-ezkit:

--

Linux version 2.6.31-ADI-2010R1-pre-svn7313 (test@uclinux67-533ezkit) (gcc version 4.1.2 (ADI svn)) #80 Mon Sep 14 23:52:09 CST 9

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 32MB

Kernel Managed Memory: 32MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00105b40

  rodata    = 0x00105b40-0x00159088

  bss       = 0x0015a000-0x0016a9b4

  data      = 0x0016a9b4-0x0017a000

    stack   = 0x00178000-0x0017a000

  init      = 0x0017a000-0x006d4000

  available = 0x006d4000-0x01eff000

  DMA Zone  = 0x01f00000-0x02000000

Hardware Trace Active and Enabled

Boot Mode: 0

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Warning: Compiled for Rev 3, but running on Rev 4

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 594 MHz core clock and 118 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 7873

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=27000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

PID hash table entries: 128 (order: 7, 512 bytes)

Dentry cache hash table entries: 4096 (order: 2, 16384 bytes)

Inode-cache hash table entries: 2048 (order: 1, 8192 bytes)

Memory available: 24460k/32768k RAM, (5480k init code, 1042k kernel code, 466k data, 1024k dma, 296k reserved)

NR_IRQS:49

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 1183.74 BogoMIPS (lpj=2367488)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (52 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

bio: create slab <bio-0> at 0

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 1024 (order: 1, 8192 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 1024 bind 1024)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 47

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-dma: initialized

Serial: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0x0 (irq = 21) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@cam.org>

eth0: SMC91C11xFD (rev 1) at 20310300 IRQ 42 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:b1:2e

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-06-01 00:02:02 UTC (1086048122)

eth0: link down

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf533-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 5480k freed

dma_alloc_init: dma_page @ 0x01706000 - 256 pages at 0x01f00000

eth0: link up, 100Mbps, full-duplex, lpa 0x41E1

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.15.0 (2009-09-14 14:38:46 CST) hush - the humble shell

root:/> version

kernel:    Linux release 2.6.31-ADI-2010R1-pre-svn7313, build #80 Mon Sep 14 23:52:09 CST 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8852, build #509 Mon Sep 14 23:51:20 CST 2009

root:/> bfin-dma

open(/dev/bfin-dma) = 3

ioctl(3, 0: BF_DMA_REQUEST, 0x27aee0) = 0

ioctl(3, 2: BF_DMA_RUN, 0x27aee0) = 0

memcmp = 15

73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73 73

64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64 64

ioctl(3, 1: BF_DMA_FREE, 0x27aee0) = -1 (Invalid argument)

ioctl(3, 0: BF_DMA_REQUEST, 0x27aeb4) = -1 (Device or resource busy)

ioctl(3, 3: BF_DMA_ARUN, 0x27aeb4) = 0

--

Last passed version:

--

root:/> version

kernel:    Linux release 2.6.30.6-ADI-2010R1-pre-svn7299, build #61 Sat Sep 12 08:27:29 CST 2009

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)

user-dist: release svn-8837, build #456 Sat Sep 12 08:26:42 CST 2009

--

Follow-ups

--- Graf Yang                                                2009-10-26 22:38:46

This bug also existed on BF537-stamp board.

--- Graf Yang                                                2009-10-27 00:10:59

The get_blk_size ioctls is moved outisde from file_ioctl, its ioctl number

FIGETBSZ conflicts with BF_DMA_RUN. Now is fixed on trunk.

--- Vivi Li                                                  2009-10-30 00:01:29

OK now.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.