Article [#5658] [ltp] ltp test case umount02 fail with kernel dump info

[#5658] [ltp] ltp test case umount02 fail with kernel dump info

Submitted By: Vivi Li

Open Date

2009-11-04 04:07:25     Close Date

2009-11-12 05:02:43

Priority:

Medium     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

Tests     Board:

N/A

Processor:

BF548     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1-09r1-rc9

App binary format:

N/A     

Summary: [ltp] ltp test case umount02 fail with kernel dump info

Details:

ltp test case umount02 fails with kernel dump info.

This is not a regression result. This case are not tested before.

Bellow is the log on bf548-ezkit, and /dev/sdb1 is a ext2 fs on usb.

--

root:/> umount02 -D /dev/sdb1

NULL pointer access

Deferred Exception context

CURRENT PROCESS:

COMM=umount02 PID=349 CPU=0

TEXT = 0x00bc0040-0x00bcc800        DATA = 0x00bcc804-0x00bcfc4c

BSS = 0x00bcfc4c-0x00bd7ac4  USER-STACK = 0x00bdff54

return address: [0x00bc6486]; contents of:

0x00bc6460:  3018  1006  e801  0000  6000  0538  0010  5048

0x00bc6470:  3209  0981  63f8  0788  6018  5403  0c00  184c

0x00bc6480:  0000  0000  3213 [9950] 0c00  183c  300b  601a

0x00bc6490:  2005  3211  9950  0c00  1836  6409  5411  0c00

ADSP-BF548-0.2 525(MHz CCLK) 131(MHz SCLK) (mpu off)

Linux version 2.6.31.5-ADI-2010R1-pre-svn7743 (test@uclinux61-bf548-std) (gcc version 4.3.4 (ADI-trunk/svn-3648) ) #72 Tue Nov 39

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00000027  IPEND: 0008  IMASK: ffff  SYSCFG: 0006

  EXCAUSE   : 0x27

  physical IVG3 asserted : <0xffa007b0> { _trap + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x00b66000> /* kernel dynamic memory */

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x00bc5326> [ umount02 + 0x52e6 ]

PC  : <0x00bc6486> [ umount02 + 0x6446 ]

DCPLB_FAULT_ADDR: <0x00000013> /* Maybe null pointer? */

ICPLB_FAULT_ADDR: <0x00bc6486> [ umount02 + 0x6446 ]

PROCESSOR STATE:

R0 : 00000003    R1 : 00000012    R2 : 00000008    R3 : 00000013

R4 : 0000000b    R5 : 00000000    R6 : 00000007    R7 : 0000000e

P0 : 00000013    P1 : ffffffff    P2 : 00000013    P3 : 0000004d

P4 : 00000000    P5 : 00000000    FP : 00bdf488    SP : 00b65f24

LB0: 00bc60f1    LT0: 00bc60ee    LC0: 00000000

LB1: 00bc538d    LT1: 00bc538c    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 00bcf9b4

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 00000000

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000020   A0.x: 00000000   A1.w: 00000020   A1.x: 00000000

USP : 00bdf488  ASTAT: 02003004

Hardware Trace:

   0 Target : <0x0000522c> { _trap_c + 0x0 }

     Source : <0xffa00744> { _exception_to_level5 + 0xa4 } CALL pcrel

   1 Target : <0xffa006a0> { _exception_to_level5 + 0x0 }

     Source : <0xffa00554> { _bfin_return_from_exception + 0x18 } RTX

   2 Target : <0xffa0053c> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa005f8> { _ex_trap_c + 0x74 } JUMP.S

   3 Target : <0xffa00584> { _ex_trap_c + 0x0 }

     Source : <0xffa0080a> { _trap + 0x5a } JUMP (P4)

   4 Target : <0xffa007b0> { _trap + 0x0 }

     Source : <0x00bc6484> [ umount02 + 0x6444 ] 0x3213

   5 Target : <0x00bc646e> [ umount02 + 0x642e ]

     Source : <0x00bc6462> [ umount02 + 0x6422 ] IF !CC JUMP

   6 Target : <0x00bc6458> [ umount02 + 0x6418 ]

     Source : <0x00bc5322> [ umount02 + 0x52e2 ] CALL pcrel

   7 Target : <0x00bc530a> [ umount02 + 0x52ca ]

     Source : <0x00bc50dc> [ umount02 + 0x509c ] IF !CC JUMP

   8 Target : <0x00bc50c8> [ umount02 + 0x5088 ]

     Source : <0x00bc4f90> [ umount02 + 0x4f50 ] IF CC JUMP

   9 Target : <0x00bc4f6e> [ umount02 + 0x4f2e ]

     Source : <0x00bc5118> [ umount02 + 0x50d8 ] JUMP.S

  10 Target : <0x00bc5110> [ umount02 + 0x50d0 ]

     Source : <0x00bc4f5c> [ umount02 + 0x4f1c ] IF !CC JUMP

  11 Target : <0x00bc4f4e> [ umount02 + 0x4f0e ]

     Source : <0x00bc5490> [ umount02 + 0x5450 ] RTS

  12 Target : <0x00bc548a> [ umount02 + 0x544a ]

     Source : <0x00bc5478> [ umount02 + 0x5438 ] IF CC JUMP

  13 Target : <0x00bc5404> [ umount02 + 0x53c4 ]

     Source : <0x00bc4f4a> [ umount02 + 0x4f0a ] CALL pcrel

  14 Target : <0x00bc4f42> [ umount02 + 0x4f02 ]

     Source : <0x00bc5706> [ umount02 + 0x56c6 ] RTS

  15 Target : <0x00bc5700> [ umount02 + 0x56c0 ]

     Source : <0x00bc584c> [ umount02 + 0x580c ] JUMP.S

Userspace Stack

Stack info:

SP: [0x00bdf488] <0x00bdf488> [ umount02 + 0x1f488 ]

FP: (0x00bdf488)

Memory from 0x00bdf480 to 00be0000

00bdf480: 0000004d  00bdf5d8 [00bdf5d8]<00bc5326> 0000000e  00000000  00000000  00000000

00bdf4a0: 00000000  00000000  00000013  20000000  00000000  00000007  00bccadf  ffffffff

00bdf4c0: 00000000  00000073  00000000  00000020  00000000  00000001  00000013  00010000

00bdf4e0: 00000003  00000008  00000008  00000008  00000008  00000008  00000008  00000008

00bdf500: 00000008  00bdfea0  00000013  00000000  00000000  00000000  00000000  00000000

00bdf520: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf540: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf560: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf580: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf5a0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf5c0: 00000000  00000000  00000000  00000000  00bdf508  20000000  00bdf648 <00bc4a4e>

00bdf5e0: 00bcc804  00bcf9d0  00000003  ff42097f  00000013  00bc0990  00bdff8e  00bdf608

00bdf600: 00000000  00000000  000000d0  fffffffe  00bdf680  ffffffff  00bdf6cd  00bdf680

00bdf620: 00bdf680  ffffffff  00000000  00000000  00000000  00000000  00000000  00000000

00bdf640: 00000000  00000000  00bdf664 <00bc49c4> 00bd1c90  00000000  00000000  00000000

00bdf660: 00bdfe94  00bdfe80 <00bc2c3a> 00000000  00000000  00000000  00000000  00bdfe94

00bdf680: 6e756f6d  29322874  69616620  2064656c  6d206f74  746e756f  76656420  20656369

00bdf6a0: 7665642f  6264732f  74612031  756f6d20  6f70746e  20746e69  5f746e6d  2c393433

00bdf6c0: 746f4720  72726520  2d206f6e  00000020  00000000  00000000  00000000  00000000

00bdf6e0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf700: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf720: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf740: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf760: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf780: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf7a0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf7c0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf7e0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf800: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf820: 00000000  00000000  00000000  00000000  00bcdc1a  00000000  00000000  00000000

00bdf840: 00000000  00000000  00000000  00bcdc1a  00000008  00000003  00bdf888  00000000

00bdf860: 00000000  00bdf8bc  00000008  00000008  00000008  00bdf9dc <00bc4f42> 00bcdc17

00bdf880: 00bdf9dc <00bc50c6> 00bcdc21  00000006  00000003  00000000  00000000  00000000

00bdf8a0: 00000000  00000000  00000000  00bcc824  20000000  00000000  00000003  00bcdc1b

00bdf8c0: 00000003  00000000  00000073  00000000  00000020  00000000  00000001  00000013

00bdf8e0: 00010000  00000003  00000008  00000008  00000008  00000008  00000008  00000008

00bdf900: 00000008  00000008  00bdfa84  00bcc824  00000000  00000000  00000000  00000000

00bdf920: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf940: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf960: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf980: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdf9a0: 00000000  00bdfa8c  00bdfa34 <00bc8478> 00000006  00000000  00000000  00000000

00bdf9c0: 84210843  00bd3c00  00bdfa94  00000000  00000000  00bdf90c  20000000  00bdfa4c

00bdf9e0:<00bc4a4e> 00bcc804  00bcf9d0  00000003  00000400  00bdff58  00bd3be4  00bcc7cc

00bdfa00: 00bdfa0c  00000000  00bdfa34 <00bc67d0> 00bdfa34 <00bc67e4> 00bdfe8c  00bdfa9a

00bdfa20: 00bdfa8c  00bdfa8c  00bdfe8c  dd5ef4d0  00000014  00bdfa5c <00bc656e> 00bcc804

00bdfa40: 00bcf9d0  00000000  0000000f  00000003  00bd3be4  00bcc7cc  00bdfa8c  00bdfe94

00bdfa60:<00bc31f0> 00bdfe94 <00bc330a> 00bcf89c  00000000  00000000  00000000  00bcdc24

00bdfa80: 00bcc824  00000000  00000000  706d742f  6f6d752f  4a473677  0000646b  00000000

00bdfaa0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfac0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfae0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfb00: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfb20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfb40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfb60: 00000000  00000000  00bdfc9c <00bc6738> 00bdfcc4  00000000  00000000  00000000

00bdfb80: 00000008  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfba0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfbc0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfbe0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfc00: 00000000  00000000  00000000  00000000  00bc2ffc  10000000  00000000  00000000

00bdfc20: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfc40: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfc60: 00000000  00000000  00bccbdd  00000000  00000000  00000000  00000000  00000000

00bdfc80: 00000000  00bccbdd  00000008  00000000 <00bc8984> 00000000  00000000  00bdfcf4

00bdfca0: 00000008  00000000  00000004  00bdfe14 <00bc5000> 00000000  00bdfe14 <00bc533e>

00bdfcc0: 00000000  00000000  00000003  00000000  00000000  00000000  00000000  fffffff6

00bdfce0: 00000057  00bdfe08  20000000  00000000  00000003  00bccbde  ffffffff  00000000

00bdfd00: 00000064  00000000  00000020  00000000  00000001  00000006  00010000  00000000

00bdfd20: 00000008  00000008  00000008  00000008  00000008  00000008  00000008  00000008

00bdfd40: 00bdfeb4  0000015d  00000000  00000000  00000000  00000000  00000000  00000000

00bdfd60: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfd80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfda0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

00bdfdc0: 00000000  00000000  00000000  00000000  00000000  10000000  00000000  00000000

00bdfde0: 00bdfe9c <00bc2fa2> 00000030  00bc2ffc  00000000  00bdfe48  00bdfe48  00000037

00bdfe00: 00000044  00bdff58  00bdfe58  00000003  20000000  00bdfe84 <00bc4a4e> 00bcc804

00bdfe20: 00bcf9d0  00000003  ff42e36f  00bdff58  00bd3be4  00bcc7cc  00bdfe44  00000000

00bdfe40: 00bdfe80  00bd00d0  fffffffe  00bd1c90  ffffffff  00bd1c97  00bdfe7c <00bc659e>

00bdfe60: 00bcc804  00bd3b7c  00000013  00bc0990 <00bc0f4e> 00bdfec8 <00bc15ea> 00bdfebc

00bdfe80: 00bdfebc <00bc05dc> 00000002  00bc0990 <00bcca9c> 00bdff8e  00bd1c90  00000013

00bdfea0: 00bd3b7c <00bc0986> 00000001  00bc2ffc  00000001  00000018  00000000  00bdff00

00bdfec0:<00bc02e2> 00000000  00bdff58  00bd3be4  00bcc7cc  00000000  00000000  00bcf648

00bdfee0:<00bc0ab8> 0000002f  00bdff00 <00bcc7d8> 00bcc804  00000000  00000000  00000000

00bdff00: 00bdff14 <00bc7f88> 00000003  00bdff58  00000000  00000000 <02d15e20> 00bcc804

00bdff20: 02d5d7bc  00000000  00000000  02a2e129  02f6dff1  0027a270  00bc015c  00000000

00bdff40: 00000000  00bcc7cc  00bcc7de  00000000  02f6dff6  00000003  00bdff82  00bdff8b

00bdff60: 00bdff8e  00000000  00bdff98  00bdffa3  00bdffcb  00bdffdf  00bdffe5  00000000

00bdff80: 6d750000  746e756f  2d003230  642f0044  732f7665  00316264  4d524554  6e696c3d

00bdffa0: 50007875  3d485441  6e69622f  73752f3a  69622f72  732f3a6e  3a6e6962  7273752f

00bdffc0: 6962732f  622f3a6e  48006e69  5f485355  53524556  3d4e4f49  35312e31  5000322e

00bdffe0: 2f3d4457  504d5400  6d742f3d  622f0070  752f6e69  6e756f6d  00323074  00000000

Return addresses in stack:

   frame  1 : <0x00bc5326> [ umount02 + 0x52e6 ]

   frame  2 : <0x00bc4a4e> [ umount02 + 0x4a0e ]

   frame  3 : <0x00bc49c4> [ umount02 + 0x4984 ]

   frame  4 : <0x00bc2c3a> [ umount02 + 0x2bfa ]

    address : <0x00bc4f42> [ umount02 + 0x4f02 ]

    address : <0x00bc50c6> [ umount02 + 0x5086 ]

    address : <0x00bc8478> [ umount02 + 0x8438 ]

    address : <0x00bc4a4e> [ umount02 + 0x4a0e ]

    address : <0x00bc67d0> [ umount02 + 0x6790 ]

    address : <0x00bc67e4> [ umount02 + 0x67a4 ]

    address : <0x00bc656e> [ umount02 + 0x652e ]

    address : <0x00bc31f0> [ umount02 + 0x31b0 ]

    address : <0x00bc330a> [ umount02 + 0x32ca ]

    address : <0x00bc6738> [ umount02 + 0x66f8 ]

    address : <0x00bc8984> [ umount02 + 0x8944 ]

    address : <0x00bc5000> [ umount02 + 0x4fc0 ]

    address : <0x00bc533e> [ umount02 + 0x52fe ]

    address : <0x00bc2fa2> [ umount02 + 0x2f62 ]

    address : <0x00bc4a4e> [ umount02 + 0x4a0e ]

    address : <0x00bc659e> [ umount02 + 0x655e ]

    address : <0x00bc0f4e> [ umount02 + 0xf0e ]

    address : <0x00bc15ea> [ umount02 + 0x15aa ]

   frame  5 : <0x00bc05dc> [ umount02 + 0x59c ]

    address : <0x00bcca9c> [ umount02 + 0xca9c ]

    address : <0x00bc0986> [ umount02 + 0x946 ]

   frame  6 : <0x00bc02e2> [ umount02 + 0x2a2 ]

    address : <0x00bc0ab8> [ umount02 + 0xa78 ]

    address : <0x00bcc7d8> [ umount02 + 0xc798 ]

   frame  7 : <0x00bc7f88> [ umount02 + 0x7f48 ]

   frame  8 : <0x02d15e20> [ sh + 0x15e20 ]

umount02    1  BROK  :  Unexpected signal 11 received.

umount02    2  BROK  :  Remaining cases broken

umount02    3  BROK  :  Remaining cases broken

umount02    4  BROK  :  Remaining cases broken

umount02    5  BROK  :  Remaining cases broken

--

Follow-ups

--- Graf Yang                                                2009-11-11 04:40:24

Patch the attached patch for umount02.c, test passed,

root:/ltp> ./umount02 -D /dev/sda1

EXT2-fs warning: mounting unchecked fs, running e2fsck is recommended

umount02    1  PASS  :  umount(2) expected failure; Got errno - EBUSY : Already

mounted/busy

umount02    2  PASS  :  umount(2) expected failure; Got errno - EFAULT :

Invalid address space

umount02    3  PASS  :  umount(2) expected failure; Got errno - ENOENT :

Directory not found

umount02    4  PASS  :  umount(2) expected failure; Got errno - EINVAL :

Invalid  device

umount02    5  PASS  :  umount(2) expected failure; Got errno - ENAMETOOLONG :

Pathname too long

--- Vivi Li                                                  2009-11-12 05:02:43

OK now.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

umount02.patch    application/octet-stream    705    Graf Yang

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.