Article [#5674] traps test 21 prefetch _l1_no fails on trunk head On bf548 and bf518 and bf527

[#5674] traps test 21 prefetch _l1_no fails on trunk head On bf548 and bf518 and bf527

Submitted By: Sonic Zhang

Open Date

2009-11-11 05:04:41     Close Date

2010-04-19 00:02:37

Priority:

Medium     Assignee:

Vivi Li

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

svn trunk

App binary format:

N/A     

Summary: traps test 21 prefetch _l1_no fails on trunk head On bf548 and bf518 and bf527

Details:

--- Mingquan Pan                                             2009-09-22 14:53:39

On bf548 ezkit and bf518f-ezkit, there is one more fail test 21. It is not found

failing on other boards.

Running test 19 for exception 0x00: prefetch l1_dataB^M

... PASS (test completed 1/1 times, as expected by signal 0: Unknown signal

0)^M

^M

Running test 20 for exception 0x00: prefetch l1_instruction^M

... FAIL (test exited sucessfully, and we expected 4 Illegal instruction

failure^M

FAIL (test completed properly 0/1 times)^M

^M

Running test 21 for exception 0x00: prefetch _l1_non^M

... FAIL (test failed, but not with the right signal)^M

        (We expected 0 'Unknown signal 0' but instead we got 11 'Segmentation

fault')^M

FAIL (test completed properly 0/1 times)^M

^M

--- Mingquan Pan                                             2009-10-16 16:25:18

It is strange that when the testing target board is switching to bf527 ezkit 0.2

on Sep 22, case 21 also fails. While this case used to be passed on bf527 ezkit

0.0.

Running test 21 for exception 0x00: prefetch _l1_non^M

... FAIL (test failed, but not with the right signal)^M

        (We expected 0 'Unknown signal 0' but instead we got 11 'Segmentation

fault')^M

FAIL (test completed properly 0/1 times)^M

The revision changes are:

failed revision: uclinux-dist   8880   linux 7402

passed revision: uclinux-dist   8871    linux 7391

Follow-ups

--- Mingquan Pan                                             2009-11-18 23:26:56

As we changes the toolchain from 09r1-10 4.1 toolchain to svn trunk head 4.3

toolchain (svn-3679), this case also fails when built into fdpic format.

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   bf537-2.6.31.5-ADI-2010R1-pre-sv

   Created:      2009-11-05  14:15:12 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3919038 Bytes =  3.7 MB

   Load Address: 00001000

   Entry Point:  0018d784

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 0018d784

Linux version 2.6.31.5-ADI-2010R1-pre-svn7752

(test@uclinux72-kernel-elf-ad1938) (gcc version 4.3.4 (ADI-trunk/svn-3679) ) #4

Thu Nov 5 22:15:06 CST 2009

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

...

unning test 19 for exception 0x00: prefetch l1_dataB

... PASS (test completed 1/1 times, as expected by signal 0: Unknown signal 0)

Running test 20 for exception 0x00: prefetch l1_instruction

... FAIL (test exited sucessfully, and we expected 4 Illegal instruction

failure

FAIL (test completed properly 0/1 times)

Running test 21 for exception 0x00: prefetch _l1_non

... FAIL (test failed, but not with the right signal)

        (We expected 0 'Unknown signal 0' but instead we got 4 'Illegal

instruction')

FAIL (test completed properly 0/1 times)

Running test 22 for exception 0x00: prefetch _sysmmr

... PASS (test completed 1/1 times, as expected by signal 0: Unknown signal 0)

--- Sonic Zhang                                              2010-04-16 05:49:00

As mentioned in bug 5468, Vivi please help to disable the prefetch tests in

traps tests.

--- Vivi Li                                                  2010-04-19 00:00:55

Traps test is passed now.

So close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.