Article [#5768] ping fails on bf518f-ezbrd 09r1.1 branch kernel after ifconfig

[#5768] ping fails on bf518f-ezbrd 09r1.1 branch kernel after ifconfig

Submitted By: Mingquan Pan

Open Date

2009-12-11 05:20:22     Close Date

2010-01-03 23:20:49

Priority:

Medium High     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2009R1-RC6     Release:

Category:

N/A     Board:

N/A

Processor:

BF518     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

09r1.1-rc2

App binary format:

N/A     

Summary: ping fails on bf518f-ezbrd 09r1.1 branch kernel after ifconfig

Details:

ping fails on bf518f-ezbrd 09r1.1 branch kernel after ifconfig. The default DSA config is off.

And in u-boot, the network is through.

-Boot 2008.10-svn2133 (ADI-2009R1.1-rc1) (Dec  3 2009 - 12:45:45)

CPU:   ADSP bf518-0.0 (Detected Rev: 0.1) (parallel flash boot)

Board: ADI BF518F EZ-Board board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 80 MHz

RAM:   64 MB

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

Net:   Blackfin EMAC

MAC:   00:E0:22:FE:66:9A

Hit any key to stop autoboot:  0

bfin>

bfin> tftp 0x2000000 uImage

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x2000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         ################################

done

Bytes transferred = 4278511 (4148ef hex)

bfin> bootm

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   Linux-2.6.28.10-ADI-2009R1.1-svn

   Created:      2009-12-11  10:40:15 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4278447 Bytes =  4.1 MB

   Load Address: 00001000

   Entry Point:  00180b70

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 00180b70

Linux version 2.6.28.10-ADI-2009R1.1-svn7960 (test@uclinux80-bf518f) (gcc version 4.1.2 (ADI svn)) #8 Fri Dec 11 18:40:05 CST 2009

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00102ec0

  rodata    = 0x00102ec0-0x00151a14

  bss       = 0x00152000-0x001627b4

  data      = 0x001627b4-0x00174000

    stack   = 0x00172000-0x00174000

  init      = 0x00174000-0x007af000

  available = 0x007af000-0x03eff000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF518 Rev 0.0

Warning: Compiled for Rev 0, but running on Rev 1

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 400 MHz core clock and 80 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

Data Cache Enabled for CPU0 (write-back)

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16001

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600

Configuring Blackfin Priority Driven Interrupts

PID hash table entries: 256 (order: 8, 1024 bytes)

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 56072k/65536k RAM, (6380k init code, 1031k kernel code, 453k data, 1024k dma, 572k reserved)

Calibrating delay loop... 796.67 BogoMIPS (lpj=1593344)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (15 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

net_namespace: 288 bytes

NET: Registered protocol family 16

Blackfin DMA Controller

ezbrd_init(): registering device resources

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 109

io scheduler noop registered (default)

Serial: Blackfin serial driver

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=15)@sclk=80MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc03400, dma channel@5

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-05-31 04:43:53 UTC (1085978633)

Freeing unused kernel memory: 6380k freed

dma_alloc_init: dma_page @ 0x007ac000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.13.4 (2009-12-11 13:02:38 CST) built-in shell (msh)

Enter 'help' for a list of built-in commands.

root:/> ifconfig eth0 10.100.4.50

root:/> PHY: 0:01 - Link is Up - 100/Full

root:/> ifconfig

eth0      Link encap:Ethernet  HWaddr 00:E0:22:FE:66:9A

          inet addr:10.100.4.50  Bcast:10.255.255.255  Mask:255.0.0.0

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          UP LOOPBACK RUNNING  MTU:16436  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

root:/> ping 10.100.4.174

PING 10.100.4.174 (10.100.4.174): 56 data bytes

^C

--- 10.100.4.174 ping statistics ---

5 packets transmitted, 0 packets received, 100% packet loss

Follow-ups

--- Graf Yang                                                2009-12-15 04:26:32

The RXERR(PG1) pin on the old BF518-ezbrd(REV 0.1) is also not used by KSZ

switch. So there is a hardware workaround on this board, which pulled down this

pin by a 1K resister.

The new board(REV 1.0) not have this workaround, so this bug existed.

Mike afforded a software workaround which disabled the PG1's peripheral

function.

This workaround also works for old board.

I think we need add the hardware workaround to the new board as the old board

did.

--- Mingquan Pan                                             2010-01-03 23:20:14

It pings ok now on this bf518 board after applying the hareware workaround. So

close.

--- Graf Yang                                                2010-03-04 21:26:09

The pin PG1/MII RXER (I have a typo error in my previous comment) should be

pulled to low.

This pin is named ERXER on the schedmatic.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.