Article [#5771] gadget zero control may hang at test 14 in bf548-ezkit

[#5771] gadget zero control may hang at test 14 in bf548-ezkit

Submitted By: Vivi Li

Open Date

2009-12-14 05:30:20     Close Date

2010-11-08 22:57:30

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2009R1-RC6     Release:

Category:

Tests     Board:

EZKIT Lite

Processor:

BF548     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Out of Date

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_09r1.1-2

App binary format:

N/A     

Summary: gadget zero control may hang at test 14 in bf548-ezkit

Details:

Gadget test in bf548-ezkit is not as stable as in bf527-ezkit.

For example, gadget_zero test may fail at test 14 occasionally, and it's hard to reproduce.

bf527-ezkit has better result and gadget test always pass.

Trunk and 09r1 branch has the same problem.

--

sudo ./src/testusb -D /proc/bus/usb/0 ^M02/120 -t14 -c 15000 -s 256 -v 1^M

unknown speed   /proc/bus/usb/002/120^M

/proc/bus/usb/002/120 test 14,    3.824969 secs^M

timeout: testusb t14

--

Follow-ups

--- Cliff Cai                                                2009-12-14 23:38:26

mm,it seems that the workaround provided by hardware guys is not stable on

BF54x.

Cliff

--- Sonic Zhang                                              2010-06-29 04:16:05

Bob needs to send email about the issue of the workaround to hardware supporting

engineer at processor.support@analog.com.

--- Bob Liu                                                  2010-07-07 00:07:13

Updated Host OS's kernel from 2.6.25 to 2.6.31.

This bug disappeared.

--- Vivi Li                                                  2010-11-08 22:57:30

Update kernel and can't see this bug now.

So close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.