Article [#5780] bfin-dma test fails on BF518F-ezbrd with 0.1 silicon revision

[#5780] bfin-dma test fails on BF518F-ezbrd with 0.1 silicon revision

Submitted By: Vivi Li

Open Date

2009-12-16 22:13:42     Close Date

2009-12-20 21:51:00

Priority:

Medium High     Assignee:

Graf Yang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

Tests     Board:

N/A

Processor:

BF518     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.1_09r1.1-rc2

App binary format:

N/A     

Summary: bfin-dma test fails on BF518F-ezbrd with 0.1 silicon revision

Details:

bfin-dma test fails on BF519F-ezbrd with 1.0 board revision and 0.1 silicon revision.

--

Linux version 2.6.28.10-ADI-2009R1.1-svn8032 (test@uclinux80-bf518f) (gcc version 4.1.2 (ADI svn)) #4 Thu Dec 17 04:04:07 CST 2009^M

bootconsole [early_shadow0] enabled^M

bootconsole [early_BFuart0] enabled^M

early printk enabled on early_BFuart0^M

Board Memory: 64MB^M

Kernel Managed Memory: 64MB^M

Memory map:^M

  fixedcode = 0x00000400-0x00000490^M

  text      = 0x00001000-0x00104180^M

  rodata    = 0x00104180-0x00153728^M

  bss       = 0x00154000-0x001647c0^M

  data      = 0x001647c0-0x00176000^M

    stack   = 0x00174000-0x00176000^M

  init      = 0x00176000-0x006f4000^M

  available = 0x006f4000-0x03eff000^M

  DMA Zone  = 0x03f00000-0x04000000^M

Hardware Trace Active and Enabled^M

Boot Mode: 1^M

Blackfin support (C) 2004-2009 Analog Devices, Inc.^M

Compiled for ADSP-BF518 Rev 0.1^M

Blackfin Linux support by http://blackfin.uclinux.org/^M

Processor Speed: 400 MHz core clock and 80 MHz System Clock^M

NOMPU: setting up cplb tables^M

Instruction Cache Enabled for CPU0^M

Data Cache Enabled for CPU0 (write-back)^M

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16001^M

Kernel command line: root=/dev/mtdblock0 rw earlyprintk=serial,uart0,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf518f-ezbrd:eth0:off^M

Configuring Blackfin Priority Driven Interrupts^M

PID hash table entries: 256 (order: 8, 1024 bytes)^M

console [ttyBF0] enabled, bootconsole disabled^M

console [ttyBF0] enabled, bootconsole disabled^M

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)^M

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)^M

Memory available: 56820k/65536k RAM, (5624k init code, 1036k kernel code, 456k data, 1024k dma, 572k reserved)^M

Calibrating delay loop... 796.67 BogoMIPS (lpj=1593344)^M

Security Framework initialized^M

Mount-cache hash table entries: 512^M

Blackfin Scratchpad data SRAM: 4 KB^M

Blackfin L1 Data A SRAM: 16 KB (15 KB free)^M

Blackfin L1 Data B SRAM: 16 KB (16 KB free)^M

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)^M

net_namespace: 288 bytes^M

NET: Registered protocol family 16^M

Blackfin DMA Controller^M

ezbrd_init(): registering device resources^M

NET: Registered protocol family 2^M

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)^M

TCP established hash table entries: 2048 (order: 2, 16384 bytes)^M

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)^M

TCP: Hash tables configured (established 2048 bind 2048)^M

TCP reno registered^M

NET: Registered protocol family 1^M

msgmni has been set to 110^M

io scheduler noop registered (default)^M

Serial: Blackfin serial driver^M

bfin-uart.1: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART^M

brd: module loaded^M

bfin_mii_bus: probed^M

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=15)@sclk=80MHz)^M

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1^M

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7^M

bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc03400, dma channel@5^M

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0^M

i2c /dev entries driver^M

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400^M

bfin-wdt: initialized: timeout=20 sec (nowayout=0)^M

TCP cubic registered^M

NET: Registered protocol family 17^M

rtc-bfin rtc-bfin: setting system clock to 2004-05-31 06:24:31 UTC (1085984671)^M

dma_alloc_init: dma_page @ 0x03b9f000 - 256 pages at 0x03f00000^M

IP-Config: Complete:^M

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,^M

     host=bf518f-ezbrd, domain=, nis-domain=(none),^M

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=^M

Freeing unused kernel memory: 5624k freed^M

PHY: 0:01 - Link is Up - 100/Full^M

                           _____________________________________^M

        a8888b.           / Welcome to the uClinux distribution \^M

       d888888b.         /       _     _                         \^M

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |^M

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |^M

       8'    .88       \        | |   | |  _ \| | | | \  /        |^M

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |^M

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |^M

     dP   .    Y8b.       \   For embedded processors including   |^M

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /^M

   d8"         'Y88b        \___________________________________/^M

  :8P    '      :888^M

   8a.   :     _a88P         For further information, check out:^M

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/^M

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/^M

/     \.___.d|    .'           - http://www.uclinux.org/^M

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin^M

^M

Have a lot of fun...^M

^M

^M

BusyBox v1.13.4 (2009-12-16 19:51:53 CST) built-in shell (msh)^M

Enter 'help' for a list of built-in commands.^M

^M

root:/> version^M

kernel:    Linux release 2.6.28.10-ADI-2009R1.1-svn8032, build #4 Thu Dec 17 04:04:07 CST 2009^M

toolchain: bfin-uclinux-gcc release gcc version 4.1.2 (ADI svn)^M

user-dist: release svn-9277, build #32 Thu Dec 17 04:03:29 CST 2009^M

root:/> successful boot attempt^M

root:/>

************** STEP 3: Start testing

bfin-dma^M

fd != -1: No such file or directory^M

root:/>

--

Follow-ups

--- Graf Yang                                                2009-12-17 03:57:42

I tried it on branch, it works fines.

It will print 'bfin-dma: initialized' when booting. But this text not existed

in your boot log.

Please check the test scripts.

--- Vivi Li                                                  2009-12-20 21:51:01

Test script is improved.

Test is pass now.

Close this bug.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.