Article [#5790] Cannot read flash under Linux

[#5790] Cannot read flash under Linux

Submitted By: Jie Zhang

Open Date

2009-12-23 22:59:44     Close Date

2009-12-24 03:34:06

Priority:

Medium     Assignee:

Barry Song

Status:

Closed     Fixed In Release:

N/A

Found In Release:

snaps     Release:

Category:

N/A     Board:

STAMP

Processor:

BF533     Silicon Revision:

0.3

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

Latest trunk     Toolchain version or rev.:

Latest trunk

App binary format:

N/A     

Summary: Cannot read flash under Linux

Details:

$ cat t.c

#include <stdio.h>

int main ()

{

  unsigned char *p = (unsigned char *) 0x20000000;

  printf ("0x20000000: %02x %02x %02x %02x\n", p[0], p[1], p[2], p[3]);

  return 0;

}

$ bfin-uclinux-gcc -o t t.c

Then run t under Linux on bf533-stamp, the output is not expected. Just random values.

The expected result, as on bf537-stamp, is

root:/> ./t                                                                    

0x20000000: 0e e1 ec 0f                                                        

root:/>

Follow-ups

--- Barry Song                                               2009-12-24 01:47:21

not a bug for 533 nor flash. 533 is sharing flash with network card. When kernel

access it, it need

static void switch_to_flash(struct async_state *state)

{

        local_irq_save(state->irq_flags);

        gpio_set_value(state->enet_flash_pin, 0);

        state->save_ambctl0 = bfin_read_EBIU_AMBCTL0();

        state->save_ambctl1 = bfin_read_EBIU_AMBCTL1();

        bfin_write_EBIU_AMBCTL0(state->flash_ambctl0);

        bfin_write_EBIU_AMBCTL1(state->flash_ambctl1);

        SSYNC();

}

After accessing, it will release:

static void switch_back(struct async_state *state)

{

        bfin_write_EBIU_AMBCTL0(state->save_ambctl0);

        bfin_write_EBIU_AMBCTL1(state->save_ambctl1);

        SSYNC();

        gpio_set_value(state->enet_flash_pin, 1);

        local_irq_restore(state->irq_flags);

}

Then you are accessing network card.

--- Jie Zhang                                                2009-12-24 02:23:24

Barry, Thanks. Is there a config option in linux kernel, so I can access flash

instead of network?

--- Barry Song                                               2009-12-24 03:13:35

No special option for it. But deleting "smc91x" and "mtd" in

kernel config will help you. That just keeps the gpio status unchanged.

1.

Ethernet (10 or 100Mbit)                                                      

                < >   SMC 91C9x/91C1xxx support  

2.

< > Memory Technology Device (MTD) support 

                                                        

--- Jie Zhang                                                2009-12-24 03:33:52

Thanks!

--- Mike Frysinger                                           2009-12-24 07:50:08

why dont you read flash via the /dev/mtd* devices like normal ?

--- Jie Zhang                                                2009-12-24 08:30:55

I found gdbproxy could not read flash. So I wrote this test case to mimic what

gdbproxy does.

--- Mike Frysinger                                           2009-12-24 08:40:22

then gdbproxy is behaving correctly and doesnt need changing.  it's up to the

user to make sure the board state is how they need it to be.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.