Article [#5805] load library like libosipparser2.so.4 sometimes fails on trunk head built by gcc 4.3

[#5805] load library like libosipparser2.so.4 sometimes fails on trunk head built by gcc 4.3

Submitted By: Mingquan Pan

Open Date

2010-01-03 23:45:04     Close Date

2010-12-28 21:59:40

Priority:

Medium High     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

4.3.4 (ADI-trunk/svn-3771)

App binary format:

N/A     

Summary: load library like libosipparser2.so.4 sometimes fails on trunk head built by gcc 4.3

Details:

load library like libosipparser2.so.4 sometimes fails on trunk head. This happens in linphone testing. For the first time loading, it can't find the library, while the second time to run linphone, it can find it then.

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf537-2.6.32.2-ADI-2010R1-pre-sv

   Created:      2010-01-03   8:06:55 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    5048510 Bytes =  4.8 MB

   Load Address: 00001000

   Entry Point:  001bf760

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001bf760

Linux version 2.6.32.2-ADI-2010R1-pre-svn8107 (test@uclinux56-ad73322-snormtd-df) (gcc version 4.3.4 (ADI-trunk/svn-3771) ) #24 Sun Jan 3 08:06:45 GMT 2010

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0012e5d0

  rodata    = 0x0012e5d0-0x0018fc70

  bss       = 0x00190000-0x001a178c

  data      = 0x001a178c-0x001b2000

    stack   = 0x001b2000-0x001b4000

  init      = 0x001b4000-0x009a9000

  available = 0x009a9000-0x03800000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 46884k/65536k RAM, (8148k init code, 1205k kernel code, 535k data, 2048k dma, 6716k reserved)

Hierarchical RCU implementation.

NR_IRQS:98

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (36 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 91

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

Advanced Linux Sound Architecture Driver Version 1.0.21.

dma_alloc_init: dma_page @ 0x02a0a000 - 512 pages at 0x03e00000

ALSA device list:

  #0: Analog Devices AD73322 at PF10 SPORT0,rx/tx dma ch:3/4,err irq:45

TCP cubic registered

NET: Registered protocol family 17

6IP-Config: Complete:tting system clock to 2004-05-31 10:38:33 UTC (1085999913)

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 8148k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - https://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.15.3 (2010-01-03 08:03:15 GMT) hush - the humble shell

root:/> PHY: 0:01 - Link is Up - 100/Full

root:/>

root:/> linphonec

linphonec:582: can't map '/usr/lib/libosipparser2.so.4'

linphonec:582: can't map '/usr/lib/libosipparser2.so.4'

linphonec: can't load library 'libosipparser2.so.4'

root:/> linphonec

NLS disabled.

ALSA lib /home/test/work/cruise/checkouts/uclinux-dist/lib/alsa-lib/alsa-lib-1.0.18/src/conf.c:3952:(snd_config_expand) Unknown parameters 0

ALSA lib /home/test/work/cruise/checkouts/uclinux-dist/lib/alsa-lib/alsa-lib-1.0.18/src/control/control.c:909:(snd_ctl_open_noupdate) Invalid CTL default:0

Ready

Warning: video is disabled in linphonec, use -V or -C or -D to enable.

linphonec>

test@uclinux56-ad73322-snormtd-df:..logs/2010_Jan_02_22_52>

This also sometimes happens to libgcc_s.so.1:

root:/> reboot

reboot:582: can't map '/lib/libgcc_s.so.1'

reboot:582: can't map '/lib/libgcc_s.so.1'

reboot:582: can't map '/lib/libgcc_s.so.1'

reboot: can't load library 'libgcc_s.so.1'

root:/>

root:/>                                                                                                                                                   

Follow-ups

--- Barry Song                                               2010-01-13 02:36:18

For those cases mapping/loading library fail, tracing log:

[kernel]

do_filp_open file:02beb4c0 filename:/usr/lib/libosipparser2.so.4

do_mmap2 file:02beb4c0 addr:00000000 pgoff:0 len:22b24 mmaped addr:01000000

prot:5 flags:2

[user]

linphonec:582: can't map '/usr/lib/libosipparser2.so.4'

[kernel]

do_filp_open file:02beb340 filename:/usr/lib/libosipparser2.so.4

do_mmap2 file:02beb340 addr:00000000 pgoff:0 len:22b24 mmaped addr:00980000

prot:5 flags:2

[user]

linphonec:582: can't map '/usr/lib/libosipparser2.so.4'

linphonec: can't load library 'libosipparser2.so.4'

For failure library, user will call sys_mmap2 to same offset twice, everytime

kernel will return success, but user print failure. For successful library, I

only saw one sys_mmap2 to a same offset.

Then need to trace ld to find the reason. Keep Jie in the loop too.

--- Barry Song                                               2010-01-13 03:15:31

A check-in in toolchain close to svn 3771 has caused this problem.

--- Vivi Li                                                  2010-01-15 02:24:58

Refer to bug [#5823], gcc4.3 svn 3679 is OK.

--- Mingquan Pan                                             2010-02-20 05:21:33

When testing feature reserve memory in fdpic kernel, it would fail to start at

init sometimes.

The kernel is quite normal and the only difference is the newly set bootargs in

u-boot.

U-Boot 2009.11.1-svn2233 (ADI-2010R1-pre) (Feb 08 2010 - 18:06:24)

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz

RAM:   64 MB

RAM size is 64 MB.

Flash:  4 MB

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   Blackfin EMAC

Hit any key to stop autoboot:  0

bfin> set bootargs root=/dev/mtdblock0 rw mem=32M max_mem=64M

console=ttyBF0,57600

bfin> set serverip 10.100.4.174

bfin> set ipaddr 10.100.4.50

bfin> save

Saving Environment to Flash...

. done

Un-Protected 1 sectors

Erasing Flash...

. done

Erased 1 sectors

Writing to Flash... done

. done

Protected 1 sectors

bfin>

bfin> tftpboot 0x2000000 uImage

Using Blackfin EMAC device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x2000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

done

Bytes transferred = 3806495 (3a151f hex)

Image size is 3a151f

bfin> run addip

bfin> bootm

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   bf537-2.6.32.8-ADI-2010R1-pre-sv

   Created:      2010-02-20   3:23:53 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    3806431 Bytes =  3.6 MB

   Load Address: 00001000

   Entry Point:  001997a4

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001997a4

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (36 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 1024 (order: 1, 8192 bytes)

TCP bind hash table entries: 1024 (order: 0, 4096 bytes)

TCP: Hash tables configured (established 1024 bind 1024)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 46

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs_base@ffc00500, dma channel@7

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1,

mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

IP-Config: Complete:etting system clock to 1970-04-18 12:07:59 UTC (9288479)

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 6020k freed

dma_alloc_init: dma_page @ 0x017cb000 - 256 pages at 0x01f00000

/init:582: can't map '/lib/libgcc_s.so.1'

/init:582: can't map '/lib/libgcc_s.so.1'

/init:582: can't map '/lib/libgcc_s.so.1'

/init: can't load library 'libgcc_s.so.1'

Kernel panic - not syncikernel panic detected... trying to recover from

ittest@uclinux72-

And in oprofile fdpic testing, it is also frequently see this issue:

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   bf537-2.6.32.8-ADI-2010R1-pre-sv

   Created:      2010-02-19  15:56:19 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    6579933 Bytes =  6.3 MB

   Load Address: 00001000

   Entry Point:  001f5974

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001f5974

Linux version 2.6.32.8-ADI-2010R1-pre-svn8323

(test@uclinux72-kernel-elf-ad1938) (gcc version 4.3.4 (ADI-trunk/svn-3815) )

#178 Fri Feb 19 23:56:14 CST 2010

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00131b80

  rodata    = 0x00131b80-0x0019d8b0

  bss       = 0x0019e000-0x001d2044

  data      = 0x001d2060-0x001ea000

    stack   = 0x001e8000-0x001ea000

  init      = 0x001ea000-0x00cfd000

  available = 0x00cfd000-0x03800000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50

earlyprintk=serial,uart0,57600 console=ttyBF0,57600

ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf537-stamp:eth0:off

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 43476k/65536k RAM, (11340k init code, 1218k kernel code, 738k

data, 1024k dma, 7740k reserved)

Hierarchical RCU implementation.

NR_IRQS:130

Configuring Blackfin Priority Driven Interrupts

bfin-rtc: invalid date; resetting

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 997.37 BogoMIPS (lpj=1994752)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (36 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

msgmni has been set to 84

io scheduler noop registered

io scheduler anticipatory registered (default)

io scheduler cfq registered

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs_base@ffc00500, dma channel@7

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1,

mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

oprofile: using timer interrupt.

TCP cubic registered

NET: Registered protocol family 17

IP-Config: Complete:etting system clock to 1970-01-01 08:54:50 UTC (32090)

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 11340k freed

dma_alloc_init: dma_page @ 0x029ea000 - 256 pages at 0x03f00000

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - https://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.15.3 (2010-02-19 23:53:32 CST) hush - the humble shell

root:/> version

kernel:    Linux release 2.6.32.8-ADI-2010R1-pre-svn8323, build #178 Fri Feb 19

23:56:14 CST 2010PHY: 0:01 - Link is Up - 100/Full

toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.4

(ADI-trunk/svn-3815)

user-dist: release svn-9458, build #3721 Fri Feb 19 23:55:19 CST 2010

root:/> successful boot attempt

************** STEP 3: Start oprofile kernel test

/usr/bin/bfin_opcontrol --init

mkdir: cannot create directory '/var/lib/': File exists

root:/>

Case 1 ...PASS

Case 1 ...PASS

/usr/bin/bfin_opcontrol --start-daemon &

[1] 165 /usr/bin/bfin_opcontrol --start-daemon

root:/> ./oprofiled:582: can't map '/lib/libgcc_s.so.1'

./oprofiled:582: can't map '/lib/libgcc_s.so.1'

./oprofiled:582: can't map '/lib/libgcc_s.so.1'

./oprofiled: can't load library 'libgcc_s.so.1'

--- Mingquan Pan                                             2010-02-20 22:04:44

In reserve memory testing, after set bootargs to reserve the 32M memory, it also

need to run addip, which makes this bug reproduce almost everytime.

version:

kernel:    Linux release 2.6.32.8-ADI-2010R1-pre-svn8325, build #182 Sat Feb 20

11:23:46 CST 2010

toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.4

(ADI-trunk/svn-3815)

user-dist: release svn-9458, build #3774 Sat Feb 20 11:23:16 CST 2010

--- Sonic Zhang                                              2010-09-16 04:40:28

Fixed. Should check address range across the border of init section and generic

allocable memory properly.

refer to bug 6254.

--- Vivi Li                                                  2010-12-28 21:59:40

OK now. Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.linux.reserve_mem    application/octet-stream    35482    Mingquan Pan

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.