Article [#5814] PREEMPT_RT: cyclic test shows no significant improvement for system latency

[#5814] PREEMPT_RT: cyclic test shows no significant improvement for system latency

Submitted By: Yi Li

Open Date

2010-01-05 05:30:09     Close Date

2010-04-16 06:06:05

Priority:

Low     Assignee:

Cliff Cai

Status:

Closed     Fixed In Release:

N/A

Found In Release:

snaps     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

2009R1-rc10

App binary format:

N/A     

Summary: PREEMPT_RT: cyclic test shows no significant improvement for system latency

Details:

Using the cyclic test (http://rt.wiki.kernel.org/index.php/Cyclictest) to test system latency (irq + schedule), enabling PREEMPT_RT shows no significant improvement over PREEPT_VOLUNTORY.

Here is the result (testing clock_nanosleep() latency) (all result is in microsecond (us)).

PREEMT_VOLUNTORY

-----------------

1. 100% CPU workload:

root:/> ./cyclictest -p 80 -t1 -n -i 10000 -l 10000

timer mode: 1

policy: fifo: loadavg: 5.13 4.19 2.14 6/41 453         

T: 0 (  405) P:80 I:10000 C:  10000 Min:     32 Act:   57 Avg:  104 Max:    6712

2. no workload:

root:/> ./cyclictest -p 80 -t1 -n -i 10000 -l 10000

timer mode: 1

policy: fifo: loadavg: 0.00 0.00 0.00 1/31 169         

T: 0 (  169) P:80 I:10000 C:  10000 Min:     24 Act:   35 Avg:   40 Max:     120

PREEMPT_RT

-----------

1. 100% CPU workload:

root:/> ./cyclictest -p 80 -t1 -n -i 10000 -l 10000

timer mode: 1

policy: fifo: loadavg: 4.55 1.68 0.61 6/48 237         

T: 0 (  205) P:80 I:10000 C:  10000 Min:     29 Act:   65 Avg:   87 Max:    6747

2. no workload:

root:/> ./cyclictest -p 80 -t1 -n -i 10000 -l 10000

timer mode: 1

policy: fifo: loadavg: 0.00 0.00 0.00 1/36 174         

T: 0 (  174) P:80 I:10000 C:  10000 Min:     24 Act:   31 Avg:   32 Max:      73

We need to find out why maxinum latency is as high as 6747 us when there is 100% workload.

kernel version:

blackfin_preempt_rt patch + patch-2.6.31.6-rt19 + svn trunk linux kernel r7915.

Follow-ups

--- Yi Li                                                    2010-01-05 05:32:42

Attached kernel configuration and workload script. Cyclic test is using

rttest-0.6.

--- Yi Li                                                    2010-01-05 23:45:49

Compared similar test with xenomai (on 2009R1.1). The max latency in xenomai

case is much better (48 us VS. 6747 us).

100% workload:

root:/usr/bin> ./cyclictest -p 80 -n -t1 -i 10000 -l 10000

4.86 2.46 0.97 6/33 419         

T: 0 (  335) P:80 I:   10000 C:   10000 Min:      22 Act:      34 Avg:      34

Max:      48

--- Yi Li                                                    2010-01-26 04:56:50

I use wakeup-rt tracer on kernel with PREEMPT_VOLUNTORY, result shows even for

tasks with real-time priority, the wake up latency is more than 7000 us.

root:/> cat /sys/kernel/debug/tracing/trace                

# tracer: wakeup_rt

#

# wakeup_rt latency trace v1.1.5 on 2.6.32.5-ADI-2010R1-pre-svn8224

# --------------------------------------------------------------------

# latency: 7651 us, #4/4, CPU#0 | (M:desktop VP:0, KP:0, SP:0 HP:0)

#    -----------------

#    | task: -478 (uid:0 nice:0 policy:1 rt_prio:80)

#    -----------------

#

#                  _------=> CPU#           

#                 / _-----=> irqs-off       

#                | / _----=> need-resched   

#                || / _---=> hardirq/softirq

#                ||| / _--=> preempt-depth  

#                |||| /_--=> lock-depth      

#                |||||/     delay            

#  cmd     pid   |||||| time  |   caller     

#     \   /      ||||||   \   |   /          

      ls-493     0d.h..    6us+:    493:120:R   + [000]   478: 19:S cyclictest

      ls-493     0d.h..   21us!: _wake_up_process <-_hrtimer_wakeup

      ls-493     0d.... 7636us+: _schedule <-_system_call

      ls-493     0d.... 7643us :    493:120:R ==> [000]   478: 19:R

cyclictest

After detailed analysis, I think the main cause is still that, kernel cannot be

preempted when return from interrupt to kernel space. See attached trace log.

--- Yi Li                                                    2010-01-27 03:33:15

Some system call (e.g do_exec()) will task a very long time (e.g,

load_flat_binary() may take 50ms, when executing "ls" with FLAT

format).

It is interesting that using FDPIC format, cyclic test gives much lower maximum

latency.

PREEMT_VOLUNTORY

-----------------

100% CPU workload:

root:/> ./cyclictest -p 80 -t 1 -n -l 10000 -i 10000         

timer mode: 1

policy: fifo: loadavg: 5.03 4.09 2.08 6/30 425         

T: 0 (  378) P:80 I:10000 C:  10000 Min:     37 Act:  106 Avg:   96 Max:   

323

--- Yi Li                                                    2010-04-08 01:03:28

The cause is: kernel spends a lot of time in do_execve()→load_flat_binary(),

without any chance to call “schedule()”, until do_execve() system call

finally finished (i.e, return to user space). So the wake-up latency happens

because kernel cannot be preempted.

For details, please refer to:

http://docs.blackfin.uclinux.org/doku.php?id=linux-kernel:ftrace

This bug is kind of depends on task 5718

(https://blackfin.uclinux.org/gf/project/uclinux-dist/tracker/?action=TrackerItemEdit&tracker_id=328&tracker_item_id=5718),

if kernel can be preempted when returning from interrupt.

--- Sonic Zhang                                              2010-04-16 06:04:25

Not a real bug. It depends on task 5718. Low priority.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

trace.log    text/x-log    18113    Yi Li

fork_workload.sh    application/x-sh    194    Yi Li

bugreport.tar.gz    application/x-gzip    19216    Yi Li

Attachments:
https://ez.analog.com/cfs-file/__key/articles/092bf6fcd847424ea8c4529b7fce36d1-a-bb9a55306da54c64b22ff14621ed3d87/fork_5F00_workload.sh

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.