Article [#5844] Gadget serial dirver test fail when transfer a file

[#5844] Gadget serial dirver test fail when transfer a file

Submitted By: Vivi Li

Open Date

2010-01-21 22:11:53     Close Date

2010-11-16 07:14:30

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3_trunk3771

App binary format:

N/A     

Summary: Gadget serial dirver test fail when transfer a file

Details:

When Gadget Serial dirver talk with Serial Driver talk on Linux host PC, file with lots of characters can not be transferred correctly.

This happens between BF548-EZKIT/BF527-EZKIT and Generic USB Serial Driver on host PC.

It also happens between BF527-EZKIT and Linux ACM driver on host PC.

--

Linux version 2.6.32.4-ADI-2010R1-pre-svn8215 (test@uclinux62-548-usbdev) (gcc version 4.3.4 (ADI-trunk/svn-3771) ) #116 Fri Jan 22 03:04:47 CST 2010

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart1] enabled

early printk enabled on early_BFuart1

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0019c2e0

  rodata    = 0x0019c2e0-0x00232bfc

  bss       = 0x00233000-0x002477f4

  data      = 0x002477f4-0x00264000

    stack   = 0x00262000-0x00264000

  init      = 0x00264000-0x009df000

  available = 0x009df000-0x03e00000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Reset caused by Software reset

Blackfin support (C) 2004-2009 Analog Devices, Inc.

Compiled for ADSP-BF548 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

  L2 SRAM        : uncacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-through) in data cache

  L2 SRAM        : uncacheable in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15748

Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart1,57600 console=ttyBF1,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf548-ezkit:eth0:off

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 52812k/65536k RAM, (7660k init code, 1644k kernel code, 800k data, 2048k dma, 572k reserved)

Hierarchical RCU implementation.

NR_IRQS:295

Configuring Blackfin Priority Driven Interrupts

console [ttyBF1] enabled, bootconsole disabled

console [ttyBF1] enabled, bootconsole disabled

Calibrating delay loop... 1046.52 BogoMIPS (lpj=2093056)

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

Blackfin L2 SRAM: 128 KB (128 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

bio: create slab <bio-0> at 0

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Switching to clocksource jiffies

musb_hdrc: version 6.0, musb-dma, peripheral, debug=0

musb_hdrc: USB Peripheral mode controller at ffc03c00 using DMA, IRQ 82

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

NET: Registered protocol family 1

Slow work thread pool: Starting up

Slow work thread pool: Ready

msgmni has been set to 103

io scheduler noop registered

io scheduler anticipatory registered (default)

bf54x-lq043: FrameBuffer initializing...

dma_alloc_init: dma_page @ 0x029dd000 - 512 pages at 0x03e00000

bfin-otp: initialized

bfin-uart: Blackfin serial driver

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 48) is a BFIN-UART

brd: module loaded

register bfin atapi driver

scsi0 : pata-bf54x

ata1: PATA max UDMA/66 irq 68

physmap platform flash device: 02000000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Using buffer write method

Using auto-unlock on power-up/resume

cfi_cmdset_0001: Erase suspend on write enabled

RedBoot partition parsing not available

Using physmap partition information

Creating 3 MTD partitions on "physmap-flash.0":

0x000000000000-0x000000040000 : "bootloader(nor)"

0x000000040000-0x000000440000 : "linux kernel(nor)"

0x000000440000-0x000001000000 : "file system(nor)"

BF5xx on-chip NAND FLash Controller Driver, Version 1.2 (c) 2007 Analog Devices, Inc.

bf5xx-nand bf5xx-nand.0: page_size=256, data_width=8, wr_dly=3, rd_dly=3

NAND device: Manufacturer ID: 0x20, Chip ID: 0xda (ST Micro NAND 256MiB 3,3V 8-bit)

Creating 2 MTD partitions on "NAND 256MiB 3,3V 8-bit":

0x000000000000-0x000000400000 : "linux kernel(nand)"

0x000000400000-0x000010000000 : "file system(nand)"

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x000000000000-0x000000040000 : "bootloader(spi)"

ata1.00: ATA-7: FUJITSU MHW2040AT, 0000000B, max UDMA/100

ata1.00: 78140160 sectors, multi 16: LBA

0x000000040000-0x000000200000 : "linux kernel(spi)"

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@4

bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc02300, dma channel@5

ata1.00: configured for UDMA/66

blk_queue_max_hw_segments: set to minimum 1

scsi 0:0:0:0: Direct-Access     ATA      FUJITSU MHW2040A 0000 PQ: 0 ANSI: 5

smsc911x: Driver version 2008-10-21.

smsc911x-mdio: probed

eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1)

net eth0: MAC Address: 00:e0:22:fe:bd:09

sd 0:0:0:0: [sda] 78140160 512-byte logical blocks: (40.0 GB/37.2 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

Initializing USB Mass Storage driver...

sda:

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

input: bf54x-keys as /devices/platform/bf54x-keys/input/input0

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc00700

i2c-bfin-twi i2c-bfin-twi.1: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc02200

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

bfin-sdh bfin-sdh.0: unable to request DMA channel

bfin-sdh: probe of bfin-sdh.0 failed with error -16

usbcore: registered new interface driver usbhid

usbhid: v2.6:USB HID core driver

Advanced Linux Sound Architecture Driver Version 1.0.21.

dma rx:0 tx:1, err irq:10, regs:ffc00800

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2005-02-17 04:02:41 UTC (1108612961)

sda1

sd 0:0:0:0: [sda] Attached SCSI disk

net eth0: SMSC911x/921x identified at 0x24000000, IRQ: 175

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf548-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 7660k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - https://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.15.3 (2010-01-22 01:24:58 CST) hush - the humble shell

root:/> version

kernel:    Linux release 2.6.32.4-ADI-2010R1-pre-svn8215, build #116 Fri Jan 22 03:04:47 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3771)

user-dist: release svn-9405, build #90 Fri Jan 22 03:03:55 CST 2010

root:/> ifconfig eth0 10.100.4.50

root:/>

root:/> modprobe g_serial use_acm=0

g_serial gadget: Gadget Serial v2.4

g_serial gadget: g_serial ready

root:/> g_serial gadget: high speed config #1: Generic Serial config

root:/> dmesg|tail

sd 0:0:0:0: [sda] Attached SCSI disk

net eth0: SMSC911x/921x identified at 0x24000000, IRQ: 175

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf548-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 7660k freed

g_serial gadget: Gadget Serial v2.4

g_serial gadget: g_serial ready

g_serial gadget: high speed config #1: Generic Serial config

root:/>

spawn /bin/bash

su

test@uclinux62-548-usbdev:..testsuites/usbdev> su

Password:

uclinux62-548-usbdev:..testsuites/usbdev #

sudo mount -t usbfs none /proc/bus/usb/

uclinux62-548-usbdev:..testsuites/usbdev #

uclinux62-548-usbdev:..testsuites/usbdev # cat /proc/bus/usb/devices|grep -i gad get

S:  Product=Gadget Serial v2.4

uclinux62-548-usbdev:..testsuites/usbdev # sudo modprobe usbserial vendor=0x0525  product=0xA4A6

uclinux62-548-usbdev:..testsuites/usbdev # lsmod |grep usbserial

usbserial              51120  0

usbcore               164684  9 usbserial,usb_storage,cdc_acm,cdc_ether,usbnet,usbhid,ehci_hcd,uhci_hcd

uclinux62-548-usbdev:..testsuites/usbdev # stty -F /dev/ttyUSB0 -icrnl

uclinux62-548-usbdev:..testsuites/usbdev # cat /dev/ttyUSB0 > host_file

root:/> cat /proc/kallsyms > test_file

root:/> cat test_file > /dev/ttyGS0

root:/>

uclinux62-548-usbdev:..testsuites/usbdev # rcp root@10.100.4.50:/test_file .

uclinux62-548-usbdev:..testsuites/usbdev # dos2unix host_file

dos2unix: converting file host_file to UNIX format ...

uclinux62-548-usbdev:..testsuites/usbdev # diff test_file host_file

6c6

< 000012e8 T _name_to_dev_t

---

> 000012e8 T _name_to_dev_t0

9c9

< 00001510 T _flush_thread

---

> ^00001510 T _flush_thread

16c16

< 00001934 T _bfin_clone

---

> 00001934 T _bfin_clone0

26c26

< 00001af8 T _syscall_trace

---

> 00001af8 T _syscall_trace^

36c36

< 0000274c t _setup_rt_frame

---

> 0000274c t _setup_rt_frame0

45c45

< 00003d14 T _bfin_request_exception

---

> 00003d14 T _bfin_request_exception^

54c54

< 00004a54 T _show_stack

---

> 00004a54 T _show_stack0

63c63

< 00005710 T ___dma_sync

---

> ^00005710 T ___dma_sync

71c71

< 00005b00 W _native_machine_restart

---

> 00005b00 W _native_machine_restart0

79c79

< 00005c08 T _portmux_setup

---

> 00005c08^ T _portmux_setup

...

--

Follow-ups

--- Bob Liu                                                  2010-09-01 23:09:19

fixed.

The issue is that the serial communication maybe do some addition action due to

some special ASCII words. So we must use serial tools to test it instead of

simple 'cat file> /dev/ttyGS0'.

The detail test process is like this:

1. config "lrz,lsz,login,getty" support on user config(I attached the

config file).

2. on device:

root:/> modprobe g_serial use_acm=0

root:/> getty 9600 /dev/ttyGS0

3. on host,open another minicom use minicom /dev/ttyUSB0 and config baud to

9600.

your need to enter username: root

and on the device console input passwd: uClinux

then use this minicom's zmodem to transfer file and compare the result.

--- Vivi Li                                                  2010-11-16 07:14:30

Fixed in testsuites.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

user.config    text/plain    49703    Bob Liu

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.