Article [#5851] device nodes are not created as soon as they are use to be

[#5851] device nodes are not created as soon as they are use to be

Submitted By: Vivi Li

Open Date

2010-01-26 23:31:23     Close Date

2010-03-29 02:57:27

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

Drivers     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3_trunk3771

App binary format:

N/A     

Summary: device nodes are not created as soon as they are use to be

Details:

Frame buffer device is not created immediately after LCD driver is installed. The first time to run video_test will fail and after that it works.

This happens on bf537/bf548/bf527.

The similar problem happens with usb device.

It does not mean that the device not can not be created. We need to wait some seconds before it is ready to use.

--

root:/> modprobe bf537-lq035

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

root:/> video_test

Unable to open frame buffer device /dev/fb0: No such file or directory

root:/>

--

Last passed version:

--

kernel:    Linux release 2.6.32.3-ADI-2010R1-pre-svn8141, build #32 Wed Jan 13 02:04:16 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3771)

user-dist: release svn-9368, build #323 Wed Jan 13 02:03:25 CST 2010

--

First failed version:

--

kernel:    Linux release 2.6.32.3-ADI-2010R1-pre-svn8151, build #36 Thu Jan 14 22:35:21 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3771)

user-dist: release svn-9376, build #412 Thu Jan 14 22:34:33 CST 2010

--

Follow-ups

--- Mike Frysinger                                           2010-01-28 01:26:13

this is probably related to enabling mdev.seq support in mdev.  iirc, it delays

a little to make sure there arent more events coming.

--- Vivi Li                                                  2010-02-24 23:21:48

Yeah, I wait some time after installing module and it'll be fine then.

Workaround this in test scripts.

--- Sonic Zhang                                              2010-03-29 02:56:05

Expected behavior after enabled mdev.seq

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.tftlcd.landscape    application/octet-stream    35382    Vivi Li

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.