Article [#5920] mke2fs fails to create a valid file system

[#5920] mke2fs fails to create a valid file system

Submitted By: Vivi Li

Open Date

2010-02-22 04:02:05     Close Date

2010-07-28 23:24:20

Priority:

Medium High     Assignee:

Mike Frysinger

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

EZKIT Lite

Processor:

BF548     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2010_Jan_22

App binary format:

N/A     

Summary: mke2fs fails to create a valid file system

Details:

Sometimes it fails to format ext2 file system in mmc or hard disk on bf548-ezkit.

--

root:/> mke2fs /dev/mmcblk0p1

mke2fs 1.41.9 (22-Aug-2009)

ext2fs_check_if_mount: Can't check if filesystem is mounted due to missing mtab file while determining whether /dev/mmcblk0p1 is.

Filesystem label=

OS type: Linux

Block size=4096 (log=2)

Fragment size=4096 (log=2)

62080 inodes, 247998 blocks

12399 blocks (5.00%) reserved for the super user

First data block=0

Maximum filesystem blocks=255852544

8 block groups

32768 blocks per group, 32768 fragments per group

7760 inodes per group

Superblock backups stored on blocks:

        32768, 98304, 163840, 229376

Writing inode tables: done

Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 35 mounts or

180 days, whichever comes first.  Use tune2fs -c or -i to override.

root:/>

root:/> mke2fs /dev/mmcblk0p1

mke2fs 1.41.9 (22-Aug-2009)

ext2fs_check_if_mount: Can't check if filesystem is mounted due to missing mtab file while determining whether /dev/mmcblk0p1 is.

Filesystem label=

OS type: Linux

Block size=4096 (log=2)

Fragment size=4096 (log=2)

62080 inodes, 247998 blocks

12399 blocks (5.00%) reserved for the super user

First data block=0

Maximum filesystem blocks=255852544

8 block groups

32768 blocks per group, 32768 fragments per group

7760 inodes per group

Superblock backups stored on blocks:

        32768, 98304, 163840, 229376

Writing inode tables: done

Writing superblocks and filesystem accounting information:

Warning, had trouble writing out superblocks.done

This filesystem will be automatically checked every 25 mounts or

180 days, whichever comes first.  Use tune2fs -c or -i to override.

root:/>

--

--

root:/> mke2fs /dev/sda1

mke2fs 1.41.9 (22-Aug-2009)

ext2fs_check_if_mount: Can't check if filesystem is mounted due to missing mtab file while determining whether /dev/sda1 is moun.

Filesystem label=

OS type: Linux

Block size=4096 (log=2)

Fragment size=4096 (log=2)

502944 inodes, 2008117 blocks

100405 blocks (5.00%) reserved for the super user

First data block=0

Maximum filesystem blocks=2059403264

62 block groups

32768 blocks per group, 32768 fragments per group

8112 inodes per group

Superblock backups stored on blocks:

        32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632

Writing inode tables: done

Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 26 mounts or

180 days, whichever comes first.  Use tune2fs -c or -i to override.

root:/> mke2fs /dev/sda1

mke2fs 1.41.9 (22-Aug-2009)

ext2fs_check_if_mount: Can't check if filesystem is mounted due to missing mtab file while determining whether /dev/sda1 is moun.

Filesystem label=

OS type: Linux

Block size=4096 (log=2)

Fragment size=4096 (log=2)

502944 inodes, 2008117 blocks

100405 blocks (5.00%) reserved for the super user

First data block=0

Maximum filesystem blocks=2059403264

62 block groups

32768 blocks per group, 32768 fragments per group

8112 inodes per group

Superblock backups stored on blocks:

        32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632

Writing inode tables:  0/62

Could not write 8 blocks in inode table starting at 496: Attempt to write block from filesystem resulted in short write

root:/>

--

Last passed version:

--

kernel:    Linux release 2.6.32.8-ADI-2010R1-pre-svn8319, build #135 Thu Feb 18 09:14:54 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3815)

user-dist: release svn-9456, build #3461 Thu Feb 18 09:14:24 CST 2010

--

First failed version:

--

kernel:    Linux release 2.6.32.8-ADI-2010R1-pre-svn8323, build #139 Fri Feb 19 12:16:00 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.4 (ADI-trunk/svn-3815)

user-dist: release svn-9458, build #3553 Fri Feb 19 12:15:29 CST 2010

--

Follow-ups

--- Mike Frysinger                                           2010-02-22 14:33:20

i noticed this myself but havent had time to debug it.  the storage location

doesnt seem to matter because it fails even on a file.  exporting the hard drive

over USB gadget lets the PC format the disk drive just fine.

not sure when i'll get a chance to look as i wont be back in the US for ~2

weeks

--- Mike Frysinger                                           2010-06-04 02:07:58

can you try with e2fsprogs-1.4.12 (current in trunk) ?  it seems to work OK for

me now ...

i'm running this overnite to be sure:

while mke2fs -q /dev/sda1 ; do mount /dev/sda1 /mnt/ ; ls /mnt; umount /mnt;

done

--- Mike Frysinger                                           2010-06-04 13:25:16

ran it over nite without any problems on my bf548-ezkit

--- Vivi Li                                                  2010-07-28 23:24:20

It's OK in last two months. So close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.config.sdiommc    application/octet-stream    47909    Vivi Li

config.linux.sdiommc    application/octet-stream    44310    Vivi Li

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.