Article [#6215] Failed to probe AD7877 Touchscreen when test touchscreen over spi on bf527-ezkit-2.0(2010)

[#6215] Failed to probe AD7877 Touchscreen when test touchscreen over spi on bf527-ezkit-2.0

Submitted By: angelia wu

Open Date

2010-08-31 01:58:22     Close Date

2010-09-14 06:35:22

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1     Release:

Category:

N/A     Board:

EZKIT Lite

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

svn-4681

App binary format:

N/A     

Summary: Failed to probe AD7877 Touchscreen when test touchscreen over spi on bf527-ezkit-2.0

Details:

touchscreen over spi on board bf527-ezkit 2.0

Failed to probe AD7877 Touchscreen.

the log as follow.

bfin> run ramboot

Using bfin_mac device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         ########################################################

done

Bytes transferred = 4629987 (46a5e3 hex)

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf527-2.6.34.6-ADI-2010R1-pre-sv

   Created:      2010-08-31   5:47:30 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4629923 Bytes = 4.4 MiB

   Load Address: 00001000

   Entry Point:  002046ac

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 002046ac

Linux version 2.6.34.6-ADI-2010R1-pre-svn9117 (test@uclinux41) (gcc version 4.3.5 (ADI-trunk/svn-4681) ) #181 Tue Aug 31 13:47:24 CST 2010

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart1] enabled

early printk enabled on early_BFuart1

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00156008

  rodata    = 0x00156008-0x001cb990

  bss       = 0x001cc000-0x001e08bc

  data      = 0x001e08bc-0x001fa000

    stack   = 0x001f8000-0x001fa000

  init      = 0x001fa000-0x008c0000

  available = 0x008c0000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 600 MHz core clock and 50 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16002

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF1,57600 ip=10.100.4.50:10.100.4.174:f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 54984k/65536k RAM, (6936k init code, 1364k kernel code, 656k data, 1024k dma, 572k reserved)

Hierarchical RCU implementation.

NR_IRQS:159

Configuring Blackfin Priority Driven Interrupts

Console: colour dummy device 80x25

Linux version 2.6.34.6-ADI-2010R1-pre-svn9117 (test@uclinux41) (gcc version 4.3.5 (ADI-trunk/svn-4681) ) #181 Tue Aug 31 13:47:24 CST 2010

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart1] enabled

early printk enabled on early_BFuart1

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00156008

  rodata    = 0x00156008-0x001cb990

  bss       = 0x001cc000-0x001e08bc

  data      = 0x001e08bc-0x001fa000

    stack   = 0x001f8000-0x001fa000

  init      = 0x001fa000-0x008c0000

  available = 0x008c0000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 1

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 600 MHz core clock and 50 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16002

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart1,57600 console=tty0 console=ttyBF1,57600 ip=10.100.4.50:10.100.4.174:f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 54984k/65536k RAM, (6936k init code, 1364k kernel code, 656k data, 1024k dma, 572k reserved)

Hierarchical RCU implementation.

NR_IRQS:159

Configuring Blackfin Priority Driven Interrupts

Console: colour dummy device 80x25

console [tty0] enabled

console [ttyBF1] enabled, bootconsole disabled

console [ttyBF1] enabled, bootconsole disabled

Calibrating delay loop... 1196.03 BogoMIPS (lpj=2392064)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (42 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

bio: create slab <bio-0> at 0

SCSI subsystem initialized

spi spi0.2: Warning: SPI CPHA not set: Slave Select not under software control!

See Documentation/blackfin/bfin-spi-notes.txt

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

musb_hdrc: version 6.0, musb-dma, host, debug=0

musb_hdrc musb_hdrc.0: MUSB HDRC host driver

musb_hdrc musb_hdrc.0: new USB bus registered, assigned bus number 1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

musb_hdrc musb_hdrc.0: USB Host mode controller at ffc03800 using DMA, IRQ 59

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

msgmni has been set to 107

io scheduler noop registered

io scheduler cfq registered (default)

bfin-otp: initialized

bfin-uart: Blackfin serial driver

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

brd: module loaded

adp5520 0-0032: failed writing 0x80 to 0x00

adp5520 0-0032: failed to write

adp5520: probe of 0-0032 failed with error -1

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x000000000000-0x000000040000 : "bootloader(spi)"

0x000000040000-0x000000200000 : "linux kernel(spi)"

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:03, irq=-1, mdc_clk=2500000Hz(mdc_div=9)@sclk=50MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ad7877 spi0.2: Warning: SPI CPHA not set: Slave Select not under software control!

See Documentation/blackfin/bfin-spi-notes.txt

ad7877 spi0.2: spi0.2: Failed to probe AD7877 Touchscreen

ad7879 0-002c: Failed to write AD7879 Touchscreen

ad7879: probe of 0-002c failed with error -1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-05 20:15:05 UTC (418505)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf527-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

dma_alloc_init: dma_page @ 0x028d4000 - 256 pages at 0x03f00000

Freeing unused kernel memory: 6936k freed

PHY: 0:03 - Link is Up - 100/Full

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - https://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.16.2 (2010-08-31 12:05:51 CST) hush - the humble shell

root:/> e

echo        env         event_test  expr

root:/> event_test /dev/input/event0

evtest: No such file or directory

root:/>

Follow-ups

--- Bob Liu                                                  2010-09-06 03:03:03

On BF527-ezkit-v2.2 and BF537-stamp, it works well.

And every time I connectted one Oscilloscope probe to the DCLK on EVAL-ad7877eb

it works well aslo, so I think it's BF527-ezkit-v2.0's hardware problem.

--- angelia wu                                               2010-09-14 06:35:22

ok, i closed the bug.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

kernel.527_2.0_touchscreen.config    application/x-config    44479    angelia wu

user.527_2.0_touchscreen.config    application/x-config    48796    angelia wu

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.