Article [#6324] There is confict in sport emulate spi with spi flash card on board bf537-stamp when boot.(2010)

[#6324] There is confict in sport emulate spi with spi flash card on board bf537-stamp when boot.

Submitted By: angelia wu

Open Date

2010-11-01 03:44:15    

Priority:

Medium     Assignee:

Vivi Li

Scott Jiang

Status:

Open     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Blackfin Linux:2010R1

Category:

N/A     Board:

STAMP

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

2010RC4

App binary format:

N/A     

Summary: There is confict in sport emulate spi with spi flash card on board bf537-stamp when boot.

Details:

There is confict in sport emulate spi with spi flash card on board bf537-stamp when boot.

So the case "sport emulate spi with spi flash " can't be tested.

the log as follow.

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)

Board: ADI BF537 stamp board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 500 MHz, Core: 500 MHz, System: 62.500 MHz

RAM:   64 MiB

Flash: 4 MiB

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Using HDD IDE Mode

Bus 0: not available 

Net:   bfin_mac

Hit any key to stop autoboot:  0

bfin> run ramboot

Using bfin_mac device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x1000000

Loading: T #################################################################

         #################################################################

         #################################################################

         #################################################################

         #####################################################

done

Bytes transferred = 4585407 (45f7bf hex)

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf537-2.6.34.7-ADI-2010R1-svn929

   Created:      2010-11-01   6:35:42 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4585343 Bytes = 4.4 MiB

   Load Address: 00001000

   Entry Point:  001a5684

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001a5684

Linux version 2.6.34.7-ADI-2010R1-svn9290 (test@uclinux41) (gcc version 4.3.5 (ADI-2010R1-RC4) ) #204 Mon Nov 1 14:35:37 CST 2010

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00118260

  rodata    = 0x00118260-0x00176564

  bss       = 0x00177000-0x001874d0

  data      = 0x001874d0-0x0019a000

    stack   = 0x00198000-0x0019a000

  init      = 0x0019a000-0x00877000

  available = 0x00877000-0x03800000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 62 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 48108k/65536k RAM, (7028k init code, 1116k kernel code, 520k data, 1024k dma, 7740k reserved)

Hierarchical RCU implementation.

NR_IRQS:138

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 991.23 BogoMIPS (lpj=1982464)

Security Framework initialized

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (35 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

msgmni has been set to 93

io scheduler noop registered

io scheduler cfq registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin-sport-spi bfin-sport-spi.1: Emulate a SPI bus with via Blackfin SPORT, regs_base@ffc00800

pin group conflict! request pin 30 func 1 conflict with pin 31 func 0

bfin-sport-spi bfin-sport-spi.2: requesting peripherals failed

bfin-sport-spi: probe of bfin-sport-spi.2 failed with error -16

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=11)@sclk=62MHz)

bfin_mac bfin_mac.0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:45:14 UTC (2714)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

dma_alloc_init: dma_page @ 0x028da000 - 256 pages at 0x03f00000

Freeing unused kernel memory: 7028k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - https://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.16.2 (2010-11-01 14:19:29 CST) hush - the humble shell

root:/> PHY: 0:01 - Link is Up - 100/Full

root:/>

Follow-ups

--- Bob Liu                                                  2010-11-01 04:58:45

Must follow wiki to change file

linux-2.6.x/arch/blackfin/mach-bf537/boards/stamp.c for testing.

--- angelia wu                                               2010-11-04 03:07:50

I test it again according to  the description  as the above, but there is still

the problem.

--- Bob Liu                                                  2010-11-07 21:44:03

The conflict problem has been fixed by commit 9479.

But the spiflash seems still can't work.

--- Bob Liu                                                  2010-11-15 04:38:28

After using the correct cs pin, it works sometime.

I tested the spiflash using "modprobe m25p80; rmmod m25p80".

The first time it can't work but after that it works fine.

--- Bob Liu                                                  2010-11-16 06:06:27

The reason the spiflash can't work at the first time is that there is no sport

clock.

But if don't plug in the spiflash, the sport can provide clock correctly at the

first time modprobe.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.linux.sport_spiflash    application/octet-stream    35834    angelia wu

config.config.sport_spiflash    application/octet-stream    49215    angelia wu

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.