Article [#6342] ad1836 hangs while using sport1(2010)

[#6342] ad1836 hangs while using sport1

Submitted By: Bob Liu

Open Date

2010-11-17 02:32:45     Close Date

2010-11-17 03:13:26

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

STAMP

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Assigned (Not Start)

Uboot version or rev.:

    Toolchain version or rev.:

trunk

App binary format:

N/A     

Summary: ad1836 hangs while using sport1

Details:

During aplay test, ad1836 will hang while using sport1, but use sport0 it works fine.

root:/> arecord -t wav -c 1 -f S16_LE -r 44100 -d 5 wav

Recording WAVE 'wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Mono

root:/>

root:/> aplay 73322.wav

Playing WAVE '73322.wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Mono

^CAborted by signal Interrupt...

root:/> aplay 73322.wav

Playing WAVE '73322.wav' : Signed 16 bit Little Endian, Rate 8000 Hz, Mono

^CAborted by signal Interrupt...

root:/>

Follow-ups

--- Bob Liu                                                  2010-11-17 03:13:26

It's the board's hardware problem, I changed a board and aplay works fine.

So close this bug.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.