Article [#6412] SRAM allocation test fail as sram-alloc-test is updated(2010)

[#6412] SRAM allocation test fail as sram-alloc-test is updated

Submitted By: Vivi Li

Open Date

2010-12-20 22:05:19     Close Date

2011-01-20 01:14:55

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-trunk

App binary format:

N/A     

Summary: SRAM allocation test fail as sram-alloc-test is updated

Details:

SRAM allocation test fail as sram-alloc-test coverage is extended significantly since uclinux-dist svn revision 9999.

--

Linux version 2.6.36.2-ADI-2011R1-pre-svn9530 (test@uclinux59-kernel-perf) (gcc version 4.3.5 (ADI-trunk/svn-5013) ) #34 Sat Dec0

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00117e88

  rodata    = 0x00117e88-0x00174d9c

  bss       = 0x00175000-0x001856d0

  data      = 0x001856d0-0x00198000

    stack   = 0x00196000-0x00198000

  init      = 0x00198000-0x008ae000

  available = 0x008ae000-0x03800000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47888k/65536k RAM, (7256k init code, 1115k kernel code, 513k data, 1024k dma, 7740k reserved)

Hierarchical RCU implementation.

        RCU-based detection of stalled CPUs is disabled.

        Verbose stalled-CPUs detection is disabled.

NR_IRQS:138

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 993.28 BogoMIPS (lpj=1986560)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (35 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 93

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-12 10:30:39 UTC (988239)

dma_alloc_init: dma_page @ 0x028f5000 - 256 pages at 0x03f00000

Freeing unused kernel memory: 7256k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    tèe Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.17.4 (2010-12-18 10:19:16 GMT) hush - the humble shell

root:/> sram_alloc

Testing L1_INST_SRAM on cpu 0 ...

sram_alloc(1, L1_INST_SRAM) = 0xffa032b8: PASS

sram_free(0xffa032b8) = 0: PASS

sram_alloc(1, L1_INST_SRAM) = 0xffa032b8: PASS

sram_free(0xffa032b8) = 0: PASS

sram_free(0xffa032b8) = -1: PASS

sram_alloc(0x1000000, L1_INST_SRAM) = (nil): PASS

sram_alloc(<all>, L1_INST_SRAM) = <9042 allocs>: PASS

sram_free(<all>) = 0: PASS

sram_alloc(1, L1_INST_SRAM) = 0xffa032b8: PASS

sram_free(0xffa032b8) = 0: PASS

Testing L1_DATA_A_SRAM on cpu 0 ...

sram_alloc(1, L1_DATA_A_SRAM) = 0xff800000: PASS

sram_free(0xff800000) = 0: PASS

sram_alloc(1, L1_DATA_A_SRAM) = 0xff800000: PASS

sram_free(0xff800000) = 0: PASS

sram_free(0xff800000) = -1: PASS

sram_alloc(0x1000000, L1_DATA_A_SRAM) = (nil): PASS

sram_alloc(<all>, L1_DATA_A_SRAM) = <4096 allocs>: PASS

sram_free(<all>) = 0: PASS

sram_alloc(1, L1_DATA_A_SRAM) = 0xff800000: PASS

sram_free(0xff800000) = 0: PASS

Testing L1_DATA_B_SRAM on cpu 0 ...

sram_alloc(1, L1_DATA_B_SRAM) = 0xff900000: PASS

sram_free(0xff900000) = 0: PASS

sram_alloc(1, L1_DATA_B_SRAM) = 0xff900000: PASS

sram_free(0xff900000) = 0: PASS

sram_free(0xff900000) = -1: PASS

sram_alloc(0x1000000, L1_DATA_B_SRAM) = (nil): PASS

sram_alloc(<all>, L1_DATA_B_SRAM) = <4096 allocs>: PASS

sram_free(<all>) = 0: PASS

sram_alloc(1, L1_DATA_B_SRAM) = 0xff900000: PASS

sram_free(0xff900000) = 0: PASS

Testing L1_DATA_SRAM on cpu 0 ...

sram_alloc(1, L1_DATA_SRAM) = 0xff800000: PASS

sram_free(0xff800000) = 0: PASS

sram_alloc(1, L1_DATA_SRAM) = 0xff800000: PASS

sram_free(0xff800000) = 0: PASS

sram_free(0xff800000) = -1: PASS

sram_alloc(0x1000000, L1_DATA_SRAM) = (nil): PASS

sram_alloc(<all>, L1_DATA_SRAM) = <8192 allocs>: PASS

sram_free(<all>) = 0: PASS

sram_alloc(1, L1_DATA_SRAM) = 0xff800000: PASS

sram_free(0xff800000) = 0: PASS

Testing L1_DATA_SRAM+A+B on cpu 0 ...

sram_alloc(1, L1_DATA_SRAM+A+B) = 0xff800000: PASS

sram_free(0xff800000) = 0: PASS

sram_alloc(1, L1_DATA_SRAM+A+B) = 0xff800000: PASS

sram_free(0xff800000) = 0: PASS

sram_free(0xff800000) = -1: PASS

sram_alloc(0x1000000, L1_DATA_SRAM+A+B) = (nil): PASS

sram_alloc(<all>, L1_DATA_SRAM+A+B) = <8192 allocs>: PASS

sram_free(<all>) = 0: PASS

sram_alloc(1, L1_DATA_SRAM+A+B) = 0xff800000: PASS

sram_free(0xff800000) = 0: PASS

Testing L2_SRAM on cpu 0 ...

sram_alloc(1, L2_SRAM) = <not available?>: SKIP

General tests on cpu 0 ...

sram_free(bad pointer) = 0: PASS

Parallel tests on all cpus ...

        pid 164 on cpu 0

        pid 165 on cpu 0

        pid 166 on cpu 0

        pid 167 on cpu 0

        pid 168 on cpu 0

        pid 169 on cpu 0

        pid 170 on cpu 0

        pid 171 on cpu 0

        pid 172 on cpu 0

        pid 173 on cpu 0

child exited with 65280: FAIL

child exited with 65280: FAIL

child exited with 65280: FAIL

child exited with 65280: FAIL

child exited with 65280: FAIL

child exited with 65280: FAIL

child exited with 65280: FAIL

child exited with 65280: FAIL

child exited with 65280: FAIL

child exited with 65280: FAIL

Test summary: some tests FAIL

root:/>

--

Follow-ups

--- Sonic Zhang                                              2011-01-04 04:17:54

Fixed.

--- Vivi Li                                                  2011-01-20 01:14:55

OK now. Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.