Article [#6422] [ltp] sendfile04 and sendfile04_64 fail in latest trunk(2010)

[#6422] [ltp] sendfile04 and sendfile04_64 fail in latest trunk

Submitted By: Vivi Li

Open Date

2010-12-23 22:57:07     Close Date

2011-01-12 22:35:23

Priority:

Medium     Assignee:

steven miao

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-trunk

App binary format:

N/A     

Summary: [ltp] sendfile04 and sendfile04_64 fail in latest trunk

Details:

LTP test cases of sendfile04 and sendfile04_64 fail in latest trunk, with ltp-full-20101031.

They are new cases, not a regression bug.

--

root:/> sendfile04

sendfile04    1  TFAIL  :  call succeeded unexpectedly

sendfile04    2  TFAIL  :  call succeeded unexpectedly

sendfile04    3  TFAIL  :  call succeeded unexpectedly

sendfile04    4  TFAIL  :  call succeeded unexpectedly

sendfile04    5  TFAIL  :  call succeeded unexpectedly

root:/> sendfile04_64

sendfile04_64    1  TFAIL  :  call succeeded unexpectedly

sendfile04_64    2  TFAIL  :  call succeeded unexpectedly

sendfile04_64    3  TFAIL  :  call succeeded unexpectedly

sendfile04_64    4  TFAIL  :  call succeeded unexpectedly

sendfile04_64    5  TFAIL  :  call succeeded unexpectedly

root:/>

--

Follow-ups

--- steven miao                                              2011-01-05 03:07:50

since blackfin arch has no process vm area protection implementation, it will

not return -EFAULT as expected when you pass a unmapped buffer pointer or

protected buffer pointer.

--- Vivi Li                                                  2011-01-12 22:35:22

So disable sendfile04 and sendfile04_64 in ltp_auto_test.exp.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.