Article [#6427] Characters are missing in kernel prompt(2010)

[#6427] Characters are missing in kernel prompt

Submitted By: Vivi Li

Open Date

2010-12-28 04:18:29     Close Date

2011-01-20 00:10:04

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-Dec_09.5013

App binary format:

N/A     

Summary: Characters are missing in kernel prompt

Details:

Characters are missing in kernel prompt.

Bellow is the log:

--

Linux version 2.6.36.2-ADI-2011R1-pre-svn9536 (test@uclinux71-lcd-ad73311) (gcc version 4.3.5 (ADI-trunk/svn-5013) ) #4 Tue Dec 0

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00117800

  rodata    = 0x00117800-0x001740b4

  bss       = 0x00175000-0x001856d0

  data      = 0x001856d0-0x00198000

    stack   = 0x00196000-0x00198000

  init      = 0x00198000-0x008ac000

  available = 0x008ac000-0x03800000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 125 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 47896k/65536k RAM, (7248k init code, 1114k kernel code, 514k data, 1024k dma, 7740k reserved)

Hierarchical RCU implementation.

        RCU-based detection of stalled CPUs is disabled.

        Verbose stalled-CPUs detection is disabled.

NR_IRQS:138

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (35 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 93

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=24)@sclk=125MHz)

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

>IP-Config: Complete:tting system clock to 1971-11-02 08:38:18 UTC (57919098)

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

dma_alloc_init: dma_page @ 0x0277f000 - 256 pages at 0x03f00000

Freeing unused kernel memory: 7248k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.18.1 (2010-12-28 16:44:33 CST) hush - the humble shell

root:/> PHY: 0:01 - Link is Up - 100/Full

>

>

>

> version

kernel:    Linux release 2.6.36.2-ADI-2011R1-pre-svn9536, build #4 Tue Dec 28 17:16:01 CST 2010

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5013)

user-dist: release svn-10023, build #2 Tue Dec 28 17:15:09 CST 2010

root:/>

>

> ls

bin   etc   init  mnt   root  sys   usr

dev   home  lib   proc  sbin  tmp   var

root:/>

>

>

--

Follow-ups

--- Mike Frysinger                                           2010-12-28 12:29:00

what chars are you talking about ?  it looks fine to me.

--- Vivi Li                                                  2010-12-28 21:20:49

The kernel prompt should be "root:/>", but now it's

">", "root:/" is missing.

--- Mike Frysinger                                           2010-12-28 21:23:46

i see "root:/>".  is each of those ">" you hitting

return ?  or is it debug output of expect ?

--- Vivi Li                                                  2010-12-28 21:33:15

There is nothing to do with expect. I run all this manually.

When I hit return right after kernel prompt, it shows ">".

But when I run a command, kernel prompt shows up correctly after the command

result.

--- Bob Liu                                                  2011-01-03 22:07:40

Busybox-1.17.4 works fine, so maybe ask busybox-list for help.

--- Bob Liu                                                  2011-01-09 21:13:31

should be fixed by commit 10043

--- Vivi Li                                                  2011-01-17 02:28:59

OK. Close it.

--- Vivi Li                                                  2011-01-17 05:07:47

I find this bug is not completely fixed, reopen it.

When run a process in the background, character will be missing again.

--

root:/> ls &

>

>

>

> ls

[1] 143 ls

bin   etc   init  mnt   root  sys   usr

dev   home  lib   proc  sbin  tmp   var

[1] Done                   ls

bin   etc   init  mnt   root  sys   usr

dev   home  lib   proc  sbin  tmp   var

root:/>

--

--- Bob Liu                                                  2011-01-19 03:58:17

should be fixed by commit 10058

--- Vivi Li                                                  2011-01-20 00:10:04

OK, close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.