Article [#6453] SMP kernel fails to boot on bf561-ezkit in trunk(2011)

[#6453] SMP kernel fails to boot on bf561-ezkit in trunk

Submitted By: Vivi Li

Open Date

2011-01-17 22:30:16     Close Date

2011-05-30 05:50:56

Priority:

Medium     Assignee:

steven miao

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF561     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2010_Dec_09

App binary format:

N/A     

Summary: SMP kernel fails to boot on bf561-ezkit in trunk

Details:

SMP kernel crashed on bf561-ezkit in trunk.

--

Linux version 2.6.37-ADI-2011R1-pre-svn9570 (test@uclinux65-561-SMP) (gcc version 4.3.5 (ADI-trunk/svn-5013) ) #171 SMP Tue Jan 1

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00122840

  rodata    = 0x00122840-0x0017a9cc

  bss       = 0x0017b000-0x0018d1a0

  data      = 0x0018d1a0-0x001a0000

    stack   = 0x0019e000-0x001a0000

  init      = 0x001a0000-0x00734000

  available = 0x00734000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace Active and Enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF561 Rev 0.5

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 600 MHz core clock and 100 MHz System Clock

NOMPU: setting up cplb tables

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

  L2 SRAM        : uncacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-through) in data cache

  L2 SRAM        : uncacheable in data cache

PERCPU: Embedded 8 pages/cpu @007b9000 s8288 r8192 d16288 u32768

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16002

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=30000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 56492k/65536k RAM, (5712k init code, 1158k kernel code, 502k data, 1024k dma, 648k reserved)

Hierarchical RCU implementation.

NR_IRQS:153

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 1191.93 BogoMIPS (lpj=2383872)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CoreB bootstrap code to SRAM ff600000 via DMA.

------------[ cut here ]------------

kernel BUG at kernel/workqueue.c:2797!

Kernel panic - not syncing: BUG()

Hardware Trace:

   0 Target : <0x000045c0> { _trap_c + 0x0 }

     Source : <0x0000af4c> { _exception_to_level5 + 0xb4 } CALL pcrel

   1 Target : <0x0000af1a> { _exception_to_level5 + 0x82 }

     Source : <0x0000af16> { _exception_to_level5 + 0x7e } IF !CC JUMP pcrel

   2 Target : <0x0000ae98> { _exception_to_level5 + 0x0 }

     Source : <0x0000ad3c> { _bfin_return_from_exception + 0x20 } RTX

   3 Target : <0x0000ad1c> { _bfin_return_from_exception + 0x0 }

     Source : <0x0000adf0> { _ex_trap_c + 0x84 } JUMP.S

   4 Target : <0x0000ad84> { _ex_trap_c + 0x18 }

     Source : <0x0000ad80> { _ex_trap_c + 0x14 } IF !CC JUMP pcrel

   5 Target : <0x0000ad6c> { _ex_trap_c + 0x0 }

     Source : <0x0000b06c> { _trap + 0xb4 } JUMP (P4)

   6 Target : <0x0000b02c> { _trap + 0x74 }

     Source : <0x0000b028> { _trap + 0x70 } IF !CC JUMP pcrel

   7 Target : <0x0000b012> { _trap + 0x5a }

     Source : <0x0000b00e> { _trap + 0x56 } IF CC JUMP pcrel

   8 Target : <0x0000affe> { _trap + 0x46 }

     Source : <0x0000afec> { _trap + 0x34 } JUMP.S

   9 Target : <0x0000afb8> { _trap + 0x0 }

      FAULT : <0x00029dec> { ___alloc_workqueue_key + 0xbc } BUG

     Source : <0x00029dea> { ___alloc_workqueue_key + 0xba } IF CC JUMP pcrel (BP)

  10 Target : <0x00029de4> { ___alloc_workqueue_key + 0xb4 }

     Source : <0x00029edc> { ___alloc_workqueue_key + 0x1ac } JUMP.S

  11 Target : <0x00029eda> { ___alloc_workqueue_key + 0x1aa }

     Source : <0x0005190e> { _pcpu_alloc + 0x2ae } RTS

  12 Target : <0x000518e8> { _pcpu_alloc + 0x288 }

     Source : <0x00121ce2> { _mutex_unlock + 0x26 } RTS

  13 Target : <0x00121cd8> { _mutex_unlock + 0x1c }

     Source : <0x0000d316> { ___raw_atomic_update_asm + 0x1a } RTS

  14 Target : <0x0000d312> { ___raw_atomic_update_asm + 0x16 }

     Source : <0x0000d012> { _put_core_lock + 0x1a } RTS

  15 Target : <0x0000cff8> { _put_core_lock + 0x0 }

     Source : <0x0000d30e> { ___raw_atomic_update_asm + 0x12 } JUMP.L

Stack info:

SP: [0x0202bd70] <0x0202bd70> /* kernel dynamic memory (maybe user-space) */

FP: (0x0202bf8c)

Memory from 0x0202bd70 to 0202c000

0202bd70:[0014f528] 00120cfc  0202be68  0014f528  00181b63  00181b63  00181b63  0202bdb8

0202bd90: 0202bf54  000049d8  0202be68  00000000  001547e0  00008008  00002021  00000021

0202bdb0: 00000013  007bab78  0000003f  0000001f  00000002  02028ebc  02028ec0  0000f9e0

0202bdd0: 0202830c  007bab78  02028314 <0000f19c> 02028d60  007bab40  0202be08  0000fac6

0202bdf0: 020282e0  007bab78  00015ce6  020282e0  007bab40  02028d60  0202be40  00121138

0202be10: ffe05000  02028d60  02028ebc  02028d60  0202be58  00121138  0202a008  00001015

0202be30: 00000000  00732c20  00000000  0000ffff  0000af50  0017d000  ffe02014  00008008

0202be50: 00002021  00000100 <020260c8> 7fffffff  00000000  00000480  00000480  00008008

0202be70: 00002021  00000000  0202bf44  00000480  00029dec  00029eda  000000e0  00003004

0202be90: 000a2ebe  000a3cf8  000a2eb4  000a3cf8  00000000  00000000  00000000  00000000

0202beb0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0202bed0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

0202bef0: 02004000  00000000  00000000  0202bf54  001876a0  020260c0  001547e0  001883f4

0202bf10: 00195fc4  feb00000  00000000  00000100  00000100 <020260c8> 00000001  0000001f

0202bf30: 007352e0  000000e0  000000e0  feb00000  00000006  00000000  001883ec  00000000

0202bf50: 0000001f  00123a1c  001a90c2  001876a0  00000002  00732320  00000000  0017d000

0202bf70: 00123a18  0018dbc0  0011d0e4  0011d0ec  00000000  00000000  00000000 (00000000)

0202bf90:<0000113c> 001b7ebc  0017b00c  001a8f04  0202a000  00000000  00000000  00000000

0202bfb0: 00000000  00000000  ff600000  001a02c0  001b7ebc  001b7ec0  00000000  0202a000

0202bfd0: 00000000  00000000  00000000  00000000  00000002 <000016ae> 00000000  00000000

0202bff0: 00000000  00000000  ffffffff  00000006

Return addresses in stack:

    address : <0x0000f19c> { _deactivate_task + 0x34 }

    address : <0x020260c8> /* kernel dynamic memory (maybe user-space) */

    address : <0x020260c8> /* kernel dynamic memory (maybe user-space) */

   frame  1 : <0x0000113c> { _do_one_initcall + 0x94 }

    address : <0x000016ae> { _kernel_thread_helper + 0x6 }

--

Follow-ups

--- Vivi Li                                                  2011-01-23 22:33:02

I found the config for 561 smp kernel is wrong. Update build_policy_kernel.exp

to fix this.

--- Vivi Li                                                  2011-01-24 22:27:28

Configuration is OK now. But it will still crash.

--- steven miao                                              2011-01-31 05:27:53

percpu data is unaligned caused this crash. tuning PERCPU(PAGE_SIZE) definition

in vmlinux.lds.S link script can resolve this unalignment.

--- Vivi Li                                                  2011-05-30 05:59:20

OK. Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.smp    application/octet-stream    29152    Vivi Li

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.