Article [#6596] Error info will show up during mmc test in trunk(2011)

[#6596] Error info will show up during mmc test in trunk

Submitted By: Vivi Li

Open Date

2011-05-12 23:37:30     Close Date

2011-06-02 05:55:40

Priority:

Medium     Assignee:

steven miao

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF518     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Not reproducible

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2010_Dec_09

App binary format:

N/A     

Summary: Error info will show up during mmc test in trunk

Details:

Error info will show up during mmc test in trunk.

Last passed version:

--

kernel:    Linux release 2.6.37-ADI-2011R1-pre-svn9600, build #30 Fri Feb 11 17:48:07 CST 2011

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5013)

user-dist: release svn-10076, build #327 Fri Feb 11 17:45:14 CST 2011

--

Bellow is the error log:

--

U-Boot 2010.12-svn2586 (ADI-2011R1-pre) (Jan 18 2011 - 19:07:43)

CPU:   ADSP bf518-0.0 (Detected Rev: 0.1) (parallel flash boot)

Board: ADI BF518F EZ-Board board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 400 MHz, Core: 400 MHz, System: 80 MHz

RAM:   64 MiB

Flash: 4 MiB

MMC:   Blackfin SDH: 0

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   bfin_mac

Hit any key to stop autoboot:  0

bfin>

bfin> run ramboot

Using bfin_mac device

TFTP from server 10.100.4.174; our IP address is 10.100.4.50

Filename 'uImage'.

Load address: 0x1000000

Loading: #################################################################

         #################################################################

         #################################################################

         #################################################################

         #######################################

done

Bytes transferred = 4377003 (42c9ab hex)

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf518-0.1-2.6.39-rc7-ADI-2011R1-

   Created:      2011-05-12  17:58:41 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4376939 Bytes = 4.2 MiB

   Load Address: 00001000

   Entry Point:  001c3f2c

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001c3f2c

Linux version 2.6.39-rc7-ADI-2011R1-pre-svn9880 (test@uclinux80-bf518f) (gcc version 4.3.5 (ADI-trunk/svn-5013) ) #6 Fri May 13 1

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00135d68

  rodata    = 0x00135d68-0x0019886c

  bss       = 0x00199000-0x001a9a5c

  data      = 0x001a9a5c-0x001bc000

    stack   = 0x001ba000-0x001bc000

  init      = 0x001bc000-0x007d3000

  available = 0x007d3000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace active and enabled

Boot Mode: 1

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF518 Rev 0.1

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 400 MHz core clock and 80 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16002

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 55892k/65536k RAM, (6236k init code, 1235k kernel code, 537k data, 1024k dma, 612k reserved)

NR_IRQS:159

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 792.57 BogoMIPS (lpj=1585152)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 32 KB (25 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

ezbrd_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc00500, dma channel@7

bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0, regs_base@ffc03400, dma channel@5

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 109

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 29) is a BFIN-UART

bfin-otp: initialized

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=15)@sclk=80MHz)

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

dma_alloc_init: dma_page @ 0x02775000 - 256 pages at 0x03f00000

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-05-31 21:03:17 UTC (1086037397)

mmc0: host does not support reading read-only switch. assuming write-enable.

mmc0: new SD card at address e624

mmcblk0: mmc0:e624 SD02G 1.89 GiB

mmcblk0: p1 p2

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf518f-ezbrd, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

Freeing unused kernel memory: 6236k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - https://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.18.4 (2011-05-12 23:01:18 CST) hush - the humble shell

root:/> PHY: 0:01 - Link is Up - 100/Full

root:/>

root:/> mke2fs /dev/mmcblk0p2

mke2fs 1.41.12 (17-May-2010)

ext2fs_check_if_mount: Can't check if filesystem is mounted due to missing mtab file while determining whether /dev/mmcblk0p2 is.

Filesystem label=

OS type: Linux

Block size=4096 (log=2)

Fragment size=4096 (log=2)

Stride=0 blocks, Stripe width=0 blocks

62080 inodes, 248256 blocks

12412 blocks (5.00%) reserved for the super user

First data block=0

Maximum filesystem blocks=255852544

8 block groups

32768 blocks per group, 32768 fragments per group

7760 inodes per group

Superblock backups stored on blocks:

        32768, 98304, 163840, 229376

Writing inode tables: done

Writing superblocks and filesystem accounting information: done

This filesystem will be automatically checked every 34 mounts or

180 days, whichever comes first.  Use tune2fs -c or -i to override.

root:/> mount /dev/mmcblk0p2 /mnt/

root:/> cd /mnt/

root:/mnt> ls

lost+found

root:/mnt> time dd conv=fsync if=/dev/zero of=/mnt/10.bin bs=1M count=10

10+0 records in

10+0 records out

real    0m 5.16s

user    0m 0.00s

sys     0m 0.93s

root:/mnt> ls

10.bin      lost+found

root:/mnt> cat 10.bin >/dev/null

root:/mnt> ls

10.bin      lost+found

root:/mnt> cd

root:/> umount /mnt/

root:/>

root:/> mkdosfs -F 32 /dev/mmcblk0p1

mkdosfs 3.0.5 (27 Jul 2009)

root:/> mount /dev/mmcblk0p1 /mnt/

root:/> NULL pointer access

Deferred Exception context

CURRENT PROCESS:

COMM=inetd PID=174  CPU=0

TEXT = 0x029a0040-0x029a6520        DATA = 0x029a6540-0x029a7ca8

BSS = 0x029a7ca8-0x029a83a0  USER-STACK = 0x029a9f9c

return address: [0x029a09ce]; contents of:

0x029a09a0:  6082  e300  1383  0c38  1561  e5a8  0080  4808

0x029a09b0:  11ae  3005  e300  0318  0000  916d  0c45  1842

0x029a09c0:  0000  0000  0000  a0a8  0c00  17f7  aeea [9950]

0x029a09d0:  0c00  1ff3  e5a8  0080  4c00  e6a8  0080  304c

ADSP-BF518-0.1 400(MHz CCLK) 80(MHz SCLK) (mpu off)

Linux version 2.6.39-rc7-ADI-2011R1-pre-svn9880 (test@uclinux80-bf518f) (gcc version 4.3.5 (ADI-trunk/svn-5013) ) #6 Fri May 13 1

SEQUENCER STATUS:               Not tainted

SEQSTAT: 00002027  IPEND: 0008  IMASK: ffff  SYSCFG: 0006

  EXCAUSE   : 0x27

  physical IVG3 asserted : <0xffa00734> { _trap + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x02820000> [ init + 0x0 ]

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x029a08fe> [ inetd + 0x8be ]

PC  : <0x029a09ce> [ inetd + 0x98e ]

DCPLB_FAULT_ADDR: <0x00000000> /* Maybe null pointer? */

ICPLB_FAULT_ADDR: <0x029a09ce> [ inetd + 0x98e ]

PROCESSOR STATE:

R0 : 00000000    R1 : ffffffff    R2 : 00000001    R3 : 00000000

R4 : 00000000    R5 : 00000006    R6 : 0000001f    R7 : 00000001

P0 : 00000072    P1 : 029a9f0c    P2 : 00000000    P3 : 029a9eec

P4 : 00000004    P5 : 029b729c    FP : 029a9f18    SP : 0281ff24

LB0: 029a26d3    LT0: 029a26d2    LC0: 00000000

LB1: 029a01fd    LT1: 029a01f6    LC1: 00000013

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 029a6578

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 02826300

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 00000000   A0.x: 00000000   A1.w: 00000000   A1.x: 00000000

USP : 029a9dd0  ASTAT: 02001025

Hardware Trace:

   0 Target : <0x00003fbc> { _trap_c + 0x0 }

     Source : <0xffa006c8> { _exception_to_level5 + 0xa4 } JUMP.L

   1 Target : <0xffa00624> { _exception_to_level5 + 0x0 }

     Source : <0xffa004d8> { _bfin_return_from_exception + 0x18 } RTX

   2 Target : <0xffa004c0> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa0057c> { _ex_trap_c + 0x74 } JUMP.S

   3 Target : <0xffa00508> { _ex_trap_c + 0x0 }

     Source : <0xffa0078e> { _trap + 0x5a } JUMP (P4)

   4 Target : <0xffa00734> { _trap + 0x0 }

      FAULT : <0x029a09ce> [ inetd + 0x98e ] R0 = B[P2] (X)

     Source : <0x029a09cc> [ inetd + 0x98c ] R2 = W[P5 + 11](X)

   5 Target : <0x029a09b8> [ inetd + 0x978 ]

     Source : <0x029a09ca> [ inetd + 0x98a ] IF !CC JUMP pcrel (BP)

   6 Target : <0x029a09c4> [ inetd + 0x984 ]

     Source : <0x029a094c> [ inetd + 0x90c ] JUMP.S

   7 Target : <0x029a093c> [ inetd + 0x8fc ]

     Source : <0x029a0902> [ inetd + 0x8c2 ] IF CC JUMP pcrel

   8 Target : <0x029a08fe> [ inetd + 0x8be ]

     Source : <0x029a12a0> [ inetd + 0x1260 ] RTS

   9 Target : <0x029a129c> [ inetd + 0x125c ]

     Source : <0x029a3e1c> [ inetd + 0x3ddc ] RTS

  10 Target : <0x029a3e0c> [ inetd + 0x3dcc ]

     Source : <0x029a12b4> [ inetd + 0x1274 ] RTS

  11 Target : <0x029a12a4> [ inetd + 0x1264 ]

     Source : <0x029a3e08> [ inetd + 0x3dc8 ] JUMP.L

  12 Target : <0x029a3dfe> [ inetd + 0x3dbe ]

     Source : <0xffa00c7c> { __common_int_entry + 0xcc } RTI

  13 Target : <0xffa00c1a> { __common_int_entry + 0x6a }

     Source : <0xffa00fd4> { _evt_system_call + 0x64 } JUMP.S

  14 Target : <0xffa00fd4> { _evt_system_call + 0x64 }

     Source : <0xffa0091a> { _system_call + 0xbe } RTS

  15 Target : <0xffa00916> { _system_call + 0xba }

     Source : <0xffa00906> { _system_call + 0xaa } IF !CC JUMP pcrel

Userspace Stack

Stack info:

SP: [0x029a9dd0] <0x029a9dd0> [ inetd + 0x9dd0 ]

FP: (0x029a9f48)

Memory from 0x029a9dd0 to 029aa000

029a9dd0:[029a9e04] 0000000a  00000001  00000000  029a9f0c  029a13d8  029a9e6c  00000000

029a9df0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

029a9e10: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

029a9e30: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

029a9e50: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

029a9e70: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

029a9e90: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

029a9eb0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

029a9ed0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  029a9fa0

029a9ef0: 029a64ec  029a0810  00000000  17000002  00000000  029a9f18  029a0824  00000001

029a9f10: 00000000  00000001  029a9f48  029a0dea  00000000  00000001  029a7b68  00000000

029a9f30: 029a9fa0  029a64ec  029a0d64  029a9fa0  029a9f5c  00000000 (029a9f5c)<029a3c1c>

029a9f50: 00000000  00000000  00000000 (00000000) 02820a8a  029a6540  02837b68  02837b6c

029a9f70: 00000000  40bb9d9d  00000005  00000048  00000000  00000000  00000000  029a64ec

029a9f90: 029a64fe  00000000  0281ca56  00000001  029a9fb4  00000000 <029a9fc0> 029a9fcd

029a9fb0: 00000000  6962732f  6e692f6e  00647465  4d524554  6b6e753d  6e776f6e  54415000

029a9fd0: 622f3d48  2f3a6e69  2f727375  3a6e6962  6962732f  752f3a6e  732f7273  006e6962

029a9ff0: 6962732f  6e692f6e  00647465  00000000

Return addresses in stack:

   frame  1 : <0x029a3c1c> [ inetd + 0x3bdc ]

    address : <0x029a9fc0> [ inetd + 0x9fc0 ]

root:/> ls /mnt/

root:/> time dd conv=fsync if=/dev/zero of=/mnt/10.bin bs=1M count=10

10+0 records in

10+0 records out

real    0m 6.31s

user    0m 0.00s

sys     0m 1.16s

root:/> ls /mnt/

10.bin

root:/>

--

Follow-ups

--- steven miao                                              2011-05-24 04:56:59

tested on bf518, but not reproducible

--- Vivi Li                                                  2011-06-02 04:48:40

I can still see it crash on bf518.

--- Vivi Li                                                  2011-06-02 06:03:25

Sorry, I see kernel crash, not the same problem as I addressed before.

Close this bug and open a new one.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.linux.sdiommc    application/octet-stream    34389    Vivi Li

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.