Article [#6641] ifconfig only frees the first page of tx_desc(2011)

[#6641] ifconfig only frees the first page of tx_desc

Submitted By: Regis DARGENT

Open Date

2011-06-14 06:34:20    

Priority:

Medium     Assignee:

Sonic Zhang

Status:

Open     Fixed In Release:

N/A

Found In Release:

2010R1-RC5     Release:

Category:

Networking     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

4.3.5

App binary format:

N/A     

Summary: ifconfig only frees the first page of tx_desc

Details:

When you call ifconfig <eth interface> down, only the first allocated page of the tx_desc is freed, causing memory leak.

In fact, bfin_mac_free (when CONFIG_BFIN_MAC_USE_L1 not defined), uses sizeof(ptr) to determine the number of bytes to be deallocated, which only reports the size of the first element in the case of a table. Therefore, only the page(s) corresponding to the size of one element are freed. In the case of a 10 elements table, each of size 1596 bytes, only the first 4kB page is freed instead of the 16kB allocated.

How to reproduce the bug:

a simple loop may do it:

while (1)

  ifconfig eth0 up (with a valid IP)

  wait for the interface to come up (eg 5sec)

  ifconfig eth0 down

  wait for the interface to come down (eg 5sec)

done

a proposed patch is attached.

Follow-ups

--- Sonic Zhang                                              2011-06-15 05:55:14

Thanks for the bug report. I commit a more unified patch other than put macro

around each free line.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

bfin_mac.c    application/c    47023    Regis DARGENT

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.