Article [#6678] tftlcd test on bf527 fails for unable to mmap frame buffer(2011)

[#6678] tftlcd test on bf527 fails for unable to mmap frame buffer

Submitted By: Mingquan Pan

Open Date

2011-07-05 03:49:54     Close Date

2011-08-15 03:48:36

Priority:

Medium     Assignee:

Scott Jiang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

5013

App binary format:

N/A     

Summary: tftlcd test on bf527 fails for unable to mmap frame buffer

Details:

tftlcd test on bf527 fails for unable to mmap frame buffer.

## Booting kernel from Legacy Image at 02000000 ...

   Image Name:   bf527-0.2-2.6.39.2-ADI-2011R1-pr

   Created:      2011-07-03   5:56:12 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4471025 Bytes = 4.3 MiB

   Load Address: 00001000

   Entry Point:  00204ccc

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 00204ccc

Linux version 2.6.39.2-ADI-2011R1-pre-svn10001 (test@uclinux60-bf527-std) (gcc version 4.3.5 (ADI-trunk/svn-5013) ) #12 Sun Jul 3 13:56:06 CST 2011

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart1] enabled

early printk enabled on early_BFuart1

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x0015b528

  rodata    = 0x0015b528-0x001d29a8

  bss       = 0x001d3000-0x001e4848

  data      = 0x001e4848-0x001fc000

    stack   = 0x001fa000-0x001fc000

  init      = 0x001fc000-0x00867000

  available = 0x00867000-0x03f00000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace active and enabled

Boot Mode: 1

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF527 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 16002

Kernel command line: root=/dev/mtdblock0 rw ip=10.100.4.50 earlyprintk=serial,uart1,57600 console=ttyBF1,57600 ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf527-ezkit:eth0:off

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 55300k/65536k RAM, (6572k init code, 1385k kernel code, 643k data, 1024k dma, 612k reserved)

NR_IRQS:159

Configuring Blackfin Priority Driven Interrupts

console [ttyBF1] enabled, bootconsole disabled

console [ttyBF1] enabled, bootconsole disabled

Calibrating delay loop... 1044.48 BogoMIPS (lpj=2088960)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

bio: create slab <bio-0> at 0

SCSI subsystem initialized

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@7

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller, regs_base@ffc01400

Advanced Linux Sound Architecture Driver Version 1.0.24.

musb-hdrc: version 6.0, musb-dma, host, debug=0

musb-hdrc musb-hdrc: MUSB HDRC host driver

musb-hdrc musb-hdrc: new USB bus registered, assigned bus number 1

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

musb-hdrc musb-hdrc: USB Host mode controller at ffc03800 using DMA, IRQ 59

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 108

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 31) is a BFIN-UART

bfin-otp: initialized

brd: module loaded

adp5520 0-0032: failed writing 0x80 to 0x00

adp5520 0-0032: failed to write

adp5520: probe of 0-0032 failed with error -1

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x000000000000-0x000000040000 : "bootloader(spi)"

0x000000040000-0x000000200000 : "linux kernel(spi)"

bfin_mii_bus: probed

bfin_mac: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=25)@sclk=131MHz)

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ad7879 0-002c: Failed to write AD7879 Touchscreen

ad7879: probe of 0-002c failed with error -1

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-05-31 15:18:45 UTC (1086016725)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf527-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

dma_alloc_init: dma_page @ 0x0288d000 - 256 pages at 0x03f00000

Freeing unused kernel memory: 6572k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - http://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.18.4 (2011-07-03 13:02:39 CST) hush - the humble shell

root:/> versiPHY: 0:01 - Link is Up - 100/Full

on

kernel:    Linux release 2.6.39.2-ADI-2011R1-pre-svn10001, build #12 Sun Jul 3 13:56:06 CST 2011

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-trunk/svn-5013)

user-dist: release svn-10241, build #146 Sun Jul 3 13:55:08 CST 2011

root:/> successful boot attempt

************** STEP 3: Start testing.

usb 1-1: new high speed USB device number 2 using musb-hdrc

scsi0 : usb-storage 1-1:1.0

scsi 0:0:0:0: Direct-Access     SanDisk  U3 Cruzer Micro  3.21 PQ: 0 ANSI: 2

sd 0:0:0:0: [sda] 2006673 512-byte logical blocks: (1.02 GB/979 MiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Assuming drive cache: write through

sd 0:0:0:0: [sda] Assuming drive cache: write through

sda: sda1 sda2

sd 0:0:0:0: [sda] Assuming drive cache: write through

sd 0:0:0:0: [sda] Attached SCSI removable disk

root:/> modprobe bfin_lq035q1_fb

bfin-lq035q1 bfin-lq035q1: 320x240 16-bit RGB FrameBuffer initialized

root:/>

Case 1 ...PASS

Case 1 ...PASS

lsmod

Module                  Size  Used by

bfin_lq035q1_fb         4793  0

cfbimgblt               1488  1 bfin_lq035q1_fb

cfbfillrect             2655  1 bfin_lq035q1_fb

cfbcopyarea             2599  1 bfin_lq035q1_fb

root:/>

Case 2 ...PASS

Case 2 ...PASS

video_test

Unable to mmap frame buf

Last passed time: 2011_Jun_21_15_08.

Uclinux-dist version: 10210.

Kernel verion: 9962, git-id: 9c8f4a29786bcc805f53bb1626915f6671ddb01b

Case 3 ...FAIL

Follow-ups

--- Bob Liu                                                  2011-07-22 04:32:34

fix by commit: "nommu: remap_pfn_range: add PAGE_MASK"

--- Vivi Li                                                  2011-08-15 03:48:35

No such problem now.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.