Article [#6681] icc packet test has dump info in running on bf561(2011)

[#6681] icc packet test has dump info in running on bf561

Submitted By: Mingquan Pan

Open Date

2011-07-06 03:36:47     Close Date

2011-09-07 05:03:41

Priority:

Medium     Assignee:

steven miao

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

2010R1-RC4

App binary format:

N/A     

Summary: icc packet test has dump info in running on bf561

Details:

icc packet test has dump info in running on bf561.

root:/> version^[[58;9R

kernel:    Linux release 2.6.39.2-ADI-2011R1-pre-svn9998, build #29 Tue Jul 5 14:24:24 CST 2011

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2010R1-RC4)

user-dist: release svn-10225, build #11 Tue Jul 5 14:23:49 CST 2011

root:/>

*******************************************************************

STEP 3: Starting test

^[[58;9Rcd /bin

root:/bin> ^[[58;12R./icc_loader -l ./icc

writing to 0xfeb00000, 0x668c    bytes: OK

writing to 0xff600000, 0xc4      bytes: OK

root:/bin> ^[[58;12Rsm_debug:feb1f000 COREB: @@@ gen pool create0

sm_debug:    1 : 0

sm_debug:received 1

sm_debug:feb1f040 COREB: @@@ gen pool create1

sm_debug:    2 : 1

sm_debug:received 2

Case 1 ...PASS

root:/bin>

Case 1 ...PASS

^[[58;12R./icc_losm_debug:feb1f080 COREB: before run task

sm_debug:    3 : 2

sm_debug:received 3

ader -f -e ./task1

writing to 0x03c00000, 0x2a8     bytes: OKsm_debug:ioctl type 2

task_init_addr 3c00000

sm_debug:sm_find_session bits 00000000 localep 0

sm_debug:table bits1 00000000

sm_debug:table index 0

sm_debug:table bits2 00000001

sm_debug:create ep index 0 srcep 0 type 2

sm_debug:session 0292a800

sm_debug:size of session 60

sm_debug:ioctl type 2000000

sm_debug:sm_send_packet: 0 0292a800

sm_debug:sm_send_packet: len 268 type 2000000 dst 1 dstep 5 src 0 srcep 0

sm_debug:alloc buffer 2943200

sm_debug:sm_task_sendmsg msg type 2000000

sm_debug:sm_task_sendmsg init addr03c00000

sm_debug:sm_send_packet: len 268 type 2000000 dst 1 dstep 5 src 0 srcep 0

sm_debug:sm_send_message_internal: dst 1 src 0

sm_debug:send message cpu 1 sent 1

sm_debug:feb1f0c0 COREB: sm_handle_control_message type 2000000

sm_debug:    4 : 3

sm_debug:received 4

sm_debug:feb1f100 COREB: sm_handle_control_message 2000000 2000000

sm_debug:    5 : 4

sm_debug:received 5

sm_debug:feb1f140 COREB: task init 3c00000

sm_debug:    6 : 5

sm_debug:received 6

sm_debug:feb1f180 COREB: sm_send_message_internal() dst 0 src 1 2000001

sm_debug:    7 : 6

sm_debug:received 7

sm_debug:sm_find_session bits 00000001 localep 0

sm_debug:index 0 ,local ep 0 type 2

sm_debug:session 0292a800 index 0 msg type2000001

sm_debug:sm_task_recvmsg msg type 2000001

sm_debug:sm_task_recvmsg free 2943200

sm_debug:received 8

sm_debug:feb1f000 COREB: finish sm_handle_control_message

sm_debug:    9 : 8

sm_debug:received 9

sm_debug:feb1f040 COREB: before run task

sm_debug:    10 : 9

sm_debug:received 10

sm_debug:ioctl type 2000000

root:/bin> ^[[58;12Rsm_debug:feb1f080 COREB: before run task1

sm_debug:    11 : 10

sm_debug:received 11

sm_debug:feb1f0c0 COREB: create ep

sm_debug:    12 : 11

sm_debug:received 12

sm_debug:feb1f100 COREB: create ep index 0 srcep 5

sm_debug:    13 : 12

sm_debug:received 13

sm_debug:feb1f140 COREB: icc_task_init() task1 icc index 0

sm_debug:    14 : 13

sm_debug:received 14

sm_debug:feb1f180 COREB: task loop

sm_d

Case 2 ...PASS

ebug:    15 : 14

sm_debug:received 15

root:/bin>

Case 2 ...PASS

^[[58;12R./packet_test -s 123 

sp packet 4sm_debug:ioctl type 4

begin create ep

sm_debug:sm_find_session bits 00000000 localep 9

sm_debug:table bits1 00000000

sm_debug:table index 0

sm_debug:table bits2 00000001

sm_debug:create ep index 0 srcep 9 type 4

sm_debug:session 0292a800

sm_debug:size of session 60

fism_debug:ioctl type 4n index = 0

sm_debug:sm_send_packet: 0 0292a800

sm_debug:sm_send_packet: len 16 type 4000000 dst 1 dstep 5 src 0 srcep 9

sm_debug:alloc buffer 29483c0

sm_debug:sm_default_sendmsg session type 4

sm_debug:sm_default_sendmsg: len 16 type 4000000 dst 1 dstep 5 src 0 srcep 9

sm_debug:sm_send_packet: len 16 type 4000000 dst 1 dstep 5 src 0 srcep 9

sm_debug:sm_send_message_internal: dst 1 src 0

sm_debug:send message cpu 1 sent 2

sm_debug:feb1f1c0 COREB: sm_handle_control_message type 4000000

sm_debug:    16 : 15

sm_debug:received 16

NULL pointer access

Deferred Exception context

CURRENT PROCESS:

COMM=packet_test PID=175  CPU=0

TEXT = 0x02b18040-0x02b1cb20        DATA = 0x02b1cb40-0x02b1e460

BSS = 0x02b1e460-0x02b1e6e0  USER-STACK = 0x02b1ff54

return address: [0x02b19304]; contents of:

0x02b192e0:  50d0  0e3a  1818  4349  601a  5490  0c02  1019

0x02b192f0:  44d1  c682  8441  c402  0411  c422  4411  3213

0x02b19300:  e0a2  1002 [9202] 0850  1002  0010  3013  3058

0x02b19310:  529a  3212  0c42  1804  e0a2  2002  9a01  0010

ADSP-BF561-0.3(Detected 0.5) 600(MHz CCLK) 100(MHz SCLK) (mpu off)

Linux version 2.6.39.2-ADI-2011R1-pre-svn9998 (test@adsl) (gcc version 4.3.5 (ADI-2010R1-RC4) ) #29 Tue Jul 5 14:24:24 CST 2011

SEQUENCER STATUS:        Not tainted

SEQSTAT: 00002027  IPEND: 0008  IMASK: ffff  SYSCFG: 0006

  EXCAUSE   : 0x27

  physical IVG3 asserted : <0xffa0083c> { _trap + 0x0 }

RETE: <0x00000000> /* Maybe null pointer? */

RETN: <0x02960000> [ init + 0x0 ]

RETX: <0x00000480> /* Maybe fixed code section */

RETS: <0x02b18342> [ packet_test + 0x302 ]

PC  : <0x02b19304> [ packet_test + 0x12c4 ]

DCPLB_FAULT_ADDR: <0x00000000> /* Maybe null pointer? */

ICPLB_FAULT_ADDR: <0x02b19304> [ packet_test + 0x12c4 ]

PROCESSOR STATE:

R0 : 00000000    R1 : 00000000    R2 : 00000000    R3 : 00000040

R4 : 02b1ff91    R5 : 00000000    R6 : 00000003    R7 : 02b1feb8

P0 : 00000000    P1 : 00000010    P2 : 00000040    P3 : 02b1fe98

P4 : 02b1fe94    P5 : 02b1fe78    FP : 02b1fee4    SP : 0295ff24

LB0: 02b19305    LT0: 02b19304    LC0: 00000010

LB1: 02b1adf9    LT1: 02b1adae    LC1: 00000000

B0 : 00000000    L0 : 00000000    M0 : 00000000    I0 : 02b1e30c

B1 : 00000000    L1 : 00000000    M1 : 00000000    I1 : 02b1fe98

B2 : 00000000    L2 : 00000000    M2 : 00000000    I2 : 00000000

B3 : 00000000    L3 : 00000000    M3 : 00000000    I3 : 00000000

A0.w: 0000147a   A0.x: 00000000   A1.w: 0000147a   A1.x: 00000000

USP : 02b1fe4c  ASTAT: 02002021

Hardware Trace:

   0 Target : <0x00004058> { _trap_c + 0x0 }

     Source : <0xffa007d0> { _exception_to_level5 + 0xa4 } JUMP.L

   1 Target : <0xffa0072c> { _exception_to_level5 + 0x0 }

     Source : <0xffa005e0> { _bfin_return_from_exception + 0x20 } RTX

   2 Target : <0xffa005c0> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa00684> { _ex_trap_c + 0x74 } JUMP.S

   3 Target : <0xffa00610> { _ex_trap_c + 0x0 }

     Source : <0xffa004e8> { _ex_workaround_261 + 0x1c } JUMP.S

   4 Target : <0xffa004cc> { _ex_workaround_261 + 0x0 }

     Source : <0xffa008a4> { _trap + 0x68 } JUMP (P4)

   5 Target : <0xffa0085a> { _trap + 0x1e }

     Source : <0xffa00856> { _trap + 0x1a } IF CC JUMP pcrel

   6 Target : <0xffa0083c> { _trap + 0x0 }

      FAULT : <0x02b19304> [ packet_test + 0x12c4 ] [P0++] = R2

     Source : <0xffa005e0> { _bfin_return_from_exception + 0x20 } RTX

   7 Target : <0xffa005c0> { _bfin_return_from_exception + 0x0 }

     Source : <0xffa004de> { _ex_workaround_261 + 0x12 } IF !CC JUMP pcrel

   8 Target : <0xffa004cc> { _ex_workaround_261 + 0x0 }

     Source : <0xffa008a4> { _trap + 0x68 } JUMP (P4)

   9 Target : <0xffa0085a> { _trap + 0x1e }

     Source : <0xffa00856> { _trap + 0x1a } IF CC JUMP pcrel

  10 Target : <0xffa0083c> { _trap + 0x0 }

     Source : <0x02b19300> [ packet_test + 0x12c0 ] LSETUP <> LC0= P1

  11 Target : <0x02b192dc> [ packet_test + 0x129c ]

     Source : <0x02b1833e> [ packet_test + 0x2fe ] CALL pcrel

  12 Target : <0x02b18336> [ packet_test + 0x2f6 ]

     Source : <0x02b18546> [ packet_test + 0x506 ] RTS

  13 Target : <0x02b1853e> [ packet_test + 0x4fe ]

     Source : <0x02b18530> [ packet_test + 0x4f0 ] IF CC JUMP pcrel (BP)

  14 Target : <0x02b18528> [ packet_test + 0x4e8 ]

     Source : <0xffa00da2> { __common_int_entry + 0xda } RTI

  15 Target : <0xffa00d40> { __common_int_entry + 0x78 }

     Source : <0xffa01184> { _evt_system_call + 0x64 } JUMP.S

Userspace Stack

Stack info:

SP: [0x02b1fe4c] <0x02b1fe4c> [ packet_test + 0x7e4c ]

FP: (0x02b1fee4)

Memory from 0x02b1fe40 to 02b20000

02b1fe40: 02b1fee4  02b18336  02b1feb8 [00000110] 00000000  02b1feb8  02b1cc88  00000000

02b1fe60: 02b1fea0  02b1fe9c  02b1fe90  02b1fe8c  02b1fe88  02b1fe84  00333231  00000000

02b1fe80: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000000

02b1fea0: 00000000  00000000  00000000  00000000  00000000  00000000  00000000  00000009

02b1fec0: 00000005  00000004  00000000  00000001  00000000  00000010  02b1fe78  00000000

02b1fee0: 00000000 (02b1ff14)<02b1a2e0> 00000000  00000003  02b1e320  00000000  02b1ff58

02b1ff00: 02b1cae4  02b18178  00000003  02b1ff58  00000000 (00000000) 02993dec  02b1cb40

02b1ff20: 02aeaa20  029f3dec  00000000  02aea9e0  00000000  00000000  00000000  00000000

02b1ff40: 00000000  02b1cae4  02b1caf6  00000000  029e9b88  00000003  02b1ff80 <02b1ff8e>

02b1ff60: 02b1ff91  00000000  02b1ff95  02b1ffa0  02b1ffc3  02b1ffd7  02b1ffe5  00000000

02b1ff80: 61702f2e  74656b63  7365745f  732d0074  33323100  52455400  696c3d4d  0078756e

02b1ffa0: 48544150  69622f3d  752f3a6e  622f7273  2f3a6e69  6e696273  73752f3a  62732f72

02b1ffc0: 48006e69  5f485355  53524556  3d4e4f49  38312e31  2e00342e  6361702f  5f74656b

02b1ffe0: 74736574  44575000  69622f3d  2f2e006e  6b636170  745f7465  00747365  00000000

Return addresses in stack:

   frame  1 : <0x02b1a2e0> [ packet_test + 0x22a0 ]

    address : <0x02b1ff8e> [ packet_test + 0x7f8e ]

sm_debug:feb1f000 COREB: @@@ wake up

sm_debug:    17 : 16

sm_debug:received 17

SEGV

root:/bin> ^[[58;12Rsm_debug:feb1f040 COREB: task loop

sm_debug:    18 : 17

sm_debug:received 18

sm_debug:feb1f080 COREB: index 0 ,local ep 5

sm_debug:    19 : 18

sm_debug:received 19

sm_debug:feb1f0c0 COREB: msg type 4000000 index 0 session type 4

sm_debug:    20 : 19

sm_debug:received 20

sm_debug:feb1f100 COREB: type 4000000, dstep 5, srcep 9

sm_debug:    21 : 20

sm_debug:received 21

sm_debug:feb1f140 COREB: recved packet msg handle0

sm_debug:    22 : 21

sm_debug:received 22

sm_debug:feb1f180 COREB: msg_recv_internal msg type 4000000 alloc 3d40000

sm_debug:    23 : 22

sm_debug:received 23

sm_debug:feb1f1c0 COREB: avail 1

sm_debug:    24 : 23

sm_debug:received 24

sm_debug:feb1f000 COREB: index 0 avail 1

sm_debug:    25 : 24

sm_debug:received 25

sm_debug:feb1f040 COREB:  sm_recv_packet session type 4 localep5

sm_debug:    26 : 25

sm_debug:received 26

sm_debug:feb1f080 COREB: sm_recv_packet() 123

sm_debug:    27 : 26

sm_debug:received 27

sm_debug:feb1f0c0 COREB:  sm_recv_packet msg

sm_debug:    28 : 27

sm_debug:received 28

sm_debug:feb1f100 COREB: processing msg 123

sm_debug:    29 : 28

sm_debug:received 29

sm_debug:feb1f140 COREB: coreb send buf 3d01000

sm_debug:    30 : 29

sm_debug:received 30

sm_debug:feb1f180 COREB: sm_send_packet() in pool 3d01000 finish

sm_debug:    31 : 30

sm_debug:received 31

sm_debug:feb1f1c0 COREB: sm_default_sendmsg msg type 4000000

sm_debug:    32 : 31

sm_debug:received 32

sm_debug:feb1f000 COREB: sm_send_message_internal() dst 0 src 1 4000000

sm_debug:    33 : 32

sm_debug:received 33

sm_debug:sm_find_session bits 00000001 localep 9

sm_debug:index 0 ,local ep 9 type 4

sm_debug:session 0292a800 index 0 msg type4000000

sm_debug:sm_default_recvmsg msg type 4000000

sm_debug:msg_recv_internal wakeup wait thread

sm_debug:received 34

sm_debug:feb1f080 COREB: sm_send_message_internal() dst 0 src 1 4000001

sm_debug:    35 : 33

sm_debug:received 35

sm_debug:sm_find_session bits 00000001 localep 9

sm_debug:index 0 ,local ep 9 type 4

sm_debug:session 0292a800 index 0 msg type4000001

sm_debug:sm_default_recvmsg msg type 4000001

sm_debug:ack matched free buf 29483c0

sm_debug:received 36

sm_debug:feb1f100 COREB: free message 3d40000

sm_debug:    37 : 35

sm_debug:received 37

sm_debug:feb1f140 COREB: task loop

sm_d

Follow-ups

--- steven miao                                              2011-07-29 02:31:07

fixed, the crash is caused by memset the wrong buffer address

--- Mingquan Pan                                             2011-09-07 05:03:41

Yes, running packet case doesn't print dump info now. So close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.