Article [#6807] kernel not starting(2011)

[#6807] kernel not starting

Submitted By: Chris Page

Open Date

2011-10-04 11:27:35     Close Date

2011-10-10 02:45:04

Priority:

Medium High     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2010R1-RC5     Release:

Category:

N/A     Board:

STAMP

Processor:

ALL     Silicon Revision:

0.3

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

2010R1-RC2     Toolchain version or rev.:

(ADI-2010R1-RC4) 4.3.5

App binary format:

FLAT     

Summary: kernel not starting

Details:

I am updating from kernel release 2009 which works great to 2010R1-RC5.

The configuration files are identical. The later release is getting hung and I have no idea why. It does not output anything. There is no activity at all. I am completely out of ideas.

The kernel is getting hung trying to start

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf537-2.6.34.7-ADI-2010R1

   Created:      2011-10-04  15:08:18 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    4077056 Bytes = 3.9 MiB

   Load Address: 00001000

   Entry Point:  001ed61c

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 001ed61c

The issue is similar to

http://blackfin.uclinux.org/gf/project/uclinux-dist/forum/?_forum_action=ForumMessageBrowse&thread_id=45292&action=ForumBrowse

Message: 100376

I have confirmed that CONFIG_MTD_UCLINUX is not set. I have enabled early printk and nothing is output. Here are my u-boot arguments.

bootargs=root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,115200 console=ttyBF0,115200

bootcmd=run nandboot

baudrate=115200

loads_echo=1

ipaddr=10.137.202.2

serverip=10.137.202.1

rootpath=/romfs

gatewayip=10.137.202.1

netmask=255.255.255.0

hostname=bf537-tft

loadaddr=0x1000000

nandboot=nand read.jffs2 0x1000000 0x1000000 0x1000000;bootm 0x1000000

stdin=serial

stdout=serial

stderr=serial

ethact=bfin_mac

I have also enabled the console so I do not believe that is the issue. Any help on what I should try would be great. I have also attached a bug report.

Follow-ups

--- Chris Page                                               2011-10-04 19:19:56

Never mind I copied and modified the new stamp.c and it worked. I am not exactly

sure what I changed to get it to work. Please close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

bugreport.tar.gz    application/x-gzip    20100    Chris Page

Attachments:

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.