Article [#6811] Fail to build bind app in latest trunk(2011)

[#6811] Fail to build bind app in latest trunk

Submitted By: Vivi Li

Open Date

2011-10-12 03:19:57     Close Date

2011-10-18 02:12:52

Priority:

Medium     Assignee:

Nobody

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

ALL     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2011R1-RC1

App binary format:

N/A     

Summary: Fail to build bind app in latest trunk

Details:

Fail to build bind app in latest trunk. It fails in configuration at openssl.

Bellow is the log:

--

checking build system type... (cached) i686-pc-linux-gnu

checking host system type... (cached) bfin-unknown-uclinux

checking whether make sets $(MAKE)... (cached) yes

checking for bfin-uclinux-ranlib... (cached) bfin-uclinux-ranlib

checking for a BSD-compatible install... (cached) /usr/bin/install -c

checking for ar... /usr/bin/ar

checking for etags... /usr/bin/etags

checking for Exuberant Ctags etags... no

checking for perl5...   GEN     /home/test/work/cruise/checkouts/uclinux-dist/user/busybox/build-busybox-1.18.4/Makefile

no

checking for perl... /usr/bin/perl

checking for bfin-uclinux-gcc... (cached) bfin-uclinux-gcc

checking for C compiler default output file name... a.out

checking whether the C compiler works... yes

checking whether we are cross compiling... yes

checking for suffix of executables...

checking for suffix of object files... (cached) o

checking whether we are using the GNU C compiler... (cached) yes

checking whether bfin-uclinux-gcc accepts -g... (cached) yes

checking for bfin-uclinux-gcc option to accept ANSI C... none needed

checking how to run the C preprocessor... (cached) bfin-uclinux-gcc -E

checking for egrep... grep -E

checking for ANSI C header files... yes

checking for fcntl.h... (cached) yes

checking for sys/time.h... (cached) yes

checking for unistd.h... (cached) yes

checking for sys/sockio.h... no

checking for sys/select.h... (cached) yes

checking for sys/param.h... (cached) yes

checking for sys/sysctl.h... (cached) yes

checking for net/if6.h... no

checking for an ANSI C-conforming const... (cached) yes

checking for inline... (cached) inline

checking for sysctlbyname... no

checking for static inline breakage... yes

checking for sys/types.h... (cached) yes

checking for sys/stat.h... (cached) yes

checking for stdlib.h... (cached) yes

checking for string.h... (cached) yes

checking for memory.h... (cached) yes

checking for strings.h... (cached) yes

checking for inttypes.h... (cached) yes

checking for stdint.h... (cached) yes

checking for unistd.h... (cached) yes

checking for size_t... (cached) yes

checking for ssize_t... (cached) yes

checking for uintptr_t... (cached) yes

checking for socklen_t... yes

checking whether time.h and sys/time.h may both be included... yes

checking for long long... yes

checking for struct lifconf... no

checking if unistd.h or sys/types.h defines fd_set... yes

checking whether byte ordering is bigendian... (cached) no

checking for OpenSSL library... using openssl from /usr/include/openssl/lib and /usr/include/openssl/include

checking whether linking with OpenSSL works... assuming it does work on target platform

checking whether linking with OpenSSL requires -ldl... unknown

configure: error: OpenSSL has unsupported dynamic loading

make[3]: *** [builddir] Error 1

--

Follow-ups

--- Sonic Zhang                                              2011-10-13 04:01:43

If you installed openssl in your host pc, make sure you install all development

components. Otherwise, please build bind without host openssl by add

--without-openssl to configure parameters.

--- Sonic Zhang                                              2011-10-13 06:46:10

Disable openssl configure option if ssl library is not built.

--- Vivi Li                                                  2011-10-18 02:17:57

OK now.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.