Article [#6845] ubifs errors after updating kernel.(2011)

[#6845] ubifs errors after updating kernel.

Submitted By: Chris Page

Open Date

2011-10-25 15:40:35    

Priority:

Medium High     Assignee:

Aaron Wu

Status:

Open     Fixed In Release:

N/A

Found In Release:

2010R1-RC5     Release:

2010R1-RC5

Category:

Memory     Board:

Custom

Processor:

BF537     Silicon Revision:

3

Is this bug repeatable?:

Yes     Resolution:

Out of Date

Uboot version or rev.:

2010R1-RC2     Toolchain version or rev.:

4.3.5

App binary format:

N/A     

Summary: ubifs errors after updating kernel.

Details:

This is the same error as [#6839] (ubifs issues while updating kernel. 2010r1-rc5 mounted nand). I have had to create another bug report because it was closed without a proper resolution.

After further testing there seems to be an issue with the ubi/nand driver and

large nands. When I use the later kernel with a smaller nand device it seemed to

work fine. I went from using a NAND04GW (4Gbit) which gave me errors shown below to a smaller NAND512 (512Mbit) that worked fine.

The driver does not appear to handle large partitions. When I use a 400M BYTE

partition and move large files (10 M BYTES) back and forth from the nand to ram I get these errors after resetting and trying to copy them from nand to ram. I Noticed you were using a small nand with a small partition (around 2 M Bytes) and tested using small files.

Have you tested a large NAND memory with large files? The file system should be

able to handle this.

So to get these errors.

1.Use a large nand partition ~400 Mbytes.

2.Format the partition

3.Move large files ~10 Mbytes back and forth from nand to ram.

4.RESET the board.

5. Remount the partition and try moving large files again.

6. Repeat resetting and moving files and after a couple of attempts you will get these errors.

/* ERRORS */

uncorrectable error :

UBI error: ubi_io_read: error -74 while reading 2836 bytes from PEB 43:73120, read 2836 bytes

UBIFS error (pid 327): try_read_node: cannot read node type 1 from LEB 21:71072, error -74

UBIFS error (pid 327): ubifs_read_node: bad node type (17 but expected 0)

UBIFS error (pid 327): ubifs_read_node: bad node at LEB 15:10056

UBIFS error (pid 327): ubifs_iget: failed to read inode 74, error -22

UBIFS error (pid 327): ubifs_lookup: dead directory entry 'variance.so', error -22

UBIFS warning (pid 327): ubifs_ro_mode: switched to read-only mode, error -22

UBI: scrubbed PEB 2106 (LEB 0:15), data moved to PEB 2107

UBIFS error (pid 327): ubifs_read_node: bad node type (0 but expected 9)

UBIFS error (pid 327): ubifs_read_node: bad node at LEB 14:107304

UBIFS error (pid 327): ubifs_iget: failed to read inode 91, error -22

UBIFS error (pid 327): ubifs_lookup: dead directory entry 'prog2', error -22

UBI: scrubbed PEB 2105 (LEB 0:14), data moved to PEB 2106

Follow-ups

--- Sonic Zhang                                              2011-10-25 23:09:30

bug 6839 is duplicated to 6840. Why not comments in 6840 instead of submitting a

new one?

https://blackfin.uclinux.org/gf/tracker/6840

Bugs item #6840, was opened at 2011-10-24 19:46:38

Priority: 2

Submitted By: Chris Page (cpage3)

Assigned to: Aaron Wu (aaronwu1)

Summary: ubifs issues while updating kernel. 2010r1-rc5 mounted nand

Status: Open

--- Chris Page                                               2011-10-26 11:21:58

Hi

Since 6840 has been closed I will continue to use this bug report. Both of the

chips I am using are correctly identified by the nand driver. As can be seen in

startup code (NAND device: Manufacturer ID: 0x20, Chip ID: 0xdc (ST Micro NAND

512MiB 3,3V 8-bit)

)

In nand_ids.c the configuration is already done {"NAND 512MiB 3,3V

8-bit",    0xDC, 0, 512, 0, LP_OPTIONS}, and the page size and erase size are

determined from the extended id bytes.  I have done all of the mtd tests and

passed. 

The nand is in the mainline kernel and there is a bug. After more testing I

believe the errors are more of a result of large files ~10MByte been read and

written from ram to nand then resetting the board after the write or read has

completed.

--- Aaron Wu                                                 2011-10-26 21:18:06

Thanks for the detailed info, did you do sync before resetting? Or will a

regular shutdown routine cause the same problem? Data in buffer may get lost if

press the reset or remove power suddenly

--- Chris Page                                               2011-10-26 23:19:51

Hi

Yes I make sure to sync every time. I even wait just to make sure there is no

data loss in the buffers. I have managed to get the same errors with files

around 2 Mega bytes in size. Files around 50 to 500 KBytes seem to be ok. 

--- Chris Page                                               2011-10-28 15:04:13

Hi

I Would like to know the status of the bug.

--- Mingquan Pan                                             2011-10-31 02:28:25

HI, I have tried as you described in the tracker. Use a large file as you said

(10 M gfortran.log), with a partition to 100M.

Bytes transferred = 10621357 (a211ad hex)

## Booting kernel from Legacy Image at 01000000 ...

   Image Name:   bf548-0.2-3.0.0-ADI-2011R1-pre-s

   Created:      2011-10-28  19:09:49 UTC

   Image Type:   Blackfin Linux Kernel Image (gzip compressed)

   Data Size:    10621293 Bytes = 10.1 MiB

   Load Address: 00001000

   Entry Point:  002a1e48

   Verifying Checksum ... OK

   Uncompressing Kernel Image ... OK

Starting Kernel at = 002a1e48

Linux version 3.0.0-ADI-2011R1-pre-svn10111 (test@uclinux61-bf548-std) (gcc

version 4.3.5 (ADI-2011R1-RC2) ) #8 Sat Oct 29 03:09:41 CST 2011

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart1] enabled

early printk enabled on early_BFuart1

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001cf960

  rodata    = 0x001cf960-0x00269248

  bss       = 0x0026a000-0x0027c43c

  data      = 0x0027c43c-0x00298000

    stack   = 0x00296000-0x00298000

  init      = 0x00298000-0x011b8000

  available = 0x011b8000-0x03e00000

  DMA Zone  = 0x03e00000-0x04000000

Hardware Trace active and enabled

Boot Mode: 1

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF548 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 525 MHz core clock and 131 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

  L2 SRAM        : uncacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-through) in data cache

  L2 SRAM        : uncacheable in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 15748

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000

earlyprintk=serial,uart1,57600 console=ttyBF1,57600

ip=10.100.4.50:10.100.4.174:10.100.4.174:255.255.255.0:bf548-ezkit:eth0:off

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 44736k/65536k RAM, (15488k init code, 1850k kernel code, 802k

data, 2048k dma, 612k reserved)

NR_IRQS:295

Configuring Blackfin Priority Driven Interrupts

console [ttyBF1] enabled, bootconsole disabled

console [ttyBF1] enabled, bootconsole disabled

Calibrating delay loop... 1044.48 BogoMIPS (lpj=2088960)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (41 KB free)

Blackfin L2 SRAM: 128 KB (128 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

ezkit_init(): registering device resources

bio: create slab <bio-0> at 0

SCSI subsystem initialized

spi spi0.2: Warning: SPI CPHA not set: Slave Select not under software

control!

See Documentation/blackfin/bfin-spi-notes.txt

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs@ffc00500, dma channel@4

bfin-spi bfin-spi.1: Blackfin on-chip SPI Controller Driver, Version 1.0,

regs@ffc02300, dma channel@5

i2c-bfin-twi i2c-bfin-twi.0: Blackfin BF5xx on-chip I2C TWI Contoller,

regs_base@ffc00700

i2c-bfin-twi i2c-bfin-twi.1: Blackfin BF5xx on-chip I2C TWI Contoller,

regs_base@ffc02200

Advanced Linux Sound Architecture Driver Version 1.0.24.

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 87

io scheduler noop registered (default)

bf54x-lq043: FrameBuffer initializing...

dma_alloc_init: dma_page @ 0x029f7000 - 512 pages at 0x03e00000

bfin-uart: Blackfin serial driver

bfin-uart.1: ttyBF1 at MMIO 0xffc02000 (irq = 48) is a BFIN-UART

bfin-otp: initialized

brd: module loaded

register bfin atapi driver

scsi0 : pata-bf54x

ata1: PATA max UDMA/66 irq 68

physmap platform flash device: 02000000 at 20000000

physmap-flash.0: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID

0x000089 Chip ID 0x00881e

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Intel/Sharp Extended Query Table at 0x010A

Using buffer write method

Using auto-unlock on power-up/resume

cfi_cmdset_0001: Erase suspend on write enabled

Using physmap partition information

Creating 5 MTD partitions on "physmap-flash.0":

0x000000000000-0x000000080000 : "bootloader(nor)"

0x000000080000-0x000000480000 : "linux kernel(nor)"

0x000000480000-0x000000fe0000 : "file system(nor)"

0x000000fe0000-0x000000ff8000 : "config(nor)"

0x000000ff8000-0x000001000000 : "u-boot env(nor)"

m25p80 spi0.1: m25p16 (2048 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x000000000000-0x000000080000 : "bootloader(spi)"

0x000000080000-0x000000200000 : "linux kernel(spi)"

BF5xx on-chip NAND FLash Controller Driver, Version 1.2 (c) 2007 Analog

Devices, Inc.

bf5xx-nand bf5xx-nand.0: data_width=8, wr_dly=3, rd_dly=3

NAND device: Manufacturer ID: 0x20, Chip ID: 0xda (ST Micro NAND 256MiB 3,3V

8-bit)

Creating 3 MTD partitions on "NAND 256MiB 3,3V 8-bit":

0x000000000000-0x000000080000 : "bootloader(nand)"

0x000000080000-0x000000480000 : "linux kernel(nand)"

0x000000480000-0x000010000000 : "file system(nand)"

smsc911x: Driver version 2008-10-21

smsc911x-mdio: probed

smsc911x smsc911x.0: eth0: attached PHY driver [Generic PHY]

(mii_bus:phy_addr=0:01, irq=-1)

smsc911x smsc911x.0: eth0: MAC Address: 00:e0:22:fe:bf:4e

input: bf54x-keys as /devices/platform/bf54x-keys/input/input0

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

i2c /dev entries driver

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 2004-06-01 06:15:29 UTC

(1086070529)

smsc911x smsc911x.0: eth0: SMSC911x/921x identified at 0x24000000, IRQ: 175

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf548-ezkit, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

mmc0: host does not support reading read-only switch. assuming write-enable.

mmc0: new SD card at address e624

ata1.00: ATA-6: TOSHIBA MK4032GAX, AD101A, max UDMA/100

ata1.00: 78140160 sectors, multi 16: LBA48

ata1.00: configured for UDMA/66

blk_queue_max_segments: set to minimum 1

scsi 0:0:0:0: Direct-Access     ATA      TOSHIBA MK4032GA AD10 PQ: 0 ANSI: 5

sd 0:0:0:0: [sda] 78140160 512-byte logical blocks: (40.0 GB/37.2 GiB)

sd 0:0:0:0: [sda] Write Protect is off

sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support

DPO or FUA

sda: sda1 sda2

sd 0:0:0:0: [sda] Attached SCSI disk

Freeing unused kernel memory: 15488k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - https://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.18.4 (2011-10-28 19:10:29 CST) hush - the humble shell

root:/>  ubiattach /dev/ubi_ctrl -m 9

UBI: attaching mtd9 to ubi0

UBI: physical eraseblock size:   131072 bytes (128 KiB)

UBI: logical eraseblock size:    129024 bytes

UBI: smallest flash I/O unit:    2048

UBI: sub-page size:              512

UBI: VID header offset:          512 (aligned 512)

UBI: data offset:                2048

UBI: max. sequence number:       79

UBI: attached mtd9 to ubi0

UBI: MTD device name:            "file system(nand)"

UBI: MTD device size:            251 MiB

UBI: number of good PEBs:        2012

UBI: number of bad PEBs:         0

UBI: number of corrupted PEBs:   0

UBI: max. allowed volumes:       128

UBI: wear-leveling threshold:    4096

UBI: number of internal volumes: 1

UBI: number of user volumes:     1

UBI: available PEBs:             1175

UBI: total number of reserved PEBs: 837

UBI: number of PEBs reserved for bad PEB handling: 20

UBI: max/mean erase counter: 846/359

UBI: image sequence number:  1622483402

UBI: background thread "ubi_bgt0d" started, PID 329

UBI device number 0, total 2012 LEBs (259596288 bytes, 247.6 MiB), available

1175 LEBs (151603200 bytes, 144.6 MiB), LEB size 129024 bytes (126.0 KiB)

root:/> mount -t ubifs ubi0:ubifs0 /mnt

UBIFS: mounted UBI device 0, volume 0, name "ubifs0"

UBIFS: file system size:   103606272 bytes (101178 KiB, 98 MiB, 803 LEBs)

UBIFS: journal size:       5160960 bytes (5040 KiB, 4 MiB, 40 LEBs)

UBIFS: media format:       w4/r0 (latest is w4/r0)

UBIFS: default compressor: lzo

UBIFS: reserved for root:  4893579 bytes (4778 KiB)

root:/> ls /mnt/

2                 3                 gfortran-4.3.log

root:/> cp /mnt/gfortran-4.3.log /home/

root:/> cp /mnt/gfortran-4.3.log /

root:/> cp gfortran-4.3.log /mnt/3/

root:/> cp gfortran-4.3.log /mnt/3/

root:/> cp gfortran-4.3.log /mnt/3/

root:/> ls -lh gfortran-4.3.log

-rwxr-xr-x    1 root     root       11.5M Jun  1 06:16 gfortran-4.3.log

root:/> umount /mnt/

UBIFS: un-mount UBI device 0, volume 0

root:/>

root:/> reboot

sd 0:0:0:0: [sda] Synchronizing SCSI cache

Restarting system.

U-Boot 2010.06-svn2467 (ADI-2010R1) (Oct 08 2010 - 16:04:41)

CPU:   ADSP bf548-0.0 (Detected Rev: 0.2) (parallel flash boot)

Board: ADI BF548 EZ-Kit board

       Support: http://blackfin.uclinux.org/

Clock: VCO: 525 MHz, Core: 525 MHz, System: 131.250 MHz

RAM:   64 MiB

Flash: 16 MiB

NAND:  256 MiB

MMC:  Blackfin SDH: 0

In:    serial

Out:   serial

Err:   serial

KGDB:  [on serial] ready

Net:   smc911x-0

Hit any key to stop autoboot:  0

I run this successively for serveral times and copy gfortran.log to and from

/mnt and root directory every time, I don't see your error message and it can

work ok.

--- Aaron Wu                                                 2011-10-31 03:55:17

Thanks Grace for verification on the trunk. I tried reading/writing to and from

the ubifs partition of 243MB with a large file of 10MB, then reset, reboot,

repeating for a couple of times. I see no difference.

--- Aaron Wu                                                 2011-10-31 03:56:30

My test is done on 2010R1 release with a bf548 board with NAND on it.

--- Chris Page                                               2011-10-31 17:57:03

I will post on the forum to see if anybody else can reproduce this. The nand

device is in the mainline kernel, passes all mtd tests. The nand works when I

use 2009R1. Once I updated to 2010R1-RC5 I get these errors. Thanks for

checking. I am shocked it is not reproducible. Which 2010R1 release candidate

were you using? Maybe I will try that.   

--- Aaron Wu                                                 2011-11-01 01:06:31

The standard 2010R1 release. SVN rev 9993.

--- Chris Page                                               2011-11-08 10:16:40

I am using the same. The bug has nothing to do with the files. There is a bug

with the ST Micro Nand Flash on EBIU. Both of the nand flashes I was checking

were ST Micro. I am not the only one. Look at the following links. Similar

issues even on the latest kernel.

http://blackfin.uclinux.org/gf/project/uclinux-dist/forum/?_forum_action=ForumMessageBrowse&thread_id=42812&action=ForumBrowse

https://ez.analog.com/thread/9923

Remember I only got these errors after updating to 2010R1.

--- Chris Page                                               2011-11-08 13:26:14

In addition to what I just posted I wanted to note these issues also arise with

the bf537. The bf54x use the Blackfin on-chip NAND Flash Controller drive which

the bf537 does not. This is a bug with the 537 and ST Micro Nand Flash.

--- Sonic Zhang                                              2011-11-08 22:06:39

We don't have your ST Macro Nand Flash addon board for bf537-stamp. If you could

ship one to us, we can help to debug.

--- Chris Page                                               2011-11-08 23:27:05

Could you please provide me with you shipping address. Who should I make it out

to? I could will send one of our boards with the NAND on it. Programs the same

as a stamp board. I will also send a separate NAND flash.

--- Aaron Wu                                                 2011-11-09 00:18:12

Hi Chris,

We just tried the BF537 aync interface for a ST NAND01GW chip on 2010R1

release, we see no problem. Likely your problem happens on specific chip.

ubiattach /dev/ubi_ctrl -m 1

UBI: attaching mtd1 to ubi0

UBI: physical eraseblock size:   131072 bytes (128 KiB)

UBI: logical eraseblock size:    129024 bytes

UBI: smallest flash I/O unit:    2048

UBI: sub-page size:              512

UBI: VID header offset:          512 (aligned 512)

UBI: data offset:                2048

UBI: attached mtd1 to ubi0

UBI: MTD device name:            "file system(nand)"

UBI: MTD device size:            124 MiB

UBI: number of good PEBs:        992

UBI: number of bad PEBs:         0

UBI: max. allowed volumes:       128

UBI: wear-leveling threshold:    4096

UBI: number of internal volumes: 1

UBI: number of user volumes:     1

UBI: available PEBs:             816

UBI: total number of reserved PEBs: 176

UBI: number of PEBs reserved for bad PEB handling: 9

UBI: max/mean erase counter: 2/1

UBI: image sequence number: 0

UBI: background thread "ubi_bgt0d" started, PID 228

UBI device number 0, total 992 LEBs (127991808 bytes, 122.1 MiB), available 816

LEBs (105283584 bytes, 100.4 MiB), LEB size 129024 bytes (126.0 KiB)

root:/> mount -t ubifs ubi0:ubifs0 /mnt

UBIFS: mounted UBI device 0, volume 0, name "ubifs0"

UBIFS: file system size:   19869696 bytes (19404 KiB, 18 MiB, 154 LEBs)

UBIFS: journal size:       1032193 bytes (1008 KiB, 0 MiB, 8 LEBs)

UBIFS: media format:       w4/r0 (latest is w4/r0)

UBIFS: default compressor: lzo

UBIFS: reserved for root:  938494 bytes (916 KiB)

root:/> cp test_data /mnt

--- Aaron Wu                                                 2011-11-09 00:27:36

Hi Chris, here is the adress:

10F, 1010-1018, One corporate Avenue, 222 Hubin Road, Shanghai, 200021, China.

Please ship to Aaron Wu.

Telephone: 8621-23208064

Yes please ship us a suite of your board, with other hardware stuffs like power

supply etc, and share me information about how to boot it. Please also send a

seperate Nand Chip.

--- Chris Page                                               2011-11-09 21:41:24

Hi Aaron,

As I was going through all the steps to program, recreate, and test the board

before I shipped it I think I figured something out. From u-boot I would erase

and clean the nand. I would then boot the image and format and mount the ubi.

This time I did a flash_eraseall (from the kernel) before formatting the UBI and

it seems to work. I had tried to flash_eraseall before but used the -j option.

With the -j option it didn't work (not sure if it has something to do with not

having gluebi configured) in this newer release. So flash_eraseall before

formatting seems to have corrected it. I will be doing more tests tomorrow and

throughout the week to make sure. If the errors arise again I will let you know.

Thanks for your patience and your help.   

--- Sonic Zhang                                              2011-12-09 05:02:34

No follow up information from customers.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

bugreport.tar.gz    application/x-gzip    20225    Chris Page

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.