Article [#6848] Can not detect ad1836 on bf533-stamp in latest trunk(2011)

[#6848] Can not detect ad1836 on bf533-stamp in latest trunk

Submitted By: Vivi Li

Open Date

2011-10-26 03:46:42     Close Date

2012-01-16 01:59:47

Priority:

Medium     Assignee:

Scott Jiang

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF533     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2011R1-RC2

App binary format:

FDPIC     

Summary: Can not detect ad1836 on bf533-stamp in latest trunk

Details:

Can not detect ad1836 on bf533-stamp in latest trunk.

BF537-STAMP is OK.

--

Linux version 3.0.0-ADI-2011R1-pre-svn10098 (test@ulinux77-533stamp-ad1836) (gcc version 4.3.5 (ADI-2011R1-RC2) ) #498 Tue Oct 21

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 128MB

Kernel Managed Memory: 128MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x001492e8

  rodata    = 0x001492e8-0x001b2138

  bss       = 0x001b3000-0x001c329c

  data      = 0x001c329c-0x001d4000

    stack   = 0x001d2000-0x001d4000

  init      = 0x001d4000-0x0086a000

  available = 0x0086a000-0x03800000

  DMA Zone  = 0x07e00000-0x08000000

Hardware Trace active and enabled

Boot Mode: 0

Reset caused by Software reset

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF533 Rev 0.3

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 497 MHz core clock and 82 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=11059200 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 48120k/131072k RAM, (6744k init code, 1312k kernel code, 556k data, 2048k dma, 72292k reserved)

NR_IRQS:81

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 989.18 BogoMIPS (lpj=1978368)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 64 KB (51 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@5

Advanced Linux Sound Architecture Driver Version 1.0.24.

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 93

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 21) is a BFIN-UART

brd: module loaded

smc91x.c: v1.1, sep 22 2004 by Nicolas Pitre <nico@fluxnic.net>

eth0: SMC91C11xFD (rev 1) at 20300300 IRQ 40 [nowait]

eth0: Ethernet addr: 00:e0:22:fe:07:5b

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

bfin-tdm bfin-tdm.0: no platform_data

ALSA device list:

  No soundcards found.

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 08:02:59 UTC (28979)

smc91x smc91x.0: eth0: link down

smc91x smc91x.0: eth0: link up, 100Mbps, full-duplex, lpa 0x45E1

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf533-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

dma_alloc_init: dma_page @ 0x02874000 - 512 pages at 0x07e00000

Freeing unused kernel memory: 6744k freed

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - https://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.18.4 (2011-10-25 03:54:04 CST) hush - the humble shell

root:/> version

kernel:    Linux release 3.0.0-ADI-2011R1-pre-svn10098, build #498 Tue Oct 25 03:56:23 CST 2011

toolchain: bfin-linux-uclibc-gcc release gcc version 4.3.5 (ADI-2011R1-RC2)

user-dist: release svn-10450, build #6338 Tue Oct 25 03:54:28 CST 2011

root:/>

--

Follow-ups

--- Scott Jiang                                              2011-10-27 23:34:46

fixed

--- Vivi Li                                                  2012-01-16 02:28:13

AD1836 can be detected in trunk.

Close this bug.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.config.audio_ad1836    application/octet-stream    51955    Vivi Li

config.linux.audio_ad1836    application/octet-stream    34452    Vivi Li

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.