Article [#6877] Fail to use wireless cf card on bf537-stamp in 2011r1 branch(2011)

[#6877] Fail to use wireless cf card on bf537-stamp in 2011r1 branch

Submitted By: Vivi Li

Open Date

2011-11-14 00:26:48     Close Date

2011-11-25 01:40:34

Priority:

Medium High     Assignee:

steven miao

Status:

Closed     Fixed In Release:

N/A

Found In Release:

2011R1     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Rejected

Uboot version or rev.:

    Toolchain version or rev.:

gcc4.3-2011R1-RC2

App binary format:

FLAT     

Summary: Fail to use wireless cf card on bf537-stamp in 2011r1 branch

Details:

Fail to use wireless cf card on bf537-stamp in 2011r1 branch.

It passed in 2010r1 branch.

--

Linux version 3.0.8-ADI-2011R1-svn10227 (test@uclinux50-bf537-9960-1836) (gcc version 4.3.5 (ADI-2011R1-RC2) ) #12 Sun Nov 13 211

register early platform devices

bootconsole [early_shadow0] enabled

bootconsole [early_BFuart0] enabled

early printk enabled on early_BFuart0

Limiting kernel memory to 56MB due to anomaly 05000263

Board Memory: 64MB

Kernel Managed Memory: 64MB

Memory map:

  fixedcode = 0x00000400-0x00000490

  text      = 0x00001000-0x00162118

  rodata    = 0x00162118-0x001d1fb4

  bss       = 0x001d2000-0x001e1c7c

  data      = 0x001e1c7c-0x001f6000

    stack   = 0x001f4000-0x001f6000

  init      = 0x001f6000-0x009a2000

  available = 0x009a2000-0x03800000

  DMA Zone  = 0x03f00000-0x04000000

Hardware Trace active and enabled

Boot Mode: 0

Blackfin support (C) 2004-2010 Analog Devices, Inc.

Compiled for ADSP-BF537 Rev 0.2

Blackfin Linux support by http://blackfin.uclinux.org/

Processor Speed: 500 MHz core clock and 62 MHz System Clock

NOMPU: setting up cplb tables

Instruction Cache Enabled for CPU0

  External memory: cacheable in instruction cache

Data Cache Enabled for CPU0

  External memory: cacheable (write-back) in data cache

Built 1 zonelists in Zone order, mobility grouping off.  Total pages: 14224

Kernel command line: root=/dev/mtdblock0 rw clkin_hz=25000000 earlyprintk=serial,uart0,57600 console=ttyBF0,57600 ip=10.100.4.50f

PID hash table entries: 256 (order: -2, 1024 bytes)

Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)

Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)

Memory available: 46872k/65536k RAM, (7856k init code, 1412k kernel code, 592k data, 1024k dma, 7780k reserved)

NR_IRQS:146

Configuring Blackfin Priority Driven Interrupts

console [ttyBF0] enabled, bootconsole disabled

console [ttyBF0] enabled, bootconsole disabled

Calibrating delay loop... 995.32 BogoMIPS (lpj=1990656)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

Blackfin Scratchpad data SRAM: 4 KB

Blackfin L1 Data A SRAM: 16 KB (16 KB free)

Blackfin L1 Data B SRAM: 16 KB (16 KB free)

Blackfin L1 Instruction SRAM: 48 KB (34 KB free)

NET: Registered protocol family 16

Blackfin DMA Controller

stamp_init(): registering device resources

bio: create slab <bio-0> at 0

bfin-spi bfin-spi.0: Blackfin on-chip SPI Controller Driver, Version 1.0, regs@ffc00500, dma channel@7

cfg80211: Calling CRDA to update world regulatory domain

Switching to clocksource bfin_cs_cycles

NET: Registered protocol family 2

IP route cache hash table entries: 1024 (order: 0, 4096 bytes)

TCP established hash table entries: 2048 (order: 2, 16384 bytes)

TCP bind hash table entries: 2048 (order: 1, 8192 bytes)

TCP: Hash tables configured (established 2048 bind 2048)

TCP reno registered

UDP hash table entries: 256 (order: 0, 4096 bytes)

UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)

NET: Registered protocol family 1

debug-mmrs: setting up Blackfin MMR debugfs

msgmni has been set to 91

io scheduler noop registered (default)

bfin-uart: Blackfin serial driver

bfin-uart.0: ttyBF0 at MMIO 0xffc00400 (irq = 18) is a BFIN-UART

brd: module loaded

bfin_mii_bus: probed

bfin_mac: attached PHY driver [SMSC LAN83C185] (mii_bus:phy_addr=0:01, irq=-1, mdc_clk=2500000Hz(mdc_div=11)@sclk=62MHz)

bfin_mac bfin_mac.0: eth0: Blackfin on-chip Ethernet MAC driver, Version 1.1

bfin_cf_pcmcia bfin_cf_pcmcia: Blackfin CompactFlash/PCMCIA Socket Driver

bfin_cf_pcmcia bfin_cf_pcmcia: : on irq 54

rtc-bfin rtc-bfin: rtc core: registered rtc-bfin as rtc0

bfin-wdt: initialized: timeout=20 sec (nowayout=0)

TCP cubic registered

NET: Registered protocol family 17

rtc-bfin rtc-bfin: setting system clock to 1970-01-01 00:09:32 UTC (572)

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

dma_alloc_init: dma_page @ 0x0294b000 - 256 pages at 0x03f00000

Freeing unused kernel memory: 7856k freed

pcmcia_socket pcmcia_socket0: pccard: PCMCIA card inserted into slot 0

pcmcia 0.0: pcmcia: registering new device pcmcia0.0 (IRQ: 54)

                           _____________________________________

        a8888b.           / Welcome to the uClinux distribution \

       d888888b.         /       _     _                         \

       8P"YP"Y88        /       | |   |_|            __  __ (TM)  |

       8|o||o|88  _____/        | |    _ ____  _   _ \ \/ /       |

       8'    .88       \        | |   | |  _ \| | | | \  /        |

       8`._.' Y8.       \       | |__ | | | | | |_| | /  \        |

      d/      `8b.       \      \____||_|_| |_|\____|/_/\_\       |

     dP   .    Y8b.       \   For embedded processors including   |

    d8:'  "  `::88b        \    the Analog Devices Blackfin      /

   d8"         'Y88b        \___________________________________/

  :8P    '      :888

   8a.   :     _a88P         For further information, check out:

._/"Yaa_:   .| 88P|            - http://blackfin.uclinux.org/

\    YP"    `| 8P  `.          - http://docs.blackfin.uclinux.org/

/     \.___.d|    .'           - http://www.uclinux.org/

`--..__)8888P`._.'  jgs/a:f    - https://www.analog.com/blackfin

Have a lot of fun...

BusyBox v1.18.4 (2011-11-13 20:56:50 CST) hush - the humble shell

root:/> PHY: 0:01 - Link is Up - 100/Full

root:/> version

kernel:    Linux release 3.0.8-ADI-2011R1-svn10227, build #12 Sun Nov 13 21:38:25 CST 2011

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2011R1-RC2)

user-dist: release svn-10489, build #167 Sun Nov 13 21:37:46 CST 2011

root:/>

root:/> modprobe orinoco_cs

root:/> lsmod

Module                  Size  Used by

orinoco_cs              4053  0

orinoco                47894  1 orinoco_cs

root:/> ifconfig

eth0      Link encap:Ethernet  HWaddr 00:E0:22:FE:00:03

          inet addr:10.100.4.50  Bcast:10.100.4.255  Mask:255.255.255.0

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:2 errors:0 dropped:0 overruns:0 frame:0

          TX packets:1 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:120 (120.0 B)  TX bytes:42 (42.0 B)

lo        Link encap:Local Loopback

          inet addr:127.0.0.1  Mask:255.0.0.0

          UP LOOPBACK RUNNING  MTU:16436  Metric:1

          RX packets:0 errors:0 dropped:0 overruns:0 frame:0

          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:0

          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

root:/> dmesg |tail

IP-Config: Complete:

     device=eth0, addr=10.100.4.50, mask=255.255.255.0, gw=10.100.4.174,

     host=bf537-stamp, domain=, nis-domain=(none),

     bootserver=10.100.4.174, rootserver=10.100.4.174, rootpath=

dma_alloc_init: dma_page @ 0x0294b000 - 256 pages at 0x03f00000

Freeing unused kernel memory: 7856k freed

pcmcia_socket pcmcia_socket0: pccard: PCMCIA card inserted into slot 0

pcmcia 0.0: pcmcia: registering new device pcmcia0.0 (IRQ: 54)

PHY: 0:01 - Link is Up - 100/Full

orinoco 0.15 (David Gibson <hermes@gibson.dropbear.id.au>, Pavel Roskin <proski@gnu.org>, et al)

root:/>

--

Follow-ups

--- steven miao                                              2011-11-23 22:12:21

it works in 2011R1, maybe it's a hardware issue

--- steven miao                                              2011-11-24 00:35:02

need Support Prism 2/2.5 chipset selected now

--- Vivi Li                                                  2011-11-25 01:55:30

OK.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.config.wireless    application/octet-stream    52126    Vivi Li

config.linux.wireless    application/octet-stream    37022    Vivi Li

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.