Article [#6963] build usbotg fails at usb/musb/musb_core.c(2012)

[#6963] build usbotg fails at usb/musb/musb_core.c

Submitted By: Mingquan Pan

Open Date

2012-02-02 02:57:20     Close Date

2012-05-14 05:28:03

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF527     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

2011r1-rc4

App binary format:

N/A     

Summary: build usbotg fails at usb/musb/musb_core.c

Details:

build usbotg fails at usb/musb/musb_core.c on bf527 ezkit.

  CC [M]  net/sunrpc/timer.o^M

  CC [M]  net/sunrpc/sunrpc_syms.o^M

  CC [M]  net/sunrpc/cache.o^M

  CC [M]  net/sunrpc/rpc_pipe.o^M

  CC [M]  net/sunrpc/svc_xprt.o^M

  CC [M]  net/sunrpc/stats.o^M

  LD [M]  net/sunrpc/sunrpc.o^M

  LD      net/built-in.o^M

  LD      vmlinux.o^M

  MODPOST vmlinux.o^M

  GEN     .version^M

  CHK     include/generated/compile.h^M

  UPD     include/generated/compile.h^M

  CC      init/version.o^M

  LD      init/built-in.o^M

  LD      .tmp_vmlinux1^M

drivers/built-in.o: In function `musb_free':^M

/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x/drivers/usb/musb/musb_core.c:1841: undefined reference to `dma_controller_destroy'^M

drivers/built-in.o: In function `musb_init_controller':^M

/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x/drivers/usb/musb/musb_core.c:1918: undefined reference to `dma_controller_create'^M

make[1]: *** [.tmp_vmlinux1] Error 1^M

make[1]: Leaving directory `/home/test/work/cruise/checkouts/uclinux-dist/linux-2.6.x'^M

make: *** [linux] Error 1^M

last known good version:

root:/> ^[[6nversion^M

kernel:    Linux release 3.2.0-ADI-2012R1-pre-svn10315, build #69 Wed Jan 18 16:36:28 CST 2012^M

toolchain: bfin-uclinux-gcc release gcc version 4.3.5 (ADI-2011R1-RC4) ^M

user-dist: release svn-10626, build #895 Wed Jan 18 16:35:09 CST 2012^M

Follow-ups

--- Bob Liu                                                  2012-02-06 04:09:00

fixed. updated default config

--- Mingquan Pan                                             2012-05-14 06:27:54

build usbotg ok now. Close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

config.linux.usbotg

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.