Article [#7153] build spi net device fails for no enc28j60_hw.h(2012)

[#7153] build spi net device fails for no enc28j60_hw.h

Submitted By: Mingquan Pan

Open Date

2012-06-08 01:32:40     Close Date

2012-06-29 03:14:27

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

ADI-2012r1-beta1

App binary format:

N/A     

Summary: build spi net device fails for no enc28j60_hw.h

Details:

build spi net device fails for no  enc28j60_hw.h.

  GZIP    kernel/config_data.gz^M

  CHK     kernel/config_data.h^M

  UPD     kernel/config_data.h^M

  CC      kernel/configs.o^M

  LD      kernel/built-in.o^M

  CC      drivers/net/ethernet/microchip/enc28j60.o^M

  CC      drivers/net/enc28j60.o^M

drivers/net/enc28j60.c:32:25: error: enc28j60_hw.h: No such file or directory^M

drivers/net/enc28j60.c:75: error: ‘MAX_FRAMELEN’ undeclared here (not in a function)^M

drivers/net/enc28j60.c: In function ‘spi_read_buf’:^M

drivers/net/enc28j60.c:100: error: ‘ENC28J60_READ_BUF_MEM’ undeclared (first use in this function)^M

drivers/net/enc28j60.c:100: error: (Each undeclared identifier is reported only once^M

drivers/net/enc28j60.c:100: error: for each function it appears in.)^M

drivers/net/enc28j60.c: In function ‘spi_write_buf’:^M

drivers/net/enc28j60.c:128: error: ‘ENC28J60_WRITE_BUF_MEM’ undeclared (first use in this function)^M

drivers/net/enc28j60.c: In function ‘spi_read_op’:^M

drivers/net/enc28j60.c:151: error: ‘SPRD_MASK’ undeclared (first use in this function)^M

drivers/net/enc28j60.c:154: error: ‘ADDR_MASK’ undeclared (first use in this function)^M

drivers/net/enc28j60.c: In function ‘spi_write_op’:^M

drivers/net/enc28j60.c:173: error: ‘ADDR_MASK’ undeclared (first use in this function)^M

drivers/net/enc28j60.c: In function ‘enc28j60_soft_reset’:^M

drivers/net/enc28j60.c:187: error: ‘ENC28J60_SOFT_RESET’ undeclared (first use in this function)^M

drivers/net/enc28j60.c: In function ‘enc28j60_set_bank’:^M

drivers/net/enc28j60.c:198: error: ‘BANK_MASK’ undeclared (first use in this function)^M

drivers/net/enc28j60.c:203: error: ‘EIE’ undeclared (first use in this function)^M

drivers/net/enc28j60.c:203: error: ‘ECON1’ undeclared (first use in this function)^M

drivers/net/enc28j60.c:207: error: ‘ECON1_BSEL0’ undeclared (first use in this function)^M

drivers/net/enc28j60.c:209: error: ‘ENC28J60_BIT_FIELD_SET’ undeclared (first use in this function)^M

drivers/net/enc28j60.c:212: error: ‘ENC28J60_BIT_FIELD_CLR’ undeclared (first use in this function)^M

drivers/net/enc28j60.c:215: error: ‘ECON1_BSEL1’ undeclared (first use in this function)^M

drivers/net/enc28j60.c: In function ‘nolock_reg_bfset’:^M

drivers/net/enc28j60.c:244: error: ‘ENC28J60_BIT_FIELD_SET’ undeclared (first use in this function)^M

drivers/net/enc28j60.c: In function ‘nolock_reg_bfclr’:^M

drivers/net/enc28j60.c:262: error: ‘ENC28J60_BIT_FIELD_CLR’ undeclared (first use in this function)^M

drivers/net/enc28j60.c: In function ‘nolock_regb_read’:^M

drivers/net/enc28j60.c:280: error: ‘ENC28J60_READ_CTRL_REG’ undeclared (first use in this function)^M

Follow-ups

--- Scott Jiang                                              2012-06-15 02:51:50

Kernel update issue. Bob will take a look at it.

--- Bob Liu                                                  2012-06-18 05:03:58

fixed

--- Vivi Li                                                  2012-06-29 04:15:01

OK now.

Close it.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.