Article [#7218] run traps prefetch l1_instruction test make kernel panic

[#7218] run traps prefetch l1_instruction test make kernel panic

Submitted By: Mingquan Pan

Open Date

2012-07-31 03:39:52     Close Date

2012-08-15 04:50:00

Priority:

Medium     Assignee:

Bob Liu

Status:

Closed     Fixed In Release:

N/A

Found In Release:

N/A     Release:

Category:

N/A     Board:

N/A

Processor:

BF537     Silicon Revision:

Is this bug repeatable?:

Yes     Resolution:

Fixed

Uboot version or rev.:

    Toolchain version or rev.:

ADI-trunk/svn-5764

App binary format:

N/A     

Summary: run traps prefetch l1_instruction test make kernel panic

Details:

run traps prefetch l1_instruction test make kernel panic now.

Running test 20 for exception 0x00: prefetch l1_instruction^M

... Double Fault^M

Kernel OOPS in progress^M

Deferred Exception context^M

CURRENT PROCESS:^M

COMM=traps_test PID=192  CPU=0^M

TEXT = 0x02ae0040-0x02ae9000        DATA = 0x02ae9020-0x02aec814^M

BSS = 0x02aec814-0x02aeccb0  USER-STACK = 0x02aedf48^M

^M

return address: [0x0003853a]; contents of:^M

0x00038510:  600e  9851  4348  0c00  1ff2  0c06  1ffa  9a21 ^M

0x00038520:  2ff9  0000  04c3  e14c  0000  014f  e10c  0000 ^M

0x00038530:  3018  3239  3402  0c44  1003 [0001] 2000  e14a ^M

0x00038540:  0000  e10a  0000  9153  6002  304b  5211  0e08 ^M

^M

ADSP-BF537-0.2 500(MHz CCLK) 125(MHz SCLK) (mpu off)^M

Linux version 3.5.0-ADI-2012R1-pre-00797-g367b7b2 (test@uclinux55-bf537-cf) (gcc version 4.3.5 (ADI-trunk/svn-5764) ) #24 Sat Jul 28 20:13:32 CST 2012^M

^M

SEQUENCER STATUS:               Not tainted^M

SEQSTAT: 0000e021  IPEND: 0038  IMASK: 0000  SYSCFG: 0006^M

  Global Interrupts Disabled (IPEND[4])^M

  Peripheral interrupts masked off^M

  Kernel interrupts masked off^M

  EXCAUSE   : 0x21^M

^M

^M

U-Boot 2011.09-dirty (ADI-2011R1) (Nov 20 2011 - 05:52:00)^M

^M

CPU:   ADSP bf537-0.2 (Detected Rev: 0.2) (bypass boot)^M

Board: ADI BF537 stamp board^M

       Support: http://blackfin.uclinux.org/^M

Clock: VCO: 500 MHz, Core: 500 MHz, System: 125 MHz^M

RAM:   64 MiB^M

Flash: 4 MiB^M

MMC:   ^M

In:    serial^M

Out:   serial^M

Err:   serial^M

KGDB:  [on serial] ready^M

Follow-ups

--- Bob Liu                                                  2012-08-09 03:22:27

root:/> traps_test 20

Running test 20 for exception 0x00: prefetch l1_instruction

... FAIL (test exited sucessfully, and we expected 4 Illegal instruction

failure

FAIL (test completed properly 0/1 times)

0/1 tests passed

root:/>

--- Bob Liu                                                  2012-08-13 02:24:02

fixed

--- Mingquan Pan                                             2012-08-15 05:48:41

Yes, it doesn't panic kernel now.Close.

    Files

    Changes

    Commits

    Dependencies

    Duplicates

    Associations

    Tags

File Name     File Type     File Size     Posted By

No Files Were Found

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.